Test & Tools
  • Technologies
  • More
Test & Tools
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • MXO 4 New Feature: Log Frequency Axis Spectrum Analysis!

    shabaz
    shabaz
    Table of Contents Introduction What is it? What does it look like? EMC Pre-Compliance Testing Noise Measurements Notch Filter Band Pass Filter Summary Introduction Due to customer requests, the MXO 4 now supports a fully log-log spectrum output...
    • 11 Aug 2023
  • PST.. Program the Pico SCPI labTool?

    PST.. Program the Pico SCPI labTool?

    Jan Cumps
    Jan Cumps
    The Pico SCPI labTool (PST) allows you to connect your PC to equipment to control and monitor all sorts of things. It runs on a Raspberry Pico.In this post: functionality, and how to use SCPI or LabVIEW to program the device. Capab...
    • 6 Aug 2023
  • PST.. Have you worked with the Pico SCPI labTool?

    shabaz
    shabaz
    Table of Contents Introduction How Does it Work? What is Needed? Setting up the PC Download a SCPI Library Create a replica of Pico SCPI labTool in your own GitHub Repository Download the Pico SCPI labTool Project to your PC Building...
    • 5 Aug 2023
  • New Supercomputer Has a High Computational Power at Four exaFLOPS

    Catwell
    Catwell
    The CG-1 supercomputer has a computational power of 4 exaFLOPS at FP-16. It also features 54 million cores across 64 CS-2 nodes, supported by over 72 thousand AMD EPYC cores. (Image Credit: Rebecca Lewington/ Cerebras Systems) G42 and Cerebras intro...
    • 27 Jul 2023
  • Experimenting with an All-Pass Filter Using the ADALM1000 from Analog Devices

    jc2048
    jc2048
    I wanted to have a look at the Bode plotting with the ADALM1000, so I've chosen to start by looking at an all-pass filter circuit. The idea of an all-pass filter, one that passes all frequencies, seems slightly odd (is it really a 'filter&#39...
    • 3 Jul 2023
  • LTSpice Simulation on Mac

    ggabe
    ggabe
    Just recently, LTSpice has become my new favorite EE tool. I use a Mac, and to my biggest surprise, the Mac version does not have the toolbar icon that I see in YouTube videos. As a result, I found myself looking at a window without knowing what to d...
    • 3 Jul 2023
  • A Short Informal Review of the ADALM1000 from Analog Devices

    jc2048
    jc2048
    Introduction The ADALM1000 is a small module that acts like a combination of an oscilloscope, waveform generator, and SMU (source-measure unit). That gives enough capability to experiment with low-frequency circuits, to characterise many semiconducto...
    • 24 Jun 2023
  • DC Voltage Measurement Accuracy: AD584KH voltage reference

    DC Voltage Measurement Accuracy: AD584KH voltage reference

    Jan Cumps
    Jan Cumps
    Follow up on  DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500 . I bought a little voltage reference based on Analog Device's AD584 . The reference is the AD584KH. The kit supports the 4...
    • 20 Jun 2023
  • Nordic Power Profiler Kit II Python API

    ralphjy
    ralphjy
    The Nordic Power Profiler Kit II (PPK2) is a tool that measures power consumption by either providing power to the external board (source meter) or acting as an ampere meter. It measures current from 500 nA to 1 A and gives a detailed pictu...
    • 12 Jun 2023
  • DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500

    Jan Cumps
    Jan Cumps
    A little follow-up on  DC Voltage Measurement Accuracy: fact check Shabaz' graph . The DMM6500 has functions to improve  DC Volt measurements.  nplc or number of power line cycles: you can set the sample time in functio...
    • 11 Jun 2023
  • DC Voltage Measurement Accuracy: fact check Shabaz' graph

    Jan Cumps
    Jan Cumps
     shabaz created a DMM measurement accuracy graph for his  MP730624 Multimeter Quick Review: Surprisingly Accurate! blog. The graph shows the spec-ed accuracy of a MP730624 . He also shows graphs for other meters, like th...
    • 10 Jun 2023
  • MP730624 Multimeter Quick Review: Surprisingly Accurate!

    shabaz
    shabaz
    Table of Contents Introduction What comes in the Box? Using the Meter Things I didn’t like Things I liked Measurement Accuracy Using Bluetooth Summary Introduction I was on the lookout for a decent multimeter, but didn’t want to spend...
    • 10 Jun 2023
  • Soldering Wishlist gift! Duratool D00374 fume extractor

    strb
    strb
    A huge thank you to the E14 community that chose me as one of the lucky winners for the Wishlist - What do you need for Soldering? giveaway. This is my first prize/gift from the E14 community and that makes it special for me! A rather big (and beat u...
    • 10 May 2023
  • Solder Fume Extractor Tenma 21-7960

    charlieo21
    charlieo21
    I got this great solder fume extractor as a gift from element14, this was part of the "Wishlist - What do you need for Soldering?" giveaway. This will help me to keep away all the bad stuff out of my lungs. Also, I bought a used bench!, it is t...
    • 29 Apr 2023
  • looking for vector network analyzer simulator

    manojroy123
    manojroy123
    I am looking for free vector network analyzer simulator for simulation of R-L-C circuits and for simulation of attenuation. if anyone knows any free VNA simulation software. Please let me know about it.
    • 24 Apr 2023
  • USB-C Soldering Iron as a Daily Tool

    shabaz
    shabaz
    Table of Contents Introduction Which Soldering Irons and Tips? C245 Tips C210 Tips L245 Look and Feel Soldering Stand USB-C Cable USB-C Power Source Grounding DIY Power Supply Cost Temperature Configuration Sleep Settings Soldering Experience Other...
    • 15 Apr 2023
  • Generating Arbitrary Waveforms

    dougw
    dougw
    Displaying graphics on an oscilloscope is an interesting exercise and I decided to do this as part of a waveform generator road test. It turned out to be quite a process, involving 9 different software programs so I thought I would make a separa...
    • 8 Apr 2023
  • Keithley DMM6500 Scanner Card - Automation with TSP script

    Keithley DMM6500 Scanner Card - Automation with TSP script

    Jan Cumps
    Jan Cumps
    The Keithley DMM6500 / DAQ6510 family supports Test Script Processing (TSP) scripts. They are an alternative for SCPI control. The underlying scripting language is LUA.In this post, I'm showing a TSP script, and a brief look at the TestScriptBui...
    • 13 Mar 2023
  • These two new carbon capture systems could mitigate climate change and reduce carbon emissions

    Catwell
    Catwell
    Wood pieces at different stages of modification, from natural (far right) to delignified (second from right) to dried, bleached, and delignified (second from left) and MOF-infused functional wood (first on the left). (Image Credit: Gustavo Raskosky...
    • 7 Mar 2023
  • Keithley DMM6500 Scanner Card - temperature and 4-wire resistance continuous measurements

    Keithley DMM6500 Scanner Card - temperature and 4-wire resistance continuous measurements

    Jan Cumps
    Jan Cumps
    I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This 4th post shows a continuously running script that logs temperature and 4-wire resistance with th...
    • 6 Mar 2023
  • Quick hot-air soldering video

    shabaz
    shabaz
    Very bad and shaky video quality, but I've decided to upload this 2-minute video anyway, in case it helps anyone, because I struggled for years with hot air tools, and it only slowly dawned on me the issues I'd had were related to things like no pre-...
    • 5 Mar 2023
  • Keithley DMM6500 Scanner Card - 2-wire and 4-wire resistance measurements

    Keithley DMM6500 Scanner Card - 2-wire and 4-wire resistance measurements

    Jan Cumps
    Jan Cumps
    I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This 3rd post shows the 2-wire and 4-wire resistance measurement mode with the scanner card. ...
    • 10 Feb 2023
  • Keithley DMM6500 Scanner Card - wiring

    Keithley DMM6500 Scanner Card - wiring

    Jan Cumps
    Jan Cumps
    I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This 2nd post shows 2 ways I wired it: for easy use and for least resistance Twisted pair For my first tests...
    • 9 Feb 2023
  • Keithley DMM6500 Scanner Card - first impressions

    Keithley DMM6500 Scanner Card - first impressions

    Jan Cumps
    Jan Cumps
    I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This is my fist little test after receiving it. I bought a 2nd hand card. 250€ on eBay. It's the ...
    • 7 Feb 2023
  • Researchers develop a new shield to block EMI and allow wireless optical signals

    Catwell
    Catwell
    The grid-patterned mesh blocks electromagnetic interference while allowing optical communication channels. (Image Credit: Optical Materials Express (2022). DOI: 10.1364/OME.478830) Electronic devices are everywhere, including factories, medical faci...
    • 7 Feb 2023
<>