Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe&Sound: Wearable Tracking Device for Miners - 13: H/W design - Wearable Device
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
  • Author Author: sunnyiut
  • Date Created: 7 Jul 2017 5:51 AM Date Created
  • Views 933 views
  • Likes 4 likes
  • Comments 2 comments
  • msp432_launchpad
  • boostxl-sensors
  • safe and sound design challenge
  • msp432p401r
  • tft
Related
Recommended

Safe&Sound: Wearable Tracking Device for Miners - 13: H/W design - Wearable Device

sunnyiut
sunnyiut
7 Jul 2017

Title: Wearable Tracking Device for Miners

By: sunnyiut       

Previous Blogs
01: Introduction02: The Kit
03: Review_MSP432P401R04: Review_430BOOST-SHARP96
05: Review_BOOSTXL-SENSORS06: Review_DLP7970ABP
07: Project proposal update08: TFT interfacing
09: Light sensor interfacing10: Environmental sensor interfacing
11: IR temperature sensor interfacing12: Integrating 3 sensors in firmware

 

Design Challenge: Safe and Sound Wearables

Blog number: 13

 

 

 

 

Intro:

This blog is about the Hardware design of the wearable device that will be mounted on the wrist of the Miners.

 

 

Objective:image

 

The first part of my Project Proposal is to design a wearable device that contains the sensors for collecting the environmental information.

The Launchpad, sensor boosterpack and other necessary components in-together will be quite big and bulky to fit on the wrist. So, my objective is to design a customized board to make it wearable.

 

Components of the Wearable Device -

  • MSP432P401r
  • Sensors -
    • OPT3001
    • BME280
    • TMP007
  • TFT displayimage
  • Power supply
  • Battery charger
  • Selection buttons

 

Optional components [Not included in this project proposal] -

     These components will be implemented in the Hardware but the Firmware integration is left for future work.

 

  • MAX30100 sensor for Heart rate and SPO2
  • WSP2110 sensor for air quality [spec. Benzene]
  • BLE [RN4020] to send/receive beacons in between miners, in case of emergency

 

Board Design:

 

MSP432P401r [MCU and other supportive circuitry] -                                           TFT display -

imageimage

 

Sensors -                                                                                                    Power supply -

imageimage

 

Bluetooth Low Energy -                                                            

image

 

 

PCB:

 

image

 

3D Layout:

imageimageimage

 

** that's basically the end of the designing the first part [wearable device] of my proposal. As the time is short, I'll try to develop the board later on, if I can manage some time.

image

Meanwhile,

I placed the order for PCB fab on 20th June.

Unfortunately, the delivery got stuck into EID vacation [it's a big one in my countryimage]  and customs clearanceimage

 

However, I have received it yesterday. I don't have much time left for the Project Submission.

So at first I'll post my blogs on the two other parts of my project proposal -

  • Miners location detection based on RFID and
  • Central monitor to display and log miners' location

 

My next blog post will be on Reading Miners' RFID tags to detect their location.

  • Sign in to reply
Parents
  • sayansarkarnitdgp
    sayansarkarnitdgp over 8 years ago

    Kindly suggest some good places for PCB fab !!! How can i integrate other sensors like MAX30100 sensor for Heart rate and SPO2 in my system ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sunnyiut
    sunnyiut over 8 years ago in reply to sayansarkarnitdgp

    for general purpose or say hobbyist lots of people go for https://www.seeedstudio.io/fusion_pcb.html

    In my case I went for myropcb

    They are little bit expensive for low volume fab. I had a discount coupon, that's why I went for myropcb.

     

    about MAX30100, I would like to suggest to go for MAX30101 or MAX30102. As far as I know MAX30100 is no more in active production.

    This sensor provides control over I2C communication. However, you need a separate 1.8v supply for it.

    you can follow the application notes from MAXIM for guideline on how to use this chip.

    this link also provides some valuable info ..... https://morf.lv/implementing-pulse-oximeter-using-max30100

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sunnyiut
    sunnyiut over 8 years ago in reply to sayansarkarnitdgp

    for general purpose or say hobbyist lots of people go for https://www.seeedstudio.io/fusion_pcb.html

    In my case I went for myropcb

    They are little bit expensive for low volume fab. I had a discount coupon, that's why I went for myropcb.

     

    about MAX30100, I would like to suggest to go for MAX30101 or MAX30102. As far as I know MAX30100 is no more in active production.

    This sensor provides control over I2C communication. However, you need a separate 1.8v supply for it.

    you can follow the application notes from MAXIM for guideline on how to use this chip.

    this link also provides some valuable info ..... https://morf.lv/implementing-pulse-oximeter-using-max30100