Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe&Sound: Wearable Tracking Device for Miners - 15: Final Post - Project summary
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
  • Author Author: sunnyiut
  • Date Created: 10 Jul 2017 8:12 AM Date Created
  • Views 1872 views
  • Likes 5 likes
  • Comments 7 comments
  • safe and sound design challenge
Related
Recommended

Safe&Sound: Wearable Tracking Device for Miners - 15: Final Post - Project summary

sunnyiut
sunnyiut
10 Jul 2017

Title: Wearable Tracking Device for Miners

By: sunnyiut

Previous Blogs
01: Introduction02: The Kit
03: Review_MSP432P401R04: Review_430BOOST-SHARP96
05: Review_BOOSTXL-SENSORS06: Review_DLP7970ABP
07: Project proposal update08: TFT interfacing
09: Light sensor interfacing10: Environmental sensor interfacing
11: IR temperature sensor interfacing12: Integrating 3 sensors in firmware
13: H/W design - Wearable Device14: RC522- reading RFID tags

 

Design Challenge: Safe and Sound Wearables

Blog number: 15

 

 

 

Intro:

This is my final blog post regarding this design challenge.

I am writing this blog at around 1 pm in my time, that is around 7 am GMT.

 

As the deadline approaches near, I am presenting whatever I have done so far.

 

 

Brief Project Proposal Overview:

image

 

My Project Proposal was to design a wearable device which will be mounted on the wrist of the Miners to collect and display environmental information and develop an RFID based system to track the location of the miners.

 

System components -

  • 1. Wearable device mounted on the wrist of the miner
    • sensors -
      • ambient light
      • ambient temperature
      • atmospheric pressure
      • relative humidity
      • contact-less IR temperature sensor to measure object temperature
    • TFT display unit
    • Battery charger and PSU
  • 2. RFID 13.56MHz tag reader to detect valid ID of the miners
    • it will be placed at the entry of the working zone
    • miners have to punch their tags during entry
    • at detection of valid ID it will display the miner's profile
    • send the miner's ID and working zone ID with entry time to the central monitor
  • 3. Central monitor will collect miners' location for all the RFID device placed at different zones, and log it for future investigation.

 

I have completed designing the first two components of the total system. Right now I am working on the 'Central Monitor' part. As I don't have any more time left on project submission deadline, I am posting the final updates of the first two components. I have already posted a couple of demonstrations regarding these devices in my previous blogs. So in this blog I'll post the final updates only.

 

1. The wearable device:

 

Experimental Setup and sample display output - demonstration can be found in this blog [12: Integrating 3 sensors in firmware]

imageimage

 

Final product - I have not populated some of the components those are not needed for this project proposal [like the TFT touch panel interface etc.]

imageimageimage

 

imageimageimage

 

imageimage

 

2. RFID Reader to locate Miners: demonstration can be found in this blog [14: RC522- reading RFID tags]

 

imageimageimage

 

Both the devices together:

imageimageimage

 

3. Central Monitor:

I am still working on this part of the system. I'll carry it on and post my updates later on..... may be after the submission deadline image

 

However, It's been a nice design challenge - I've enjoyed a lot playing with these kits.

Creative and awesome projects and blogs have been posted so far by the contestants. So many things to learn......

 

I have tried my best to contribute whatever I can, though not in a regular manner. My blog posts were irregular, I am sorry for that.

 

Thanks to ELEMENT14 and TI for this opportunity.

 

UPDATE:

A few days back I have received a gift from Element 14 to participate in this design challenge. It's a eZ430 - Chronos Development Tool from TI.

imageimage

 

There was also a thanks giving note ..... image

 

image

  • Sign in to reply

Top Comments

  • e14phil
    e14phil over 9 years ago in reply to sunnyiut +5
    This project is great, I have really enjoyed following along with your progress. Even if the competition deadline has passed I would love to see how your project will evolve and would highly recommend…
  • DAB
    DAB over 9 years ago +4
    Nice finish to a good challenge entry. The purpose of the blog requirement is to keep the community up to date on your progress so they can see your design evolve into an implementation. You managed to…
  • sunnyiut
    sunnyiut over 9 years ago in reply to e14phil +4
    thank you Phil. I'll keep posting my updates regarding this project. After all my efforts and supports from the forum, i have to make it up to a full featured system at the end.
Parents
  • DAB
    DAB over 9 years ago

    Nice finish to a good challenge entry.

     

    The purpose of the blog requirement is to keep the community up to date on your progress so they can see your design evolve into an implementation.

     

    You managed to do that well.  You have a nice platform from which to do a lot of good science data collection and I look forward to seeing what you find.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sunnyiut
    sunnyiut over 9 years ago in reply to DAB

    Thank you image

     

    Your enthusiastic words always inspired me. Also you have a great way to put your analytical comments and new ideas, which helped me and others to evolve our projects for sure.

    I'll try my best to implement the full system to check out some real life data collection.

    Indeed I have designed the hardware of the wearable device with some extra sensors and features [which I have not included in this project proposal, will work on it in near future] like air quality monitor, heart rate etc.

    I've also put one of your idea in my head to implement later on- That's using PIR motion sensor along with RFID for detection of external intruders in the mining area. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 9 years ago in reply to sunnyiut

    This project is great, I have really enjoyed following along with your progress.

     

    Even if the competition deadline has passed I would love to see how your project will evolve and would highly recommend finishing it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14phil
    e14phil over 9 years ago in reply to sunnyiut

    This project is great, I have really enjoyed following along with your progress.

     

    Even if the competition deadline has passed I would love to see how your project will evolve and would highly recommend finishing it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • sunnyiut
    sunnyiut over 9 years ago in reply to e14phil

    thank you Phil.

     

    I'll keep posting my updates regarding this project. After all my efforts and supports from the forum, i have to make it up to a full featured system at the end. image

    • Cancel
    • Vote Up +4 Vote Down