Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog First Steps - Intel Edison step 3
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
  • Author Author: mcb1
  • Date Created: 7 Feb 2017 1:29 AM Date Created
  • Views 1915 views
  • Likes 5 likes
  • Comments 7 comments
  • why upcycle
  • intel edison competition
  • recycle
  • upcycle it
  • upcycling
  • intel edison
Related
Recommended

First Steps - Intel Edison step 3

mcb1
mcb1
7 Feb 2017

Yesterday I got to this point.  First Steps - Intel Edison step 2

 

 

 

So for some unknown reason, I seem to be going backwards.

image

 

Obviously about now I'm starting to make noises or worse.

image

I want to program this on my laptop and I'm not looking forward to repeating it.

Somewhere there is 3GB of Hard Drive used, but the 292MB file it downloaded is there.

 

I decided enough was enough for tonight, and since it came back with exactly the same screen AGAIN I chose Finish.

 

As it closed there were multiple warnings about the F:\ drive requiring formatting and this

image

 

So presumably after a disconnect and repower it might wake up and we can proceed.

 

 

 

Next Day

I did some searching on the internet to see if I could sort out why it didn't want to talk.

I tried the tool but it seemed to be stuck at this picture.

image

The Next never came up.

 

Windows knew the drivers were there

image

 

 

 

I had tried the manual method of flashing it using this document.

https://software.intel.com/en-us/node/637975

How do I update/flash the IntelRegistered Edison board firmware manually?

 

Sadly no matter what I did the reboot and subsequent detection failed, so it never went through the process.

The sparkfun article suggested copying evrything to the drive, and then issue a command via PuTTy.

https://learn.sparkfun.com/tutorials/edison-getting-started-guide#updating-the-firmware-image

 

The drive showed up as a plain drive with 767MB free in windows.

But the downloaded image contained a .ext4 file that was 1.34 GB but theirs was only 536MB.

 

 

PuTTy

About this stage I was ready to try anything.

I fired up PuTTy aimed it at the right COM Port and started a session.

 

When it connected, the prompt was not what was expected and it didn't know any commands.

 

So I tried entering "reboot" and amazingly it did.

It came back to the same point.

 

Again no commands seemed to work, so I entered "exit" to see if anything might happen.

To my surprise it did a few things and gave me the Login prompt.

 

Flash the image

Since I could force a reboot and the session stayed up, I thought I'd try the manual reflash again.

 

Basically you download and extract the image, then copy dfu-util.exe and libusb-1.0.dll into the same folder.\

Open a command prompt (i ran as Administrator) and change directory to the extracted file.

You then type 'flashall.bat" and it will ask you to reboot.

 

This time I issued the command reboot via the PuTTy session and amazingly things happened.

  imageimage

 

After a period of time it completed.

image

 

So I have a working version of fireware.

 

Firmware

There seems to be a newer version of firmware labelled

iot-devkit-prof-dev-image-edison-20160606-patch.zip

 

The internet suggest you can tell what version you are running by typing in a session

"configure_edison --version"

I seem to get this response

image

 

The configuration tool seems to now be happy.

image

Interestingly if you click on the link, it takes you to here https://software.intel.com/iot/hardware/edison/downloads

Latest Yocto* Poky image is the patched version.

 

So I now have a properly flashed Intel Edison.

 

I'm not going to connect to the WiFi just yet.

I want to setup a seperate network that I can use offline.

So that step can wait.

 

 

I need to stick the Grove shield back on and fit the LED and I need to work out what jumpers J8 and J9 do.

 

Hopefully all I need to do on my Laptop is install the drivers.

 

 

Mark

 

 

This started as a simple blog, but has now grown over a few posts, so an index is appropriate.

 

Link to other posts
What is Electronic Up-Cycling
Electronic Upcycling ideas
Design Challenge Blogs
First Steps - Intel Edison
First Steps - Intel Edison step 2
First Steps - Intel Edison step 3
First Steps - Intel Edison step 4 
First Steps - Intel Edison step 5
First Steps - Intel Edison Arduino
First Steps - Intel Edison Arduino 2


  • Sign in to reply

Top Comments

  • clem57
    clem57 over 9 years ago in reply to mcb1 +1
    I am getting there sloooowwwwwly, One box at a time. It may be a few months
  • DAB
    DAB over 9 years ago +1
    Now you know why I put it aside while I deal with other issues. My current level of ADD made my brain freeze when I tried to follow the instructions, so I am looking at what you are doing. So far, you…
Parents
  • DAB
    DAB over 9 years ago

    Now you know why I put it aside while I deal with other issues.

     

    My current level of ADD made my brain freeze when I tried to follow the instructions, so I am looking at what you are doing.

     

    So far, you have confirmed my decision to wait a bit.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to DAB

    @DAB

    I have to admit that if I had more on my plate I would have put it to one side as well.

    It does seem that the Linux community are well versed in uploading images and doing things using manual methods.

     

     

    We used to have some excellent members here who were able to bridge that gap and provide a method we mortals could follow.

    I'm also certain that a Linux OS may not have had some of the problems.

     

    I didn't even open the box last night, so today ...

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to DAB

    @DAB

    I have to admit that if I had more on my plate I would have put it to one side as well.

    It does seem that the Linux community are well versed in uploading images and doing things using manual methods.

     

     

    We used to have some excellent members here who were able to bridge that gap and provide a method we mortals could follow.

    I'm also certain that a Linux OS may not have had some of the problems.

     

    I didn't even open the box last night, so today ...

     

    mark