Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog First Steps - Intel Edison step 5
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
  • Author Author: mcb1
  • Date Created: 9 Feb 2017 12:35 PM Date Created
  • Views 1387 views
  • Likes 6 likes
  • Comments 3 comments
  • upcycleit
  • why upcycle
  • intel edison competition
  • upcycle
  • recycle
  • intel edison
Related
Recommended

First Steps - Intel Edison step 5

mcb1
mcb1
9 Feb 2017


My last steps left me with a flashed image onto the Edison ... or so I thought.

 

When I plugged it into the home computer, it reported unable to detect the image.

Worse was the constant change as it detected, then dropped, detected, dropped (you get the idea) one port.

 

I was able to connect via PuTTy to the device and it was stuck in a constant reboot mode.

I was able to stop it Autobooting by pressing a key at the correct time.

Once I had the Autoboot stopped, the dropping also stopped.

 

This resulted in a limited environment which seemed to be an "Input Shell".

Typing 'help' gave me a bunch of instructions that I could use including 'reset' of the CPU.

 

About now I'm wondering if I hadn't shut it down, or that it hadn't completed something.

But I did recall it was happily sitting there, and all the power lights went out before I unplugged it, so I must have held the PWR button down for 10 secs.

 

 

I'm starting to question what I did wrong and if something in the installation was at fault.

The driver file is available, but the configuration tool seems to ignore these and do it's own thing.

 

I had added another driver at some point, and while the utility and driver install should have replaced it, I thought it was a good idea to start again.

 

I used the Uninstall software and removed the drivers that had been added recently.

The other program was also removed (it didn't seem to do anything) and then I fired up the configuration Utility (and confirmed the agreement AGAIN).

I made sure it was running in Administrator Mode, and let it install the drivers.

 

 

Reflash

My Laptop from earlier in the morning said the Edison had a new image, so in theory it should be fine.

BUT the utility reported it was unable to detect the image.

 

Once again it got stuck at the point of not detecting the board, unless I repowered or pressed the pwr button, and then the constant rebooting started.

 

By now I'm starting to feel like I'm the central character in "Ground Hog Day"

image

Photo Groundhog Day (1993) - IMDb

 

Flash Lite had some success, it got to talk with the Edison but eventually it came up with a new message that it failed and you needed to flash it manually.

image

 

 

 

Manual Reflash

I talked about the manual reflash method earlier First Steps - Intel Edison step 3

Now that I knew I could force the reboot using PuTTy, I was more confident.

 

Unzip the file, add the two files and then use the command prompt to run Flashall.bat

I had a connection via PuTTy and between the power button and the Ctrl-C, I did manage to get it to talk.

 

So after a while it uploaded and rebooted and it PuTTy sesion came back with "edison login:" and sat patiently.

image

 

The full text is below in case someone wants to compare

C:\Temp\Flash>flashall.bat
Using U-boot target: edison-blankrndis
Now waiting for dfu device 8087:0a99
Please plug and reboot the board
Dfu device found
Flashing IFWI
Download        [=========================] 100%      4194304 bytes
Download done.
Download        [=========================] 100%      4194304 bytes
Download done.
Flashing U-Boot
Download        [=========================] 100%       237568 bytes
Download done.
Flashing U-Boot Environment
Download        [=========================] 100%        65536 bytes
Download done.
Flashing U-Boot Environment Backup
Download        [=========================] 100%        65536 bytes
Download done.
Rebooting to apply partiton changes
Dfu device found
Flashing boot partition (kernel)
Download        [=========================] 100%      6144000 bytes
Download done.
Flashing rootfs, (it can take up to 5 minutes... Please be patient)
Download        [=========================] 100%   1373159424 bytes
Download done.
Rebooting
U-boot & Kernel System Flash Success...
Your board needs to reboot to complete the flashing procedure, please do not unp
lug it for 2 minutes.

C:\Temp\Flash>

 

 

 

 

Version

By now I've tried almost everything and I'm wondering if there is something I've missed.

 

You should be able to see the version number when you login with PuTTy and type "configure_edison --version"

But like earlier, it reports it's unable to.

The /media/storage folder is still a read-only, but it is 767MB in size.

 

Time to try it.

 

 

 

 

Arduino 1.8.1

I decided that it might be worth downloading the latest version since it should support the Intel Edison.

Strangely the board is not included, so using Board Manager, I received a whole lot of 1's and 0's for the Intel i686

(see here for the full description The specified item was not found. )

 

I opened the example Basics - Blink and to my surprise it had changed ... quite a bit.

/*
  Blink
  Turns on an LED on for one second, then off for one second, repeatedly.

  Most Arduinos have an on-board LED you can control. On the UNO, MEGA and ZERO 
  it is attached to digital pin 13, on MKR1000 on pin 6. LED_BUILTIN is set to
  the correct LED pin independent of which board is used.
  If you want to know what pin the on-board LED is connected to on your Arduino model, check
  the Technical Specs of your board  at https://www.arduino.cc/en/Main/Products
  
  This example code is in the public domain.

  modified 8 May 2014
  by Scott Fitzgerald
  
  modified 2 Sep 2016
  by Arturo Guadalupi
  
  modified 8 Sep 2016
  by Colby Newman
*/


// the setup function runs once when you press reset or power the board
void setup() {
  // initialize digital pin LED_BUILTIN as an output.
  pinMode(LED_BUILTIN, OUTPUT);
}

// the loop function runs over and over again forever
void loop() {
  digitalWrite(LED_BUILTIN, HIGH);   // turn the LED on (HIGH is the voltage level)
  delay(1000);                       // wait for a second
  digitalWrite(LED_BUILTIN, LOW);    // turn the LED off by making the voltage LOW
  delay(1000);                       // wait for a second
}

 

I made sure I had the right COM Port and hit upload

 

I was very surprised when it came back with :-

image

 

The verbose lines are

Sketch uses 76331 bytes (0%) of program storage space. Maximum is 10000000 bytes.
#!/bin/sh

# clupload script to invoke lsz 
# Copyright (C) 2014 Intel Corporation
starting download script
# 
Args to shell: C:\Users\MBeckett\AppData\Local\Arduino15\packages\Intel\tools\sketchUploader\1.6.2+1.0/x86/bin C:\Users\MBeckett\AppData\Local\Temp\arduino_build_468494/Blink.ino.elf COM21
# This library is free software; you can redistribute it and/or
# modify it under the terms of the GNU Lesser General Public
# License as published by the Free Software Foundation; either
# version 2.1 of the License, or (at your option) any later version.
# 
# This library is distributed in the hope that it will be useful,
# but WITHOUT ANY WARRANTY; without even the implied warranty of
# MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
# Lesser General Public License for more details.
#
# You should have received a copy of the GNU Lesser General Public
# License along with this library; if not, write to the Free Software
# Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
#

echo "starting download script"
echo "Args to shell:" $*

# ARG 1: Path to lsz executable.
# ARG 2: Elf File to download
# ARG 3: COM port to use.

#path contains \ need to change all to /
path_to_exe=$1
fixed_path=${path_to_exe//\\/\/}

#COM ports are not always setup to be addressed via COM for redirect.
#/dev/ttySx are present. Howwever, COMy -> /dev/ttySx where x = y - 1

com_port_arg=$3
com_port_id=${com_port_arg/COM/}
echo "COM PORT" $com_port_id
tty_port_id=/dev/ttyS$((com_port_id-1))
echo "Converted COM Port" $com_port_arg "to tty port" $tty_port_id

echo "Sending Command String to move to download if not already in download mode"
echo "~sketch downloadEdison" > $tty_port_id
COM PORT 21
Converted COM Port COM21 to tty port /dev/ttyS20
Sending Command String to move to download if not already in download mode

Deleting existing sketch on target
#Move the existing sketch on target.
echo "Deleting existing sketch on target"
"$fixed_path/lsz.exe" --escape -c "mv -f /sketch/sketch.elf /sketch/sketch.elf.old" <> $tty_port_id 1>&0

Transfer incomplete
# Execute the target download command

#Download the file.
host_file_name=$2
"$fixed_path/lsz.exe" --escape --binary --overwrite $host_file_name <> $tty_port_id 1>&0
Sending: Blink.ino.elf

Bytes Sent:   1024/  75668   BPS:65641    ETA 00:01  
Bytes Sent:   9216/  75668   BPS:590771   ETA 00:00  
Bytes Sent:  10240/  75668   BPS:656412   ETA 00:00  
Bytes Sent:  11264/  75668   BPS:722053   ETA 00:00  
Bytes Sent:  12288/  75668   BPS:787694   ETA 00:00  
Bytes Sent:  13312/  75668   BPS:853336   ETA 00:00  
Bytes Sent:  14336/  75668   BPS:918977   ETA 00:00  
Bytes Sent:  15360/  75668   BPS:984618   ETA 00:00  
Bytes Sent:  16384/  75668   BPS:1050259  ETA 00:00  
Bytes Sent:  17408/  75668   BPS:1115901  ETA 00:00  
Bytes Sent:  18432/  75668   BPS:1181542  ETA 00:00  
Bytes Sent:  19456/  75668   BPS:1247183  ETA 00:00  
Bytes Sent:  20480/  75668   BPS:1312824  ETA 00:00  
Bytes Sent:  21504/  75668   BPS:1378466  ETA 00:00  
Bytes Sent:  22528/  75668   BPS:1444107  ETA 00:00  
Bytes Sent:  23552/  75668   BPS:1509748  ETA 00:00  
Bytes Sent:  24576/  75668   BPS:1575389  ETA 00:00  
Bytes Sent:  25600/  75668   BPS:820514   ETA 00:00  
Bytes Sent:  26624/  75668   BPS:853334   ETA 00:00  
Bytes Sent:  27648/  75668   BPS:886155   ETA 00:00  
Bytes Sent:  28672/  75668   BPS:918975   ETA 00:00  
Bytes Sent:  29696/  75668   BPS:951796   ETA 00:00  
Bytes Sent:  30720/  75668   BPS:984616   ETA 00:00  
Bytes Sent:  31744/  75668   BPS:1017437  ETA 00:00  
Bytes Sent:  32768/  75668   BPS:1050258  ETA 00:00  
Bytes Sent:  33792/  75668   BPS:1083078  ETA 00:00  
Bytes Sent:  34816/  75668   BPS:1115899  ETA 00:00  
Bytes Sent:  35840/  75668   BPS:1148719  ETA 00:00  
Bytes Sent:  36864/  75668   BPS:1181540  ETA 00:00  
Bytes Sent:  37888/  75668   BPS:1214360  ETA 00:00  
Bytes Sent:  38912/  75668   BPS:1247181  ETA 00:00  
Bytes Sent:  39936/  75668   BPS:1280002  ETA 00:00  
Bytes Sent:  40960/  75668   BPS:1312822  ETA 00:00  
Bytes Sent:  41984/  75668   BPS:1345643  ETA 00:00  
Bytes Sent:  43008/  75668   BPS:1378463  ETA 00:00  
Bytes Sent:  44032/  75668   BPS:940855   ETA 00:00  
Bytes Sent:  45056/  75668   BPS:942595   ETA 00:00  
Bytes Sent:  46080/  75668   BPS:944263   ETA 00:00  
Bytes Sent:  47104/  75668   BPS:945864   ETA 00:00  
Bytes Sent:  48128/  75668   BPS:947402   ETA 00:00  
Bytes Sent:  49152/  75668   BPS:967560   ETA 00:00  
Bytes Sent:  50176/  75668   BPS:968630   ETA 00:00  
Bytes Sent:  51200/  75668   BPS:969679   ETA 00:00  
Bytes Sent:  52224/  75668   BPS:970689   ETA 00:00  
Bytes Sent:  53248/  75668   BPS:971662   ETA 00:00  
Bytes Sent:  54272/  75668   BPS:990347   ETA 00:00  
Bytes Sent:  55296/  75668   BPS:990950   ETA 00:00  
Bytes Sent:  56320/  75668   BPS:991532   ETA 00:00  
Bytes Sent:  57344/  75668   BPS:992094   ETA 00:00  
Bytes Sent:  58368/  75668   BPS:992637   ETA 00:00  
Bytes Sent:  59392/  75668   BPS:993161   ETA 00:00  
Bytes Sent:  60416/  75668   BPS:993668   ETA 00:00  
Bytes Sent:  61440/  75668   BPS:1010510  ETA 00:00  
Bytes Sent:  62464/  75668   BPS:1010728  ETA 00:00  
Bytes Sent:  63488/  75668   BPS:1010940  ETA 00:00  
Bytes Sent:  64512/  75668   BPS:1011144  ETA 00:00  
Bytes Sent:  65536/  75668   BPS:1011343  ETA 00:00  
Bytes Sent:  66560/  75668   BPS:1027145  ETA 00:00  
Bytes Sent:  67584/  75668   BPS:1027097  ETA 00:00  
Bytes Sent:  68608/  75668   BPS:1011903  ETA 00:00  
Bytes Sent:  69632/  75668   BPS:1027006  ETA 00:00  
Bytes Sent:  70656/  75668   BPS:1026947  ETA 00:00  
Bytes Sent:  71680/  75668   BPS:1026905  ETA 00:00  
Bytes Sent:  72704/  75668   BPS:1026864  ETA 00:00  
Bytes Sent:  73728/  75668   BPS:1026824  ETA 00:00  
Bytes Sent:  74752/  75668   BPS:1041085  ETA 00:00  
Bytes Sent:  75668   BPS:1011577                         

Transfer complete

 

And the onboard LED is blinking

 

 

Mark

 

 

 

This started as a simple blog, but has now grown over a few posts, so an index is appropriate.

 

Link to other posts
What is Electronic Up-Cycling
Electronic Upcycling ideas
Design Challenge Blogs
First Steps - Intel Edison
First Steps - Intel Edison step 2
First Steps - Intel Edison step 3
First Steps - Intel Edison step 4 
First Steps - Intel Edison step 5
First Steps - Intel Edison Arduino
First Steps - Intel Edison Arduino 2


  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +3
    Great news and really helpful for the challengers. I spotted that there are lots of Edison based projects over at CodeProject https://www.codeproject.com/search.aspx?q=edison&x=0&y=0&sbo=kw There's also…
  • mcb1
    mcb1 over 9 years ago in reply to DAB +3
    Thanks There are some other terms ... but that one is more 'public' friendly. It seems that there is some room for improvement in the utilities. I'm surprised that you have to go digging for the Flash…
  • DAB
    DAB over 9 years ago +1
    I admire your perseverance. DAB
Parents
  • DAB
    DAB over 9 years ago

    I admire your perseverance.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    I admire your perseverance.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to DAB

    Thanks

    There are some other terms ... but that one is more 'public' friendly.

     

    It seems that there is some room for improvement in the utilities.

    I'm surprised that you have to go digging for the Flash Lite utility and it has information that the other one doesn't.

     

    That said, there seems to be a lot of support from Intel within their community, and I imagine it will increase as more people find ways to do stuff.

    We've seen that with Arduino, Raspberry Pi and Beagle Bone to name a few.

     

    Hopefully today I can do a bit more discovery.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down