Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • “GB PoE+ - Ethernet-USB” adapter for industrial use with an EMC perspective

    “GB PoE+ - Ethernet-USB” adapter for industrial use with an EMC perspective

    Würth Elektronik
    Würth Elektronik
    The “GB PoE+ - Ethernet-USB” adapter was developed on the basis of the reference design “GB-Ethernet-USB Adapter”, which operates without Power over Ethernet (PoE). The adapter without PoE is described in detail in Application Note RD016; the electromagnetic compatibility tests can be found in Application Note ANP116. The “GB PoE+ - Ethernet-USB” adapter has three interfaces, one USB Type-CTm (USB 3.1), one RJ45/Ethernet…
    • 5 Sep 2023
  • See what could happen to your design even with a big insulation distance but with too much condensation

    See what could happen to your design even with a big insulation distance but with too much condensation

    Würth Elektronik
    Würth Elektronik
    Between each pole of an electrical product standards give insulation distances. This is mainly called “Creepage and clearance”. This will avoid to have short circuits or breakdown (sparks) in case of overvoltage and thus for all the life of the product.
    • 29 Aug 2023
  • ANP122 | Gigabit Power over Ethernet Interface from an EMC perspective

    ANP122 | Gigabit Power over Ethernet Interface from an EMC perspective

    Würth Elektronik
    Würth Elektronik
    The “GB PoE+ -Ethernet-USB” adapter was developed on the basis of the reference design “GB-Ethernet-USB Adapter”, which operates without Power over Ethernet (PoE).
    • 21 Aug 2023
  • ANP074 | Introduction to RF Inductors

    ANP074 | Introduction to RF Inductors

    Würth Elektronik
    Würth Elektronik
    RF inductors are used in a wide range of industries from consumer products to highly specialized scientific applications. RF inductors can be used in a plethora of functions in high frequency circuit design. These roles include circuit-tuning, impedance matching, filtering and even as high frequency chokes. One large market today is their use in wireless devices, such as tablets, but also in emerging products like IoT…
    • 25 Jul 2023
  • Simple design tips that will cool down the temperature of your PCB

    Simple design tips that will cool down the temperature of your PCB

    Würth Elektronik
    Würth Elektronik
    Temperature increase is a natural behavior of electricity. Each component has a resistance and each resistance release heat with current. This is of course the case for connectors and PCB traces. A designer needs to choose his connector and traces cross section to have as less heat as possible. But not oversize them for a question of space and cost. Arrhenius law says that increasing of 10°C the temperature of a PCB…
    • 21 Jul 2023
  • ANP114: Voltage and Frequency Dependence of Ferroelectric Class 2 Multilayer Ceramic Capacitors

    ANP114: Voltage and Frequency Dependence of Ferroelectric Class 2 Multilayer Ceramic Capacitors

    Würth Elektronik
    Würth Elektronik
    After introducing ferroelectricity, a mathematical model for the capacitance-voltage behavior of multilayer ceramic capacitors (MLCCs) is derived from a dipole polarization model. The parameters of the model are reduced to two fitting parameters. The model is tested against measurements from a selection of MLCCs in the Würth Elektronik portfolio to demonstrate practicality. Since the integral of the capacitance-voltage…
    • 10 Jul 2023
  • ANS019 | Bipolar power supply and isolated signal transmission with MagI³C-FIMM

    ANS019 | Bipolar power supply and isolated signal transmission with MagI³C-FIMM

    Würth Elektronik
    Würth Elektronik
    Industrial plants, such as warehouse logistics, filling plants, rolling mills, conveyor belts and printing presses, generally require the use of a selection of the following elements for safe operation: Isolation amplifiers, analog-to-digital converters Isolation of digital circuits Interfaces/bus isolation - RS232, RS485, CAN, Interbus, Profibus Measurement and data acquisition
    • 26 Jun 2023
  • ANE018: Plastic Material Properties

    ANE018: Plastic Material Properties

    Würth Elektronik
    Würth Elektronik
    It has been observed that the natural color of halogen-free polyamide (PA) plastic used in Würth Elektronik connectors turns brown during the SMT process (Reflow soldering). The aim of this technical note is to understand this phenomenon and demonstrate whether and how it may impact the plastic material properties of our connectors. This was achieved by conducting spectroscopy IR and differential scanning calorimetry…
    • 22 May 2023
  • Positioning & timing GNSS: Introduction

    Positioning & timing GNSS: Introduction

    Würth Elektronik
    Würth Elektronik
    GNSS (Global Navigation Satellite System) is a system, which provides positioning and time synchronization capabilities to an unlimited number of users worldwide. The system is based on signals from the following four satellite constellations.
    • 17 May 2023
  • ANP121: Filter and surge protection for I²C Bus

    ANP121: Filter and surge protection for I²C Bus

    Würth Elektronik
    Würth Elektronik
    The I²C (Inter-Integrated Circuit) bus is a popular serial communication interface on many circuit boards. It is mainly used to connect microcontrollers with peripheral ICs (e.g. sensors or memory). The bus uses a bidirectional data line (SCL) and clock line (SDA) respectively. However, the I²C bus is not only used on circuit boards. In many applications, the I²C bus is extended into other areas using various connectors…
    • 24 Apr 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 6: Modern Card Standards Secure Digital (SD) is a Non-Volatile Memory format developed by the SD Card Association (SDA) for use in portable devices. It was launched in 1999 to improve the MMC standard. SanDisk, Panasonic and Toshiba collaborated to create the SD Association in 2000. At the time, there was only one form factor for the SD card. The logo itself is a reuse of the logo created by Toshiba for the Super…
    • 17 Apr 2023
  • ANP083: Adapter PCB for filtering electromagnetic interference on an RS-485 interface

    ANP083: Adapter PCB for filtering electromagnetic interference on an RS-485 interface

    Würth Elektronik
    Würth Elektronik
    As a result of the constantly growing number of applications based on networked communication via data lines, it is becoming increasingly important to ensure trouble-free operation as well as the safety of electrical systems and devices. By filtering directly at the interface, interference emissions, electrostatic discharges (ESD) and fast transients (burst) are prevented from entering the system and thus negatively influencing…
    • 11 Apr 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 5: Memory extensions In 1973, R2E created the first microprocessor-based computer the micro-ordinateur, or microcomputer. By the end of the decade, progress made in available RAM and ergonomics made microcomputer usable even by non-trained scientists.
    • 4 Apr 2023
  • ANP007 Effective USB 3.2 Gen 2x2 filtering and protection

    ANP007 Effective USB 3.2 Gen 2x2 filtering and protection

    Würth Elektronik
    Würth Elektronik
    The USB connector and standard are one of the most widely implemented and successful interfaces ever used. The applications are commercial and industrial, and both have been pushing the standard to be faster. The USB standard has been updated to version 3.2 (Table 1). This standard increases data transfer speeds to 5 GBits/s (Gen 1), 10 GBit/s (Gen 2) and 20 GBit/s (Gen 2x2).
    • 21 Mar 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 4: Logic Memories Using logic gates (AND, OR, XOR, NOT), it is possible to create a system where you input a value (an address) and you receive a predictable answer (a data output). This form of memory is sometimes called a lookup table, or Read-Only Memory. ROM is non-volatile and fast to access. Random Access Memory will instead store data dynamically, even faster, easily editable but volatile.
    • 21 Mar 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 3: Film And Magnetic Storage In 1839, Louis Daguerre created the daguerreotype, a method of capturing a picture on a polished metal sheet using chemicals. This is the beginning of photography, lit. “Writing with light”. In 1894, the Lumière brothers created the Cinématographe, a device able to write and read a photographic film – to create a movie and then project it with the same device. A real memory storage, all…
    • 7 Mar 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 2 : Mechanical and Optical Storage The first offline memory support was made way before the first electronics. From the beginning of the nineteenth century, holes in cards made of rigid paper were used to automate a mechanical loom to weave thread: the Jacquard loom.
    • 21 Feb 2023
  • ANP116 | Gigabit Ethernet interface from an EMC perspective

    ANP116 | Gigabit Ethernet interface from an EMC perspective

    Würth Elektronik
    Würth Elektronik
    In the design of an Ethernet interface, questions often arise concerning the shield connection of the cable and the front-end design, especially regarding the ground connections. Research on the Internet reveals various suggestions for the shield connection, where a 1 nF Y-capacitor is often suggested. However, the effect of the interface on performance and the EMC behavior are not described. This App Note takes a detailed…
    • 13 Feb 2023
  • Offline Memory Technology

    Offline Memory Technology

    Würth Elektronik
    Würth Elektronik
    Part 1 : Memory Hierarchy When working in the electronic industry, sometimes we have to look at the bigger picture to avoid losing sight. After starting my career in integrated circuits manufacturing R&D, I ended up working on electromechanical components development for signal chains applications. A change of scale, of role, of place in the industry. This sparked my interest in the technological implications of my work…
    • 7 Feb 2023
  • ANP090: Keep the Balance – Balancing of Supercapacitors

    ANP090: Keep the Balance – Balancing of Supercapacitors

    Würth Elektronik
    Würth Elektronik
    Supercapacitors (SC) usually operate at low voltages of around 2.7 V. In order to reach higher operating voltages, it is necessary to build a cascade of serial connected SC cells. [1] [2] Due to production or aging related variations in capacitance and insulation resistance the voltage drop over individual capacitors may exceed the rated voltage limit. Thus, a balancing system is required to avoid accelerated aging of…
    • 23 Jan 2023
  • ANR008:WIRELESS CONNECTIVITY SDK

    ANR008:WIRELESS CONNECTIVITY SDK

    Würth Elektronik
    Würth Elektronik
    The Würth Elektronik eiSos wireless modules provide an easy to use radio interface to any embedded application. The module’s interface with the host processor of the embedded application via UART can be operated using a command interface. The Wireless Connectivity SDK is a set of software tools that enable quick software integration of Würth Elektronik eiSos wireless modules into any of the most commonly used host processors…
    • 19 Jan 2023
  • ANP109: Impedance Spectra of Different Capacitor Technologies

    ANP109: Impedance Spectra of Different Capacitor Technologies

    Würth Elektronik
    Würth Elektronik
    Impedance and capacitance spectra (or scattering parameters) are common representations of frequency dependent electrical properties of capacitors. The interpretation of such spectra provides a wide range of electrochemical, physical and technical relevant information. Those need to be separated from the ever-present measurement artifacts as well as parasitic effects. Since it is sometimes not possible to provide all…
    • 19 Dec 2022
  • Isolated MagI³C Power Module Masters the 24V Industry Bus I

    Isolated MagI³C Power Module Masters the 24V Industry Bus I

    Würth Elektronik
    Würth Elektronik
    In the industrial environment, 24 V bus systems are widely used to supply a wide range of field devices. What problems can arise during implementation and how can they be solved?
    • 19 Dec 2022
  • RD016 | Gigabit-Ethernet Front End

    RD016 | Gigabit-Ethernet Front End

    Würth Elektronik
    Würth Elektronik
    This document provides the circuit developer with an optimized circuit design and layout with all technical data for a Gigabit Ethernet Front End. The electronics board has two interfaces, one USB C (USB 3.1) - and one Gigabit RJ45/Ethernet interface. The GB-Ethernet-USB adapter was developed on the basis of the EVB-LAN7800LC Evaluation Board from Microchip. The circuit is built on a 4-layer PCB and in the present design…
    • 28 Nov 2022
  • Wireless M-bus: Introduction

    Wireless M-bus: Introduction

    Würth Elektronik
    Würth Elektronik
    Wireless Meter Bus (wM-BUS) is the extension of the meter Bus (M-BUS) with a wireless protocol and role scheme for handling communication over a standardized wireless communication interface between meters and data loggers – so called smart meter gateways (SMGW). This scheme is specified by the European standard EN 13757 and its sub-standards. The motivation of this standard is to allow an automated measuring and processing…
    • 8 Nov 2022
<>