RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Renesas Envision Kit RX65N Roadtest Part Four B - User Fit Parts
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Andrew J
  • Date Created: 3 Dec 2019 9:53 AM Date Created
  • Views 1645 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended
  • rpbrx65n
  • envision kit
  • renesas

Renesas Envision Kit RX65N Roadtest Part Four B - User Fit Parts

Andrew J
Andrew J
3 Dec 2019

There are DNF positions on the Envision Board for users to extend the capability with Ethernet, SD card and a joystick.  The User Guide details these with a set of part numbers and they are tracked up to pins on the MCU so it should just be a case of getting the parts needed and soldering them on.  Some will need the LCD removing to do so which whilst, apparently, not difficult has not been made as simple as really it ought to be given this need.  As part of my road test I am (was) intending to use the SD card so I have been looking to get the part, which led me to check on the other parts’ availability as well.  I normally acquire parts from UK.Farnell, CPC.Farnell, RS Components, Mouser and Digikey.  My preference is that Mouser and Digikey are last resort as they ship from the US - I’m in the UK.   I have not checked Amazon, eBay, Alibaba, Banggood etc as I don’t trust those sources.

 

These are my results:

 

ItemManufacturerManufacturer Part NumberAvailability
SD/ MMC Connector, SMDAmphenol101-00565-64101-00565-64Obsolete part, no longer available.  It is an unusual pin configuration, 13+2, so I can’t find a direct replacement.  It may be possible to get a smaller pin-count part and solder it off-board with wires to the relevant pads but I haven’t looked into that.
Power Management IC, SOIC8IntersilISL61861BIBZOnly available from Mouser so ships from the US and thus extremely expensive (and not very environmentally friendly)
Ethernet Connector, SMDPulseJ3011G21DNLOnly available from Mouser, or UK.Farnell as a US ship, so again financially and environmentally expensive
RMII Ethernet Transceiver, QFN24MicrochipLAN8720AReadily available.  The 24-QFN package is a bit of a pain to solder but it would seem that this particular part doesn't come in any other package

 

5-switch Joystick, SMD
ALPSSKQUDBE010SKQUDBE010Obsolete part, no longer available.  I didn’t look to find if an alternative existed.

 

So, I won’t be using the SD card in my road test.  I shall ask on the Forum and see if anyone has identified alternatives for any of these parts.

 

Summary Thoughts

For an evaluation kit they really ought to make changes to the board to bring it up to date with market-wide readily available parts.  This is pretty poor given that the board was made available in September 2017 and is still in mass production status.

 

Further Entries

I will update this entry to provide links to further instalments as I create them:

Part One: Introduction

Part Two: Getting Going

Part Three: Development Software

Part Four A: Brief note on Smart Configurator

Part Four B: Brief note on User Fit Parts (this post)

Part Four C: Segger emWin Introduction

Part Four D: Removal of the LCD

Part Four E: Analog to Digital Conversion

Part Five: Static Setup of the GUI

Part Six: Getting the Display Working

Part Seven: USB/Serial Interface

 

Roadtest review

 

Also, worth reading Jan Crump's road test as he's taking a more technical approach.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago +2
    For the SD card, a USB memory stick is an alternative. Renesas’ tfat library supports it (used in the default safe_boot example to upload firmware)
  • Andrew J
    Andrew J over 6 years ago in reply to Jan Cumps +2
    Yes I could, and might, but I had intended to use the USB port for something else. I do think the point I make is valid on this one: for something that is only just 2 years old, obsolete components already…
  • n5kzw
    n5kzw over 6 years ago +1
    It's good to see a critical review of a kit when criticism is warranted. Good job.
  • Andrew J
    Andrew J over 6 years ago in reply to Jan Cumps

    Yes I could, and might, but I had intended to use the USB port for something else.  I do think the point I make is valid on this one: for something that is only just 2 years old, obsolete components already is a bit of a letdown.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago

    For the SD card, a USB memory stick is an alternative. Renesas’ tfat library supports it (used in the default safe_boot example to upload firmware)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • n5kzw
    n5kzw over 6 years ago

    It's good to see a critical review of a kit when criticism is warranted.  Good job.