Welcome to
FPGA

FPGA discusses the latest trends in programmable logic devices, and offers access to education, workshops, webinars on FPGAs, SoCs, and other programmable devices.

Featured Content
design challenge tile
Collaborated with image

Path III is the third session in the element14 Community’s structured FPGA-based SoC training. The first Path was held in 2018 and focused on programmable logic devices PLDs and featured the AVNET MiniZed development board, based on AMD’s Zynq-7000 SoC.

Path II convened in 2019 and offered more advanced learning opportunities and featured the AVNET Ultra96-V2 development board, based on AMD’s Zynq UltraScale+ MPSoC.

Path III will double the fun by offering structured training on both the MiniZed and Ultra96-V2 boards. Each training track will be followed by a design/build phase.

Learn More

Recent Blogs
  • OrangeCrab Game Console - Part 2

    Patiently Waiting for the PCBs In these high-inflation times I try to be frugal where I can.  I've ordered boards from China in the past and while the PCB prices themselves are very affordable the $20 or so for express shipping isn't nec...
  • Master project for FPGA VHDL with Digilent Arty - Artix-7

    Dear friend, I am a new master's student, I need help with my master's project. I have a Digilent Arty - Artix-7 board. what kind of project I can research for 2 years?
  • OrangeCrab Gaming Console - Part 1

    Introduction One of the advantages of membership in the Element14 community is the opportunity to evaluate brand new products and technologies.  Back in 2021 during the summer of FPGAs I was lucky enough to be selected to road test the Oran...
  • Quadrature Sinewave Generator on Lattice XP2 using Brevia 2 Development Board

    Introduction Some more simple DSP [digital signal processing] stuff with my lovely little Lattice Brevia-2 board with its XP2 FPGA. A couple of years back, I did a collection of blogs called 'Waves' using this board (see the links at the end). For th…
  • Booting up Ultrazed-EG dev board

    Hello all, I am not able to boot up the board even after following the steps exactly given in the manual. It seems that the board is not drawing any current as the fan which I am mounting on it is also not powering up and the PS red LED is also not g…
Related Projects