FPGA
  • Technologies
  • More
FPGA
Blog XuLA2 FPGA - SD Card Read and Write
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 30 Jan 2017 9:45 PM Date Created
  • Views 5563 views
  • Likes 8 likes
  • Comments 7 comments
  • spartan_6
  • microsd
  • xilinx
  • fpga
  • xula2
  • jcxula2
  • xess
Related
Recommended

XuLA2 FPGA - SD Card Read and Write

Jan Cumps
Jan Cumps
30 Jan 2017

Let's try to do something real with the Xilinx Spartan-6 FPGA: write a set of data to an SD card.

image

 

To boost the FPGA skills, I'm refreshing theory and checking out some real designs.

For a standalone XuLA2 board, talking to SD cards is a good practical example.

 

There's  a Micro SD slot on the XuLA2 models. The only other component you need is a spare Micro SD card.

 

Don't use an SD card with your marriage photo shoot on it. You'll very likely loose that when you test this project.

 

The Xess XuLA2 github has two SD card projects. We'll use the SD Card Control Test example.

In this project, the FPGA has two main duties:

  • Read and Write SD data
  • Communicate with your PC over USB

A python script on your PC will generate test data and send it to the FPGA over USB.

The FPGA writes the data to your SD card. We're using low level protocol here, no filesystem.

When finished, it reads the data back off the SD card and verifies the results.

 

VHDL Libraries

 

Xess made a set of common VHDL libraries. The example uses several those libs.

The communication with the SD slot is via :

  • SDCard.vhd

Clocking is handled by these two:

  • ClkGen.vhd
  • SyncToClk.vhd

Talk to the PC over USB happens with this one (and the on-board PIC microcontroller):

  • HostIo.vhd

These libs are not only useful, but also a great source to learn reusable VHDL.

 

image

 

How it Works

 

The XESS blog explains the example in detail. It explains both the electrical connections and how the Micro SD protocol is handled.

The header comments of the SdCard.vhd source file document many implementation details.

Open that file by double-clicking the u3 - SdCardCtrl node in the Implementation view.

If you've ever tried to understand (or port) a microcontroller SDCard lib - maybe the one from Arduino - you'll recognise much of the logic.

 

Let's now synthesize the project and generate the programming file.

Insert the SD card, connect the XuLA2 with your laptop and load the bitstream:

 

xsload --fpga sdcardctrltest.bit

 

Once you've loaded the bitstream, your XuLA2 board sits idle. You need to tell it to read and write data.

There's a python scrip that does exactly that.

If you have retrieved the latest XuLA2 FPGA sources from GIT, you'll find a python file named SDcardTest.py in the project directory.

If you're using the examples that were installed by the XESS installer, you can retrieve the testbed from here:

https://raw.githubusercontent.com/xesscorp/XuLA2/master/FPGA/SdcardCtrlTest/SdcardTest.py

 

Run the script to write a random set of data to the SD card, read it back and check if everything is correct:

 

SDcardTest.py

 

image

 

The data is written using low level protocol. You will not be able to read the data when you insert the SD card into your PC.

The design doesn't use a filesystem or any other advanced disk management protocol. It's SD access for real blokes.

 

Windows 8 and Windows 10 with Xilinx ISE

 

If you are running WIndows 10 64-bit, you may encounter several ISE problems:

 

  • Pressing the Open Project button (and several other actions, like selecting the Preferences menu item) crashes ISE.
  • Running the Simulator results in a "failed to link the design" message and the simulator not starting.

 

Switching to the 32-bit version has solved most of them for me:

To switch,

  • alter the command in the ISE shortcut to
    "<DRIVE>:\Xilinx\14.7\ISE_DS\settings32.bat D:\Xilinx\14.7\ISE_DS\ISE\bin\nt\ise.exe"
  • in "<DRIVE>:\Xilinx\14.7\ISE_DS\ISE\bin\nt", rename fuse.exe to _fuse.exe, and copy the fuse.exe from the "..\nt64" directory over (got that from here)

 

After that, I still have one issue left: when in Simulator, the Relaunch functionality doesn't work. I have to close iSIM and restart it from within ISE.

 

I've also tested the design with a known defect card - one that's rejected by any known operating system and can't be formatted.

This test was successful. The test flagged that the FPGA wasn't able to write data, as expected:

 

image

 

The core of the example can be used in your own design as a persistent storage area.

If you want to use it as a data exchange mechanism, you'll have to find a way to read the raw data from the card. That can be done with an Arduino.

Another - advanced - option is to implement a supported file systems (fat32?) in HDL,

Whatever you do, make it a nice design and share your work.

 

 

XuLA2 FPGA - First Impressions of the Development Tools
XuLA2 FPGA - SD Card Read and Write
XuLA2 FPGA - Rotary Encoder and VHDL
XuLA2 FPGA - PWM with Dead Band in VHDL
XuLA2 FPGA - Up the Clock
XuLA2 FPGA - Utility to Generate Pin Assignments
XuLA2 FPGA - Test the VGA StickIt! Module: Image Preparation
  • Sign in to reply
Parents
  • dundich
    dundich over 8 years ago

    Hello Jan.

     

    I'd like to connect another Spartan board to SD Card and write data through script SdcardTest.py  

    But I don't heve on-board PIC microcontroller. Could I use the FTDI USB-JTAG convertor to link PC with SD Card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dundich
    dundich over 8 years ago

    Hello Jan.

     

    I'd like to connect another Spartan board to SD Card and write data through script SdcardTest.py  

    But I don't heve on-board PIC microcontroller. Could I use the FTDI USB-JTAG convertor to link PC with SD Card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to dundich

    I have been able to initialise an SD card with a Papilio board. That’s a Spartan and FTDI linked together. I used the Sd Card Init example from Michael Fields (hamster.nz).

    I don’t have the results anymore, it was in 2015.

    The example dis not exchange data, only did a valid startup sequence of the card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to dundich

    http://hamsterworks.co.nz/mediawiki/index.php/SD_card_testing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dundich
    dundich over 8 years ago in reply to Jan Cumps

    Thanks for help!