Power & Energy
  • Technologies
  • More
Power & Energy
Blog STM32H7B3I - TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
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
  • Author Author: Jan Cumps
  • Date Created: 19 Aug 2020 3:21 PM Date Created
  • Views 8215 views
  • Likes 3 likes
  • Comments 30 comments
  • stm32h7b3i
  • rt
  • stm32h7b3i-dk
Related
Recommended

STM32H7B3I - TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens

Jan Cumps
Jan Cumps
19 Aug 2020

I'm selected for the STM32H7B3I-DK -  DISCOVERY KIT road test.

I'm working on a touch screen GUI for my electronic load.

In this post I'm trying a mock interface - see how I can switch between screens

Thank you fellow roadtester jomoenginer for sending me a very good starting project.

 

image

image source: the mockup running in simulator mode on my laptop

 

Goal: Build an app with two screens, display data and info

 

I'm putting some light goals here. I've already checked other TouchGFX parts, button click event handling and showing external data.

Here, I want to see if I can:

  • react on an internal event (a timer tick)
  • show a different form on the screen, from code.
  • try if my basis user interaction scenario would work

 

image

image: proposed GUI flow

 

This is a mock interface. I do not really query my electronic load. Values and messages are made up.

Check previous posts (linked below) to see how a real interaction over a serial interface works.

 

Initial Script: use Timer to Show a Progress Bar and Status while Starting Up

 

The process I'm mocking here, is checking if the test instrument is connected, then check what mode it is in.

While doing that, display a progress bar. And intermediate statuses.

Then when that's done, move to another screen based on the instrument's mode.

 

I used ST's Progress Bar tutorial to learn about using background processes and keeping the interface active at the same time.

 

image

 

There are different locations to react to a TouchGFX tick. I want the tick to animate the screen (progress bar) so I used the home screen View's tick.

I told before that this is a mock. Instead of really checking if the electronic load is ready, I faked a few moments when to simulate that the instrument was up, and it reported it's mode:

 

void MainView::handleTickEvent() {
     static int timesAnimated = 0;

     int currentValue = progrBar.getValue();
     int16_t max;
     int16_t min;
     progrBar.getRange(min, max);


     if (currentValue == min)  {
         increase = true;
         timesAnimated++;
     } else if (currentValue == max) {
         increase = false;
         timesAnimated++;
     }

     int nextValue = increase == true ? currentValue+1 : currentValue-1;
     progrBar.setValue(nextValue);

     if (timesAnimated == 2 ) { 
       Unicode::strncpy(txtStatusBuffer, (const char*)"init THEBREADBOARD,ELECTRONICLOAD,1,1.0", TXTSTATUS_SIZE);
       txtStatus.invalidate();
     }

     if (timesAnimated == 3 ) {
       Unicode::strncpy(txtStatusBuffer, (const char*)"mode detected: constant current", TXTSTATUS_SIZE);
       txtStatus.invalidate();
     }

     if (timesAnimated == 4 ) {
       static_cast<FrontendApplication*>(Application::getInstance())->gotoDisplayCCScreenNoTransition();
     }

}

 

Most of this code is indeed simulation, but there is one new thing I wanted to test: Opening a new screen when the instrument reports ready:

 

static_cast<FrontendApplication*>(Application::getInstance())->gotoDisplayCCScreenNoTransition();

 

This is the mechanism to make the LCD switch another display.

The gotoDisplayCCScreenNoTransition() method is generated by the TouchGFX Designer.

When I created the second screen, called DisplayCC, I defined the handler for its display, by generating an interaction.

 

image

No matter in what screen yo define that interaction, the functions generted will end up in FrontendApplicationBase.cpp:

 

// DisplayCC

void FrontendApplicationBase::gotoDisplayCCScreenNoTransition() {
    transitionCallback = touchgfx::Callback<FrontendApplicationBase>(this, &FrontendApplication::gotoDisplayCCScreenNoTransitionImpl);
    pendingScreenTransitionCallback = &transitionCallback;
}

void FrontendApplicationBase::gotoDisplayCCScreenNoTransitionImpl() {
    touchgfx::makeTransition<DisplayCCView, DisplayCCPresenter, touchgfx::NoTransition, Model >(&currentScreen, &currentPresenter, frontendHeap, &currentTransition, &model);
}

 

Calling the first function from the TouchGFX Application API is all that's needed to switch screens.

The second screen is very simple too. Again a mock:

 

image

 

Then - just to check the look and feel, I animate the two mock measured values:

 

void DisplayCCView::handleTickEvent() {
  static float iCurr = 0.998;
  static float iVolt = 3.898;
  static uint16_t count = 0;

  if ((count % 50) == 15) {
    iCurr = 0.997;
    iVolt = 3.898;
  }

  if ((count % 50) == 40) {
    iCurr = 0.998;
    iVolt = 3.899;
  }

  count++;

  Unicode::snprintfFloat(txtCurrentValBuffer, TXTCURRENTVAL_SIZE, "%3.3f A", iCurr);
  Unicode::snprintfFloat(txtVoltageValBuffer, TXTVOLTAGEVAL_SIZE, "%3.3f V", iVolt);
  txtCurrentVal.invalidate();
  txtVoltageVal.invalidate();
}

 

image

image source: the mockup running on the road test kit

 

What did I learn? That it's not hard to switch screens and use the clock ticks to keep a reactive application when in parallel the system is preparing startup or other things.

With the investigations done before - serial communication, backend data integration, sending commands, I'm set for the next step: real integration.

 

Related Posts
First Experience with CubeIDE
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 1: Screen Works
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works
TouchGFX Simple Example: react on a button click
USB, freeRTOS ,Task Notifications and Interrupts
the Development Kit STMod+ Connector and Using UART2
TouchGFX Application Framework: Model, View, Presentation, Message Queue
TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
TouchGFX Application Framework: MVP and the ModelListener
Write a CubeIDE MX application: Hardware Cryptography with DMA
Attachments:
MyApplication_1_20200819.zip
  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 6 years ago in reply to Jan Cumps +2
    This is the meat I'm really interested in Jan. Looking forward to your 'real integration'.
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    I've uploaded the project file to the post.
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    Using container for the upper sceen part:
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    Using container for the upper sceen part:

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    Hello my friend!!

    this is my example but it has some inconsistencies I hope you can help me

    https://community.st.com/s/question/0D53W00000MC0XcSAL/wifi-http-server-stm32h7b3idk-with-wifi-module-ism43340m4gl4410-c…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to crisv22

    the file password is stm32h7b3i-crisv22

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • crisv22
    crisv22 over 6 years ago in reply to crisv22

    the file password is stm32h7b3i-crisv22

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    Cristian, I am afraid that I am not the right person to help.

    Your questions dig deeper in the WiFi stack than I ever dug into.

    I checked if it worked (it does, if you use the right version of Renesas examples. It fails with many obscure messages if you don't).

    I did not dig deeper than that. I will not be able to dig deeper in the future because I removed the controller from the PCB.

    Maybe you can contact another road tester, or the Renesas forum?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    Yes, please, friend, if you can put me in contact with another colleague, it would be very helpful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    I don't have colleagues that work with this controller, but you can check the other road testers by navigating to:

    STM32H7B3I-DK -  DISCOVERY KIT ,

    then  click on the RoadTesters tab.