Power & Energy
  • Technologies
  • More
Power & Energy
Blog STM32H7B3I - TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
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
  • Author Author: Jan Cumps
  • Date Created: 19 Aug 2020 3:21 PM Date Created
  • Views 8075 views
  • Likes 3 likes
  • Comments 30 comments
  • stm32h7b3i
  • rt
  • stm32h7b3i-dk
Related
Recommended

STM32H7B3I - TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens

Jan Cumps
Jan Cumps
19 Aug 2020

I'm selected for the STM32H7B3I-DK -  DISCOVERY KIT road test.

I'm working on a touch screen GUI for my electronic load.

In this post I'm trying a mock interface - see how I can switch between screens

Thank you fellow roadtester jomoenginer for sending me a very good starting project.

 

image

image source: the mockup running in simulator mode on my laptop

 

Goal: Build an app with two screens, display data and info

 

I'm putting some light goals here. I've already checked other TouchGFX parts, button click event handling and showing external data.

Here, I want to see if I can:

  • react on an internal event (a timer tick)
  • show a different form on the screen, from code.
  • try if my basis user interaction scenario would work

 

image

image: proposed GUI flow

 

This is a mock interface. I do not really query my electronic load. Values and messages are made up.

Check previous posts (linked below) to see how a real interaction over a serial interface works.

 

Initial Script: use Timer to Show a Progress Bar and Status while Starting Up

 

The process I'm mocking here, is checking if the test instrument is connected, then check what mode it is in.

While doing that, display a progress bar. And intermediate statuses.

Then when that's done, move to another screen based on the instrument's mode.

 

I used ST's Progress Bar tutorial to learn about using background processes and keeping the interface active at the same time.

 

image

 

There are different locations to react to a TouchGFX tick. I want the tick to animate the screen (progress bar) so I used the home screen View's tick.

I told before that this is a mock. Instead of really checking if the electronic load is ready, I faked a few moments when to simulate that the instrument was up, and it reported it's mode:

 

void MainView::handleTickEvent() {
     static int timesAnimated = 0;

     int currentValue = progrBar.getValue();
     int16_t max;
     int16_t min;
     progrBar.getRange(min, max);


     if (currentValue == min)  {
         increase = true;
         timesAnimated++;
     } else if (currentValue == max) {
         increase = false;
         timesAnimated++;
     }

     int nextValue = increase == true ? currentValue+1 : currentValue-1;
     progrBar.setValue(nextValue);

     if (timesAnimated == 2 ) { 
       Unicode::strncpy(txtStatusBuffer, (const char*)"init THEBREADBOARD,ELECTRONICLOAD,1,1.0", TXTSTATUS_SIZE);
       txtStatus.invalidate();
     }

     if (timesAnimated == 3 ) {
       Unicode::strncpy(txtStatusBuffer, (const char*)"mode detected: constant current", TXTSTATUS_SIZE);
       txtStatus.invalidate();
     }

     if (timesAnimated == 4 ) {
       static_cast<FrontendApplication*>(Application::getInstance())->gotoDisplayCCScreenNoTransition();
     }

}

 

Most of this code is indeed simulation, but there is one new thing I wanted to test: Opening a new screen when the instrument reports ready:

 

static_cast<FrontendApplication*>(Application::getInstance())->gotoDisplayCCScreenNoTransition();

 

This is the mechanism to make the LCD switch another display.

The gotoDisplayCCScreenNoTransition() method is generated by the TouchGFX Designer.

When I created the second screen, called DisplayCC, I defined the handler for its display, by generating an interaction.

 

image

No matter in what screen yo define that interaction, the functions generted will end up in FrontendApplicationBase.cpp:

 

// DisplayCC

void FrontendApplicationBase::gotoDisplayCCScreenNoTransition() {
    transitionCallback = touchgfx::Callback<FrontendApplicationBase>(this, &FrontendApplication::gotoDisplayCCScreenNoTransitionImpl);
    pendingScreenTransitionCallback = &transitionCallback;
}

void FrontendApplicationBase::gotoDisplayCCScreenNoTransitionImpl() {
    touchgfx::makeTransition<DisplayCCView, DisplayCCPresenter, touchgfx::NoTransition, Model >(&currentScreen, &currentPresenter, frontendHeap, &currentTransition, &model);
}

 

Calling the first function from the TouchGFX Application API is all that's needed to switch screens.

The second screen is very simple too. Again a mock:

 

image

 

Then - just to check the look and feel, I animate the two mock measured values:

 

void DisplayCCView::handleTickEvent() {
  static float iCurr = 0.998;
  static float iVolt = 3.898;
  static uint16_t count = 0;

  if ((count % 50) == 15) {
    iCurr = 0.997;
    iVolt = 3.898;
  }

  if ((count % 50) == 40) {
    iCurr = 0.998;
    iVolt = 3.899;
  }

  count++;

  Unicode::snprintfFloat(txtCurrentValBuffer, TXTCURRENTVAL_SIZE, "%3.3f A", iCurr);
  Unicode::snprintfFloat(txtVoltageValBuffer, TXTVOLTAGEVAL_SIZE, "%3.3f V", iVolt);
  txtCurrentVal.invalidate();
  txtVoltageVal.invalidate();
}

 

image

image source: the mockup running on the road test kit

 

What did I learn? That it's not hard to switch screens and use the clock ticks to keep a reactive application when in parallel the system is preparing startup or other things.

With the investigations done before - serial communication, backend data integration, sending commands, I'm set for the next step: real integration.

 

Related Posts
First Experience with CubeIDE
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 1: Screen Works
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works
TouchGFX Simple Example: react on a button click
USB, freeRTOS ,Task Notifications and Interrupts
the Development Kit STMod+ Connector and Using UART2
TouchGFX Application Framework: Model, View, Presentation, Message Queue
TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
TouchGFX Application Framework: MVP and the ModelListener
Write a CubeIDE MX application: Hardware Cryptography with DMA
Attachments:
MyApplication_1_20200819.zip
  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 6 years ago in reply to Jan Cumps +2
    This is the meat I'm really interested in Jan. Looking forward to your 'real integration'.
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    I've uploaded the project file to the post.
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    Using container for the upper sceen part:
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    I've uploaded the project file to the post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    What a good day

     

    I have not been able to test the example, it marks errors when running it with the different versions it suggests

     

    STM32Cube\Repository\STM32Cube_FW_H7_V1.8.0\Projects\STM32H7B3I-DK\Demonstrations\ClockAndWeather

     

     

    How can I test the WiFi module ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    For me, the Clock and Weather example that comes with that firmware pack 1.8 works.

    You can import it via Help -> Information Center -> Import STM32Cube Example

    image

    Do you get an error while building or while loading?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    Will you be notified of the following errors?

    if it works well?

     

    image

    How can I test the wifi module (ism43340-m4g-l44-10cf-c6.2.1.8) separately with AT commands ?

    Without using the example, as they are connected serially or spi, the serial terminal does not recognize me, it does not respond to any command AT

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    I'm using CubeIDE 1.4.2 and don't get compile errors.

     

    I haven't investigated the AT interface. I just tried that example and it connects to my wifi when I enter the password.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    thanks as soon as you know something about the wifi module let me know, I have found very little information

    good day friend

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    thanks as soon as you know something about the wifi module let me know, I have found very little information

    good day friend

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    crisv22  wrote:

     

    ... as soon as you know something about the wifi module let me know, I have found very little information ...

    The network interface, with the API for the module, is located here:

    /ClockAndWeather/Middleware/STM32_Network_Library/core

     

    Application code that talks to that API is found in these source file:

    /ClockAndWeather/Application/User/Core/clock_weather_app.c
    /ClockAndWeather/Application/User/TouchGFX/gui/model/Model.cpp

     

    The AT interface functions are found in this file:

    /ClockAndWeather/Drivers/BSP/Components/ES_WIFI/es_wifi.c

     

    static ES_WIFI_Status_t AT_ExecuteCommand(ES_WIFIObject_t *Obj, uint8_t* cmd, uint8_t *pdata);

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    hi, my friend

    you can make a WIFI http server with stm32h7b3i-dk  ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to crisv22

    There is the example we have discussed above, that shows how to get an internet connection via WiFi.

     

    There's another example,  LwIP_HTTP_Server_Netconn_RTOS, that shows how to implement a HTTP server on a STM32H7.

    It's for a different board and controller. But maybe it is portable? ST has ported it to F4 and F7 families.

     

    You could check if, by trying to combine the two, you get a working server.

     

    crisv22  wrote:

     

    hi, my friend

    you can make a WIFI http server with stm32h7b3i-dk  ???

    I have no plan to do this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisv22
    crisv22 over 6 years ago in reply to Jan Cumps

    Hello my friend

    I try to combine the programs and nothing works.

     

     

    How to configure the wifi module (ISM43340-M4G-L44-10 CF) with serial communication from how many baud to how to send AT commands from stm32h7b3i-dk?

     

     

    In the future do you plan to use the wifi module of this stm32h7b3i-dk board?