Just Encase
  • Challenges & Projects
  • Design Challenges
  • Just Encase
  • More
  • Cancel
Just Encase
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Just Encase to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Blog#6  Conclusion (Case Enclosure Reliability Monitor)

    Blog#6 Conclusion (Case Enclosure Reliability Monitor)

    skruglewicz
    skruglewicz
    Blog#6  Conclusion (Case Enclosure Reliability Monitor) This blog is a wrap up of Conclusions and Possible Future Enhancements to this Design Challenge: Just Encase  Blog Series. This is my final blog in the series. I want to thank&nb...
    • 24 Feb 2022
  • Blog#5 Testing  Part 2  TEST#2

    Blog#5 Testing Part 2 TEST#2

    skruglewicz
    skruglewicz
    BLOG#5 Testing Part 2 (Case Enclosure Reliability Monitor) Test#2 -  Enclosure 155H2GYCL Test Design For this Test, I purchased two Grove Sensors from Seeed and used two of sensors from the supplied Grove starter Kit.This is my 2nd Test, us...
    • 24 Feb 2022
  • Blog#2  Design (Case Enclosure Reliability Monitor)

    Blog#2 Design (Case Enclosure Reliability Monitor)

    skruglewicz
    skruglewicz
    Blog#2  Design (Case Enclosure Reliability Monitor) This blog will include the Design of my Idea. My Idea is described in the previous blog in this series My idea is to conduct a number of test to determine if the Ingress Properties R...
    • 24 Feb 2022
  • Blog#1 My Idea (Case Enclosure Reliability Monitor)

    Blog#1 My Idea (Case Enclosure Reliability Monitor)

    skruglewicz
    skruglewicz
    BLOG#1 - My Idea - Case Enclosure Reliability Monitor A project utilizing 2 Arduino MKR WAN 1300 & 2 Enclosure Cases supplied by Hammond Manufacturing   This is my introduction  blog post for this Design Challe...
    • 24 Feb 2022
  • Blog#3  Implementation (Case Enclosure Reliability Monitor)

    Blog#3 Implementation (Case Enclosure Reliability Monitor)

    skruglewicz
    skruglewicz
    BLOG#3 Implementation (Case Enclosure Reliability Monitor) This blog will include the implementation of the Basic Design described in the previous blog in this Series. This Basic Design will be used  as the framework implement&nb...
    • 24 Feb 2022
  • Blog#4  Testing Part 1 (Case Enclosure Reliability Monitor)

    Blog#4 Testing Part 1 (Case Enclosure Reliability Monitor)

    skruglewicz
    skruglewicz
    BLOG#4 Testing Part 1 (Case Enclosure Reliability Monitor) Test#2 -  Enclosure1554UGY Test Design This is my 1st Test design to test the reliability of the Hammond Enclosure 1554UGY The following components are being used::Arduino MKR...
    • 24 Feb 2022
  • [Pool Water Monitoring] #22 - Project Liftoff | Data collecting #1

    [Pool Water Monitoring] #22 - Project Liftoff | Data collecting #1

    feiticeir0
    feiticeir0
    Hi all ! Hope everyone is safe and well Since the past weekend, the project is live. First observations In this end, data collecting, I'm having troubles, in the sense that, a couple of AAA batteries only lasts almost a day. The code has some batter...
    • 23 Feb 2022
  • [Pool Water Monitoring] #23 - Project Liftoff | Data receiving

    feiticeir0
    feiticeir0
    Hi all ! Hope everyone is fine. Since last weekend, the project went live. I've already discussed - in part - the data collecting part. Receiving What I'm going now to describe is the other end, the receiving one. Here's the schematics, with the SD ...
    • 23 Feb 2022
  • Blog 3: Landslide monitoring for the Himalayan region - Wireless communication between two Arduinos using RF modules and remote event triggering

    rsjawale24
    rsjawale24
    Blog 3: Wireless Communication and Remote Event Triggering In the last blog, I interfaced the vibration sensor with Arduino to detect the landslides. This pretty much completes the sensing enclosure box, however, this vibration detected signal has t...
    • 23 Feb 2022
  • Blog 2: Landslide monitoring for the Himalayan region- The Sensor mechanism to detect landslides

    rsjawale24
    rsjawale24
    In the last blog, I gave a brief description of the project and the block diagram for the electronics. In this blog, I'll describe the mechanism to detect landslides and test the sensors. I'll be using a vibration sensor interfaced with an Arduino f...
    • 23 Feb 2022
  • Blog 10 - Part 2 - Software the things - draft

    Blog 10 - Part 2 - Software the things - draft

    christophesky
    christophesky
    Blog Content In this blog entry I will run through the software set up I have used on th instation end of my Just Encase design challenge for remote monitoring of my garden pond, I have split this into two main sections Hardware and Software setup. H...
    • 23 Feb 2022
  • Biofloc Monitoring System #5: Communication Between Two Arduino MKR WAN 1300

    taifur
    taifur
    Communication Using LoRa LoRaWAN is an exciting IoT technology that is expanding our communication capabilities. LoRaWAN allows devices to communicate over tens or even hundreds of kilometers (in extreme cases), all without a cell network or a high-p...
    • 23 Feb 2022
  • Biofloc Monitoring System #4: Testing the Sensors with Arduino

    taifur
    taifur
    In this blog, I will test all the sensors individually with the Arduino. Waterproof DS18B20 Digital temperature sensor testing This temperature sensor uses the Dallas 1-Wire protocol and gives up to 12 bits of precision from the onboar...
    • 23 Feb 2022
  • Orb-Weaver Rover - Blog #4 - Making the Rover!

    Orb-Weaver Rover - Blog #4 - Making the Rover!

    milosrasic98
    milosrasic98
    In this blog I cover how I designed and made a small 4 wheel rover using 3D printing and a few pieces of a PVC pipe!
    • 22 Feb 2022
  • Biofloc Monitoring System #3: Collecting the Sensors & other Components

    taifur
    taifur
    In my previous blog, I discussed the most important water parameters for a biofloc tank. I explained about temperature, pH level, ORP, and EC. In this blog, I will discuss the related sensors I am going to use for my project.  Temperature Senso...
    • 22 Feb 2022
  • Blog 11 - The launch! Floaty Mc Test Face (updated)

    Blog 11 - The launch! Floaty Mc Test Face (updated)

    christophesky
    christophesky
    The blog so far: Links should open new tabs / windows Sections 1-4. Initial thoughts, requirements,excitement and unboxing. Blog 1 - The what and why (Garden pond monitoring Background and Introductions) Blog 2 - My Method or WWHW (What, Why, How, W...
    • 21 Feb 2022
  • [Pool Water Monitoring] #21 - Project Liftoff

    feiticeir0
    feiticeir0
    Hi all ! Hope everyone is well and safe. It finally happen ! We just went live. This weekend was the time to finally put everything together and just turn it on. Data collecting One of the Arduinos MKR 1300 WAN is inside of one of Hammond's en...
    • 21 Feb 2022
  • Just Encase Solar Super Capacitor Weather Station - Outdoor Tests - Blog 7

    dougw
    dougw
    Wow, the solar super capacitor system works beyond expectations. Today is my first outdoor test of the system. It is an overcast winter day with an occasional appearance by the sun. You can see there isn't much shadow, indicating the sun is behind cl...
    • 20 Feb 2022
  • Addendum_BLOG_C_References_BLOG5

    skruglewicz
    skruglewicz
    Addendum Blog C REFERENCES (Case Enclosure Reliability Monitor) This blog is an Addendum for the link references in BLOG#5 Testing Part 2 Getting Started with the MKR Connector Carrier MKR Connector Carrier Basics | Arduino D...
    • 19 Feb 2022
  • Addendum_BLOG_B_References_BLOG3

    Addendum_BLOG_B_References_BLOG3

    skruglewicz
    skruglewicz
    Addendum Blog B REFERENCES (Case Enclosure Reliability Monitor) This blog is an Addendum for the link references in BLOG#3 - Implementation. Connect to Arduino Cloud from far away with LoRaWAN and The Things Stack The Things Stack (TTS) and...
    • 19 Feb 2022
  • Wind Turbine Health Monitoring || Hammond Enclosure Testing || Blog #5

    pratyush_cetb
    pratyush_cetb
    Wind Turbine Health Monitoring In this blog, we will put the enclosure through its paces and see how it holds up against different environmental conditions. The tests are performed on the sensor node enclosure 1554H2GYCL. The following are the series...
    • 19 Feb 2022
  • Wind Turbine Health Monitoring || Data Collection || Blog #4

    pratyush_cetb
    pratyush_cetb
    Data Collection Collecting vibration and wind data at varying wind speeds and rotor blade positions is a crucial step for accurately monitoring the health of the wind turbine. The goal here is to simulate some of the environmental conditions that an ...
    • 18 Feb 2022
  • Addendum BLOG A Testing

    Addendum BLOG A Testing

    skruglewicz
    skruglewicz
    ADDENDUM Blog for  BLOG#5 Testing Part 2 (Case Enclosure Reliability Monitor) Test#2 -  Enclosure 155H2GYCL Running the Test Design Inside the1554H2GYCL Enclosure Table of Contents PUTTING THE CASE THROUGH It's Paces. Ingress ...
    • 18 Feb 2022
  • Just Encase Solar Super Capacitor Weather - Indoor Tests - Blog 6

    dougw
    dougw
    I now have all sub-systems working so it is time to show the full system in action. I expanded the MSP430 firmware to deal with power management and Bluetooth communications and I wrote an android app to allow remote display of the weather station da...
    • 16 Feb 2022
  • Biofloc Monitoring System #2: Important Water Parameters of a Biofloc Tank

    taifur
    taifur
    Main water quality parameters in BFT Water quality maintenance and monitoring in any aquaculture are the essential practices aiming at the success of the growing cycles. Temperature, dissolved oxygen (DO), pH, salinity (EC), ORP, solids [total suspen...
    • 15 Feb 2022
<>