PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Art-a-Tronic Episode 2
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
  • Author Author: balearicdynamics
  • Date Created: 17 Mar 2019 11:57 AM Date Created
  • Views 3623 views
  • Likes 14 likes
  • Comments 17 comments
  • exhibition
  • depot09
  • cage
  • animatronic
  • mannequin
  • elegoo
  • pi-casso
  • gods
  • hackster.io
  • raspberry pi
  • cenciurio wines
  • lorenzo p merlo
  • technology in cage
  • challenge
  • art
  • digital painting
  • Making
  • pi face
  • ptron
  • mars 3d printer
  • hacking
  • neptune 3d printer
  • art-a-tronic
Related
Recommended

Art-a-Tronic Episode 2

balearicdynamics
balearicdynamics
17 Mar 2019

  • Introduction
  • Moving the Mannequin
    • Thinking on How to Move the Torso
    • The Most Affordable Solution
  • Previous Episodes
  • Next Episodes

Introduction

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have already received the notification from UPS that the challenge kit will arrive next Tuesday 19; in the meantime, the exhibition installation goes ahead. Lorenzo's operas will create a path for visitors. As there are many different points of view you can read Art-a-Tronic, as well there are different paths you can follow visiting the exhibition.

Moving the Mannequin

An almost complex part is adding the motion to the mannequin. The problem is that it has been designed and build more than half a century ago so integrating some sort of movement in it sounds very difficult. Unfortunately, the head is fixed; probably it is possible to cut the neck in the middle adding some rotation but I think that this will penalize too much the aesthetics so the head will remain fixed. There are five points that can be moved corresponding to the articulated parts of the mannequin: wrists, shoulders, and torso.

I have also considered that all the motion interventions will include some kind of alteration in the form of the joints but this can be easily masked properly dressing the parts.

There is also another important consideration; to control the motion I expect to interface a dedicated microcontroller able to manage the low-level motor motion part autonomously and in part receiving orders from the brain, the Raspberry PI 3B+

 

Thinking on How to Move the Torso

image

Torso - or, better, the upper part of the body - is fixed through an axle screwed on the upper plane of the legs (that can't move). The first ides was using a couple of motors pushing vertically from the torso with threaded bars but this implied a lot of mechanical problems, including fixing the motors on the upper part and the thread bars attach to the bottom parts.

image

Excluding the possibility to have the torso oscillating I decided for a single-motor solution acting as a linear transducer as shown in the stepper parts positioned approximately in their asset shown in the image below.

image

Using this Stepper motor just makes the body taller some cm so it is acceptable without losing the aesthetical body proportions.

The two images below show the legs upper surface by the plant. I will start from this point to design the parts that must fit inside this space.

imageimage

 

The Most Affordable Solution

Update

I have reviewed in detail the possible solutions to move the torso. The initial idea - very similar to those suggested by beacon_dave (Dave Ingels_ - sounds attracting but reviewing in depth how the two parts mannequin is joined arise a lot of difficulties, with the risk to be not feasible in a good way. The images below show how the central joint is an essential part of the entire torso support and can't be avoided. the lock nut is part of the system keeping together the two legs, as a matter of fact, the bottom half of the body.

imageimageimage

Changing this part means to replace is rebuilding one in a different way and in my opinion it is not the worth as the same result can be reached in an easiest way, apparently more complex but that requires definitely less extra 3D printed parts.

image

As shown in the above image, the shaft is not just a bar but includes a turnable spring to keep the torso in the desired orientation. This sounds good to fine-tune the upper part when there is the motor with the linear transducer. Following this proof of concept I have drafted a quoted sketch to fix the ideas before proceeding to model the parts that should be 3D printed.

image

I should make only two parts for the bottom: the stepper support that should be fixed to the plane and the back side support. To make it working without attrite, I will use a free fall bearing, part of the same 3D printing. Note that in the sketch I have designed only the bottom guide for the back of the torso but in reality, there is a counterpart that will be fixed to the bottom of the torso; both together will be thick like the motor. The threaded bar is oriented horizontally to the longitudinal (the longest side) of the torso in correspondence to the mannequin belly to be completely hidden.

 

So, don't lose the next episode.

 

Previous Episodes

  • Art-a-Tronic Episode 1

 

Next Episodes

  • Art-a-Tronic Episode 3
  • Art-a-Tronic Episode 4
  • Art-a-Tronic Episode 5
  • Art-a-Tronic Episode 6
  • Art-a-Tronic Episode 7
  • Art-a-Tronic Episode 8
  • Art-a-Tronic Episode 9
  • Art-a-Tronic Episode 10
  • Art-a-Tronic Episode 11
  • Art-a-Tronic Episode 12
  • Art-a-Tronic Episode 13
  • Art-a-Tronic Episode 14
  • Art-a-Tronic Episode 15
  • Art-a-Tronic Episode 16
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago +7
    A small slewing ring bearing with gear teeth might be worth considering ? https://en.wikipedia.org/wiki/Slewing_bearing Insert the motor vertically into that existing hole with a pinion on the end of its…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave +7
    Hello Dave, thank you for the suggestion. The idea just as you mention, unfortunately, is not reliable. The torso should have a larger base to rotate( not so many degrees) But in theory - I have already…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave +6
    Hello Dave (bis) I have reviewed again your idea. Take a look to the video below, I have already applied it in the past to make the camera pan prototype: www.youtube.com/watch I worked fine in this case…
Parents
  • beacon_dave
    beacon_dave over 7 years ago

    A small slewing ring bearing with gear teeth might be worth considering ?

    https://en.wikipedia.org/wiki/Slewing_bearing 

    Insert the motor vertically into that existing hole with a pinion on the end of its shaft to engage with the slew ring gear teeth.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 7 years ago

    A small slewing ring bearing with gear teeth might be worth considering ?

    https://en.wikipedia.org/wiki/Slewing_bearing 

    Insert the motor vertically into that existing hole with a pinion on the end of its shaft to engage with the slew ring gear teeth.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave

    Hello Dave,

     

    thank you for the suggestion. The idea just as you mention, unfortunately, is not reliable. The torso should have a larger base to rotate( not so many degrees) But in theory - I have already done one in past for another project - it is possible to make a 3D printed custom one (a sort of half circle on the opposite side of the motor) then use iron spheres; as a matter of fact I mean making a custom bearing, just for the special shape. I found the spheres, that are perfect on amazon but the expected delivery is next April 4, too late. So, for now, I am designing a mechanism where the semi=circular path on the bottom side (the legs) hosts a rail and the top side has a set of three bearings. Then if I receive the spheres in time I will change the two pieces design, but this solution - considering that I have all the components at home - should work. Not perfect by a mechanical point of view but will work.

     

    I hope I have understood what you were pointing on.

     

    Enrico

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave

    Hello Dave image (bis)

     

    I have reviewed again your idea. Take a look to the video below, I have already applied it in the past to make the camera pan prototype:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    I worked fine in this case but with the mannequin, there are some limitations to this kind of application:

    1. The shaft of the torso is not fixed but should be able to oscillate. I will keep it fixed but the base (legs) structure has a too big diameter with a big nut included in the legs base.  I have considered this method but until now I didn't saw a solution as the shaft will be too weak if the peripheral edge of the body does not stay on the base. I can use the double gear method - that remains my preferred as well, also because of the hole you saw making easy to fit the motor vertically.
    2. In the case of the video above, the gear is rotating based on the bottom while in this case the only possible solution I see is putting the gear on the torso, corresponding the motor gear to the bottom.
    3. I need to find a way to replace the actual legs-torso shaft with a different system. That is the most challenging problem I see until now.
    4. The torso edge should work with a 3D printed bearing but as I mentioned before, the balls will only arrive on April, 5.

    What is the conclusion? At the moment there is no conclusion, I will check if I can replace the shaft, make a design and see if 3D printing the gear motion will be possible. And probably trying also the alternative way of the threaded bar that increases the space between torso and legs part but as it is the less invasive maybe the worth to try it.

     

    Enrico

    • Cancel
    • Vote Up +6 Vote Down