PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Art-a-Tronic Episode 3
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
  • Author Author: balearicdynamics
  • Date Created: 22 Mar 2019 2:24 AM Date Created
  • Views 2364 views
  • Likes 12 likes
  • Comments 8 comments
  • exhibition
  • animatronic
  • elegoo
  • 3D Printing
  • stepper motor
  • teeth belt
  • nema17
  • raspberry pi
  • manequin
  • challenge
  • art
  • Making
  • hacking
  • art-a-tronic
Related
Recommended

Art-a-Tronic Episode 3

balearicdynamics
balearicdynamics
22 Mar 2019

  • Introduction
  • Moving the Torso: the Stepper Motor
  • Previous Episodes
  • Next Episodes

Introduction

image

After a series of positive comments and very good suggestions by shabaz  beacon_dave  and mcb1 it's time to go ahead another step. I mentioned the users whose comments helped me to address what in my opinion seems the best solution to proceed. What I consider important in this process is the fact the constructive critics focus the attention on possible alternative solutions as well as are helpful in identifying possible mistakes in the project. Despite I have an almost clear idea of what I aim to reach as the final result, every step reveals how changes and corrections are needed. What I am sure at this point is that the final result will be adapted in a different way than what I have supposed when I started the design.

 

Moving the Torso: the Stepper Motor

After thinking and simulating the possible solutions the most reliable seems a teeth belt rotating a pulley (only of some degrees) driven by a stepper motor to grant the needed precision but also to have the required torque. By the way, I hope that with a 140 mm diameter pulley the Nema17 stepper motor can move the upper part of the mannequin without problems.

image

The sketch in the image above is the first design on how to position the stepper motor to control the rotation. The main advantage of this solution is that the space between the dorso top-side and the top plane of the legs is the most reduced possibly. The thickest part is the motor that results submerged inside of the right leg. A small further change has been applied designing the 3D printable object with Fusion360.

The rendering below shows the support from the bottom side. I have added a small contour where the stepper motor can fit; this means that the only visible part of the motor is the shaft with the teeth pulley and 3 mm thick of the upper part of the motor support.

image

imageimage

imageimage

imageimage

After 3D printing, I found the farthest point where the support can fit leaving as much space as possible to the center area as the rotating platform should be as large as possible. Then, I have cut the hole and prepared the support to be kept in place.

imageimage

The motor has been screwed to the support with foud Allen screws, accordingly with the measures shown in the Nema17 data sheet. The image below shows the motor in position ready to be connected to be connected to the rotating platform.

image

Don't miss the making of the rotating platform in the next episode.

 

Previous Episodes

  • Art-a-Tronic Episode 1
  • Art-a-Tronic Episode 2

Next Episodes

  • Art-a-Tronic Episode 4
  • Art-a-Tronic Episode 5
  • Art-a-Tronic Episode 6
  • Art-a-Tronic Episode 7
  • Art-a-Tronic Episode 8
  • Art-a-Tronic Episode 9
  • Art-a-Tronic Episode 10
  • Art-a-Tronic Episode 11
  • Art-a-Tronic Episode 12
  • Art-a-Tronic Episode 13
  • Art-a-Tronic Episode 14
  • Art-a-Tronic Episode 15
  • Art-a-Tronic Episode 16
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago in reply to balearicdynamics +5
    Enrico, When you don't know how to do something then it is always impressive to see someone else doing it. I'm not a mechanical engineer and still struggle to get physical things to move and connect in…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie +5
    Dubbie, I see. But I am not a mechanical engineer too. As I am NOT an engineer at all, as well as a software developer (it's a fact). The point is that when you want to do something, you should move on…
  • dubbie
    dubbie over 7 years ago +4
    Impressive building. Dubbie
Parents
  • genebren
    genebren over 7 years ago

    Enrico,

     

    Coming along nicely! I hope that this design will give the range of motion that you are looking for.  Keep up the good work.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Enrico,

     

    Coming along nicely! I hope that this design will give the range of motion that you are looking for.  Keep up the good work.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to genebren

    Thank you Gene! We'll see in a very few time. I m finishing this part.

     

    Enrico