PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Art-a-Tronic Episode 8
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
  • Author Author: balearicdynamics
  • Date Created: 8 Apr 2019 4:34 PM Date Created
  • Views 2442 views
  • Likes 10 likes
  • Comments 10 comments
  • exhibition
  • sensors
  • animatronic
  • wiring
  • elegoo
  • 3D Printing
  • motion
  • raspberry pi
  • raspberry pi 3b+
  • challenge
  • pi camera
  • art
  • Making
  • arduino
  • brain
  • art-a-tronic
  • interaction
Related
Recommended

Art-a-Tronic Episode 8

balearicdynamics
balearicdynamics
8 Apr 2019

  • Introduction
  • Fitting the Brain in Place
    • Designing the Rail Support
    • Assembling the Brain
    • What is the White Band Glued to the Neck?
  • The New Eye Implant
  • Previous Episodes
  • Next Episodes

Introduction

image

The last assembly effort was finding a way to fit the Raspberry and the PI camera together with the "ears" inside the reduced space of the head. Then, I can finally close and dress 7 of 9. In this episode, I will show how I have completed this last task before moving to the software configuration and programming the boards.

The image below shows how I cut the head to save the front-view of the face, with the best possible access to the interior of the head.

imageimage

But before digging in the technical details of how I assembled the head, let me spend some word on how I decided to dress 7 of 9. As the original body characteristics, I searched for some stylish dressing accordingly with the age of the mannequin; I have found a vintage dressing store offering an incredible choice of any kind of clothes original from the period so I opted for something themed with the colors and style of the Art-a-Tronic exhibition that in my opinion gives the right emphasis to the character. As shown in the image below – the first dressing test as I was back from the shop – both clothes and shoes are original from the end of 1960 and the first years of the '70s.

image

Fitting the Brain in Place

The Raspberry PI 3B+, the "brain" of 7 of 9, should be installed inside of the head near to the left eye where the implant hosts the PI Camera. Finding a solution to assemble the interior of the head in a so reduced space I experienced how incredible engineering designs should be the implants of the Borg technology!

The connectors on the Raspberry Pl are distributed along three sides, respectively:

 

  • USB Ports to the front shorter side
  • Power connector to the left side
  • PiFace Digital 2 relay connectors to the back side

 

Designing the Rail Support

As the Raspberry PI can reach a reasonable temperature (average 40C when working), I considered avoiding to fit the board glued or wired somewhere to the internal sides of the face.

The best solution I found is to keep the Raspberry hanging in the center of the head.

For this task, I have designed and 3D printed a support to screw the Pl on two rails centered to the head internal space. Thank this solution it was sufficient using only two couple of Allen screws to keep the rail in the mid of the head meanwhile the PI has a good air circulation without the need of a fan.

image

Above: the Fusion360 rendering of the support rail to keep the Raspberry PI in the center of the head.

image

Above and below; The 3D printed rail support with the Raspberry PI screwed on it. The form factor of the support makes possible to position the PI at the best height and is easy to move it for maintenance and update, plugging the connectors, etc.

imageimage

Assembling the Brain

The images below show the sequence of positioning of the Raspberry PI fixed to the support, inside the brain.

image

imageimage

What is the White Band Glued to the Neck?

To see is more in detail, take a look at the images below:

imageimage

It is the cut part of the head support. I have drafted the profile of the cut part; then, from the draft, I have extruded it 3 mm thick and 3D printed. Using 20% only of fill percentage the 3 cm height band is almost flexible to perfectly adapt to the internal profile of the neck where it has been hot-glued. To make it easily removable I have hot-glued only in three points the removed part of the head and - at least this is the plan - the top side will be kept firmly with an original headband.

imageimage

The New Eye Implant

As discussed in Episode 6 with dubbie the original implant is not definitely viable, so I reduced the design by 75% and removed the NeoPixel ring leaving only the PI camera.

image

image

As you can see in the two above images, in my opinion, the effect is definitely better with good proportions and letting the camera circuit exposed contribute to accentuate the android effect.

Previous Episodes

  • Art-a-Tronic Episode 1
  • Art-a-Tronic Episode 2
  • Art-a-Tronic Episode 3
  • Art-a-Tronic Episode 4
  • Art-a-Tronic Episode 5
  • Art-a-Tronic Episode 6
  • Art-a-Tronic Episode 7

Next Episodes

  • Art-a-Tronic Episode 9
  • Art-a-Tronic Episode 10
  • Art-a-Tronic Episode 11
  • Art-a-Tronic Episode 12
  • Art-a-Tronic Episode 13
  • Art-a-Tronic Episode 14
  • Art-a-Tronic Episode 15
  • Art-a-Tronic Episode 16
  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +4
    I like the eye fix, though you might want to add a filter over the camera to disguise the camera a little. DAB
  • shabaz
    shabaz over 7 years ago +4
    Hi Enrico, Great work! Regarding eye, although I think this suggestion is not necessary at all, since the eye already looks impressive, here is an idea, that worked ok-ish for me, without needing much…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz +4
    Hello Shabaz! thank you for the suggestion. It is useful, really. I was thinking of something similar but the idea was using (should make some experiment) 3D printer transparent resing and 3.5mm blue LEDs…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Enrico,

     

    Great work!

    Regarding eye, although I think this suggestion is not necessary at all, since the eye already looks impressive, here is an idea, that worked ok-ish for me, without needing much space like the neopixel rings:

    Basically, it is a single LED (red in my case) and a ring made of plastic. They are just epoxied together (I sanded the LED end flat first, to diffuse light a bit) and then just wired it directly to an I/O pin on the pi, via a small resistor:

    image

    image

    You can see it wasn't perfectly illuminated, since it appears overblown at the bottom, so the light was not totally even.

    Anyway I think your mannequin's eye looks fantastic already.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Hello Shabaz!

     

    thank you for the suggestion. It is useful, really. I was thinking of something similar but the idea was using (should make some experiment) 3D printer transparent resing and 3.5mm blue LEDs. This will create (maybe four) thin tubes from the eyes to the near straining where the led lies inside. To manage some complex pattern, I discovered that I already have the solution! I bet you remember what...

     

    Cheers. Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Hello Shabaz!

     

    thank you for the suggestion. It is useful, really. I was thinking of something similar but the idea was using (should make some experiment) 3D printer transparent resing and 3.5mm blue LEDs. This will create (maybe four) thin tubes from the eyes to the near straining where the led lies inside. To manage some complex pattern, I discovered that I already have the solution! I bet you remember what...

     

    Cheers. Enrico

    • Cancel
    • Vote Up +4 Vote Down