• Safe and Sound - Invisible Hazardous Environmental Factors Monitoring System Conclusions - blog 23

    Doug Wong Back to Doug Wong's VCP Profile | Safe and Sound Observations & Surprises This project has been a very interesting journey researching a wide variety of invisible potential hazards, designing systems to measure invisible hazards…
  • Safe and Sound - Ultraviolet Light Tests - blog 22

    I have been waiting for a week to do some ultraviolet light tests - the sun just never seems to shine when I need it. I calibrated the UV sensor output to match the UV Index and wanted to test it in real sunlight. The UV Index was developed in Canada…
  • Safe and Sound - Gas Sensor Demo - blog 21

    It has been a very hectic week including a softball tournament on the weekend, but I did manage to squeeze in some work on calibrating my gas sensor module which is based on the TI MSP EXP432P401R launchpad. The 18 turn offset and gain pots on my custom…
  • Safe and Sound - Invisible Hazards Project Spin-offs - blog 20

    This week I've been sidetracked on a bit of a tangent to my build project. I was asked to make a presentation on invisible hazardous environmental factors. All I can say is the grapevine works in mysterious ways. Anyway I put together a 1 hour multi media…
  • Safe and Sound - Cell Phone Shield Test - blog 19

    The deadline for this challenge has been extended again, so I can squeeze in a few more blogs. Perhaps some real applications of all this instrumentation I have put together. This blog shows some quick tests I did to see if shielding makes a difference…
  • Safe and Sound - Invisible Hazardous Environmental Factors Monitoring System - blog 18

    This design challenge is nearing its final deadline so the pressure as been building to complete the project. I finally finished building all the hardware and all the hardware is working well. The past week has seen a lot of 3D design work and 3D printing…
  • Safe and Sound - Hazardous Factors Monitoring System - Gas Sensors Module - blog 17

    This update documents progress on power up of the custom gas and UV sensor module. I did run into a few snags getting the card to work, or rather getting the software to work. The hardware on the card is designed properly, but it has just been too long…
  • Safe and Sound - Environmental Factors - GAS Sensors - blog 16

    I have been under the weather this week, which is unusual for me. It is just so much fun trying to build electronics when you are feverish, nauseous, dizzy and coughing up a lung. None-the-less, the show must go on. The first thing I need to mention is…
  • Safe and Sound - Environmental Factors - Microwaves - blog 15

    This is the last of the hazardous environmental factors research blogs for this project, subsequent blogs in this challenge will deal with hardware builds, software programs, functional tests and test results. Microwaves are used for cell phones, Wi-Fi…
  • Safe and Sound - Environmental Factors - Wearables - blog 14

    I have been in Washington making a technical presentation in an unbelievably secure building, but now I'm back and it is time to catch up. I am still waiting for some parts for my sensor card – it is starting to look like I will have to kludge some connectors…
  • Safe and Sound - Hazardous Factors MQTT Subscriber & Publisher - blog 12

    I managed to purchase a second WiFi booster pack although the TI discount voucher I won here was not accepted This booster pack has allowed me to assemble a second system consisting of a MSP-EXP432P401R MSP-EXP432P401R a CC3100ModBoost and a 430BOOST…
  • Safe and Sound - Hazardous Environmental Factors - ELF - blog 11

    Extremely Low Frequency Electromagnetic Radiation - (ELF) I am going to arbitrarily split this large topic into just the 2 ranges of electromagnetic fields which are of most interest to me: 0 to 300 Hz and microwaves from 2 to 3 GHz. Is electromagnetic…
  • Safe and Sound - Hazardous Factors Sensor PCB - blog 10

    This blog shows the Booster Pack PCB I designed to accommodate 5 sensors. After viewing the video - I think it might have been cool to order a red card instead of green. The card was ordered from SeeedStudio and took exactly 7 days from time of order…
  • Safe and Sound - Hazardous Factors MQTT Broker - blog 9

    I have been in the throws of struggling with software and numerous other priority interrupts. Still ordering more parts and some have come in, but they will have to wait for another blog. I just have to get something posted even though it is not as complete…
  • Safe and Sound - MSP-EXP432P401 & Sharp LCD - blog 8

    This update covers my first attempt to fire up the MSP-EXP432P401R MSP-EXP432P401R I am using Energia at this point since they claim to support this platform and the Sharp display. I modified the 430BOOST-SHARP96 430BOOST-SHARP96 to be always enabled…
  • Safe and Sound - Invisible Hazards System - Kit Unboxing - blog 7

    I received a box from element14 today - so here is the unboxing video....lots of great modules..... You don't have permission to edit metadata of this video. …
  • Safe and Sound - Hazardous Factor - Radon - blog 6

    The next topic in this series on invisible hazardous substances is radioactive materials. We don't usually think of ourselves as being in danger from radioactive particle radiation, but we are all exposed to radon every day. What is Radon, why is Radon…
  • Safe and Sound - Hazardous Gasses PCB - blog 5

    This blog details the circuitry and PCB layout of my custom Booster Pack to monitor 8 hazardous gasses and ultraviolet light. I added some active circuitry to filter the CO 2 sensor PWM output since my last blog. This is a 4-pole low-pass Butterworth…
  • Safe and Sound - Hazardous Factor - Air Quality - blog 4

    This blog discusses air quality and how it can be monitored, especially odorless and colorless gasses like carbon monoxide and carbon dioxide. Air Quality The list of common items that off-gas nasty chemicals into the air is depressingly long and insidiously…
  • Safe and Sound - Hazardous Factor - UV Light - blog 3

    Hazardous environmental factors are really not anyone's idea of a fun topic, so I want to keep all the gory depressing medical details to a minimum and focus more on the technical challenges of monitoring and measuring these invisible quantities. There…
  • Safe and Sound - Hazardous Factors System - Development Plan - blog 2

    This second blog in the Hazardous Environmental Factors project publishes a bit more of the project plan and the proposed instrumentation system. The the issues addressed will be expanded upon in future blogs. The Project Plan Research - The first step…