Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Hacking/Rebuilding a MegaMax Device Programmer

    phoenixcomm
    phoenixcomm
    Hacking/Rebuilding a MegaMax Programmer I have one of these programmers. I always thought that I could get it to work, but nothing, it's not supported, and nobody would fess up, the goods.. That's how I ended up here. The goal is to u...
    • 29 May 2026
  • Standardizing Network Connections

    phoenixcomm
    phoenixcomm
    Standardizing CanAerospace Network Connections - My Way Ok, I have been using a pair of RJ-45 jacks. This was my  Blond Moment! This was not a really good idea. Ok, back to the spec. So here is what I ended up with: CanAerospac...
    • 16 May 2026
  • Flight Simulator 101 or back to college - part 15: Radio Propagation and Slant Range Math. part 3 - The Software

    phoenixcomm
    phoenixcomm
    Ok, so after slogging through the math, and going to a local college to get my head straight, and to get some help, here finally I can see some light at the end of the road. So now I have to lay out the software, for you, and myself. So I drew a litt...
    • 25 Apr 2026
  • How To: use a old PS/2 Keyboard encoder

    phoenixcomm
    phoenixcomm
    Well, this is going to be fun. What I'm about to do is to figure out what combination of pins gives us what letter. Please see my other blog: How to use a PS/2 Keyboard Encoder with interrupts.  The object is the connector at the bottom of t...
    • 25 Apr 2026
  • NexGen: CDU Pinlite Displays: Really the Final Word !! -- DEPRECATED

    phoenixcomm
    phoenixcomm
    I took a long look at the mess that I created. And I said to myself: There has to be a better way!! A few PROMS or EPROMS would be supper, but alas I don't have a programmer anymore.  It looks like I will need a bunch of TI's P...
    • 25 Apr 2026
  • New Plan For the Display!!

    phoenixcomm
    phoenixcomm
    THIS BLOG HAS BEEN DEPRECATED OK I have done some double triple checking in the doc TM 11-5841-281-12 and it seams that the three displays are independent. Refresh is now almost cake! I will still directly drive the sixteen segment display...
    • 25 Apr 2026
  • CP-1252/ASN-128 Display Interface a Final Look FINAL I hope

    phoenixcomm
    phoenixcomm
    This is a a massive update, hold on to your hats here we go! The system consists of 3 components The Nav box itself An Interface box where the Displays and Switches are connected An LRU/FRU (Line or Field Repairable Unit Communications is over a C...
    • 23 Apr 2026
  • Where are we now? New Years Day 2025

    phoenixcomm
    phoenixcomm
    As I have said before most of the simulator will be, or is written in Java EE. The question was asked why Java simple answer. Java has a much nicer easier when something happens in Software or in hardware! C / C++ Java  PEARL Program...
    • 3 Sep 2025
  • The Lab: As The World Tuns

    phoenixcomm
    phoenixcomm
    As The World Turns, Things still don't stand well. I had a forward-facing server with a public IP, for well over more than a few decades. About 2 weeks ago. I got nailed, So I had to put the server on an Internal class C address (192.168.xx.xx). I wa...
    • 13 Apr 2025
  • NexGen Blog Index VIII

    phoenixcomm
    phoenixcomm
    Nexgen Blog Index Viii 2025 1    Shift It! Challenge Start Delay 2   Design of the project: overview:
    • 5 Mar 2025
  • Documents: Synchro and Resolver Handbook and Guide

    phoenixcomm
    phoenixcomm
    If you work with robotics, avionics, an other fields that use angles you might just run into one or more these things. They are motor like devices that can transmit, or receive angles called Synchros in older aircraft they are used in pairs, a transm...
    • 17 Feb 2025
  • NexGen: The Lab: What to do with a Cuisinart 12 cup plus. use it to control a DIY Sand Blaster.

    phoenixcomm
    phoenixcomm
    I have a real problem with what to do with my Cuisinart 12 Plus that has no heat but the clock works. Rip the guts out and use it to control a DIY Sand Blaster, of course!  The cabinet will be made of 1/2" plywood painted gloss white inside...
    • 31 Jan 2025
  • Why does it matter?!

    phoenixcomm
    phoenixcomm
    Most of my work is in aviation and avionics where wifi is plage along with 'on the go' usb ports on routers so almost 99% is WIRED, and wifi turned off! This type of paranoia extends in my SmartHab project. We don't want my house security...
    • 30 Jan 2025
  • New Plan for ASN-128 Navigation Display Subsystem

    phoenixcomm
    phoenixcomm
    Ok I have done some double triple checking in the doc TM 11-5841-281-12 and it seams that the three displays are interdependent. Refresh is now almost cake! Well while writing this I realized that I the selected display character needs a LAMP TEST, a...
    • 27 Jan 2025
  • Wamco Pinlite Catalog.

    phoenixcomm
    phoenixcomm
    Here is a copy of the WAMCO Pinlite catalog.-enjoy community.element14.com/.../WAMCO_2D00_DisplayCatalog.pdf
    • 25 Jan 2025
  • Resurrection of sorts Jan 2025

    phoenixcomm
    phoenixcomm
    Ok, here we go again. This is a fresh (not quite) start Jan 2025 I have lost all of my work on the sim! So here we go one more time. Here is what I am up against. There are 4 Alphanumeric 16 digit displays these can be driven by 4 x MCP23S17 and som...
    • 21 Jan 2025
  • How Not to Catch the Worm or Viruses!

    phoenixcomm
    phoenixcomm
    A computer worm is a standalone malware computer program that replicates itself in order to spread to other computers.[1] It often uses a computer network to spread itself, relying on security failures on the t...
    • 20 Jan 2025
  • A Tale of Caution, and Misery; Staring ASUS Advanced Replacement

    phoenixcomm
    phoenixcomm
    I bought this Asus Motherboard not quite 3 years ago! When I got it home and tried to mount the cooler and fan assembly, it would not mount as the caps near the rear where too tall and interfered with the fan/cooler assembly. So back to Micro Center ...
    • 29 Dec 2024
  • New Tool Day: Kline MM720

    phoenixcomm
    phoenixcomm
    Well will wonders never cease! My bother sent me a nice Hanukkah Gift! The little guy knocked it out of the park, he knows I mess around with electrical stuff, computers, and even a MGB or a Jag!! Nowadays its just a Mazda 3 GT (2015), which has been...
    • 28 Dec 2024
  • NexGen Blog Index i

    phoenixcomm
    phoenixcomm
    NexGen Blog Index I   Alphabetic Index Component Documentation ATR Boxes Back to College: Simulator 101 CANaerospace, Adventures in RFQ       RSS: Intercommunication: Canbus Part 1    Intro to CANaerospace P...
    • 27 Dec 2024
  • NexGen: Component Documentation: Indicator, Stall Margin

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Indicator, Stall Margin Manufacture Conrac Instrument Div Part Number 30498047 Connector: 85102E145P50 pin A pin B pin C pin D pin E pin F pin G pin H pin K pin J ...
    • 8 Aug 2024
  • New Tool Day Allen Wrenches Galore!

    phoenixcomm
    phoenixcomm
    Well, here we are again more tools. I never can find the right Allen Wrench, well never again!! I just picked up the Bondhus 69600 ball end color set for metric, and US. I also uncovered in my garage my Xcelite 99PS-40 in the case! At least now I kno...
    • 7 Aug 2024
  • New Tool Day: Kett Power Shear

    phoenixcomm
    phoenixcomm
    Oh well, this orb keeps spinning and throws stuff at you some good, some well maybe not so good. I made a detour to the 25 cents shop to see if they had gotten in some more   sockets. BTW they are only $5.00 each. that's about 75% off the t...
    • 27 Jul 2024
  • Hacking the Alfie Voice Controlled Intelligent Shopper

    phoenixcomm
    phoenixcomm
    As this is my first foray into this sort of thing please bear with me. I picked up a brand new Alfie Voice Controlled Intelligent Shopper. I noticed the USB jack which they used for charging but I wondered if it could be see by my desktop. So I plug...
    • 4 Jul 2024
  • NexGen Blog Post Index VI

    phoenixcomm
    phoenixcomm
    Monthly Projects IV: 2024 Monthly Projects II: 2020 - 2024 1/25/20/20 Acoustics Competition Sep 21, 2020 Sensors Competition: Design, Control System 1/25/2020 Nexgen: FAA Nav Aid Station Morse Code Id Sep 25, 2020 Smarthab smart thermostat ...
    • 4 Jun 2024
>