Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • NexGen: Component Documentation: Antenna Controller

    phoenixcomm
    phoenixcomm
    Component Documentation Hughes Aircraft - Antenna Controller. Part Number: 435-19-2001-1 5200-215985 NSN 5985-00-090-0474 AF-33  600 2347 ser 1445 Manufacture(s) Hughes Aircraft Co. Raytheon Company NOTES: MAXIMUM VOLTAGE R...
    • 17 Apr 2023
  • Flight Simulator 101 or back to college - part 14: Programming Arduino like an adult! Kill the loop()!

    phoenixcomm
    phoenixcomm
    Why did I say "Programming Arduino like an adult! Kill the loop()!"?  First, we need to know where this construct came from. A sketch is a variant of the C++ programming language. Hell, wait doesn't C++ have a main() function? Yep, it surel...
    • 9 Apr 2023
  • NexGen: Hacking: Loadmeter, Dual, Weston 248697

    phoenixcomm
    phoenixcomm
    The Analysis: The Loadmeter is divided into 3 parts. Parts 1 and 2 are identical and are the meters. Part 3 is the lighting equipment. Let's talk about the meter for a minute.  The meter is most likely a D'Arsonval movement. . It...
    • 21 Mar 2023
  • NexGen: MPCD (F/A-18C/D MPCD): Hardware / Software Interface III

    phoenixcomm
    phoenixcomm
    Ok, So I have talked about the MPCD's Bezel more than one or two times. So why don't we start in, again in part II, I used an MCP2515 I/O expander to handle my Bezel Switches, which will stay at is,  but instead of using CANaerospa...
    • 20 Mar 2023
  • Nexgen: Dual Protocol Converter: Ethernet - 4

    phoenixcomm
    phoenixcomm
    Well here were are in part 4 of building my dual protocol converter from 2 Raspberry Pi Model 1  this will fit into one of my plastic ATR (shoe) boxes. To power the pi(s), I'm duplicating the USB power circuit with two outputs. The powe...
    • 4 Mar 2023
  • Nexgen: Dual Protocol Converter: Ethernet <> CANaerospace - 2

    phoenixcomm
    phoenixcomm
    Well,  I think it is about time to reveal the design for my dual-channel protocol converter.  This will take one of my plastic ATR boxes. This design takes two (2) Rasberry Pi(s) and two (2) SPI to CAN bus modules, and lastly one dual RJ45 ...
    • 26 Feb 2023
  • Tech Tip X: One of the best storage boxes, that I have seen.

    phoenixcomm
    phoenixcomm
    You know parts boxes are ubiquitous! If it has a top, well it is blow molded and opaque which means you can't see the stuff in the box, or you cant store odd stuff, just maybe a 3x3 cube thing like the SplashNcolor Milwaukee Packout which is ver...
    • 5 Feb 2023
  • TECHNICAL MANUAL AVIATION UNIT AND INTERMEDIATE TROUBLESHOOTING MANUAL FOR ARMY MODEL AH-64A helicopter (NSN 1520-01-106-9519) (EIC: RHA) WIRING DIAGRAMS

    phoenixcomm
    phoenixcomm
    You might not need this publication, but if you mess around with connectors like I do this publication will be invaluable to you. Thankfully I had this when I lost a lot of my docs when my hard drive crapped out. Its number is TM 1-1520-238-T-10.&nbs...
    • 4 Feb 2023
  • NexGen: Fuel Load Meter: Revised Plan of attack-UPDATE

    phoenixcomm
    phoenixcomm
    Blond Moment Ok, Boy Blond Moment Strikes Again: if you remember I used a CANbus Module hooked up via an I2C bus. But Wait nope it's the SPI bus.  And the 2 switches in my diagram showed them hooked up to Digital Pins directly, even though ...
    • 1 Jan 2023
  • NexGen: Fuel Load Meter: Revised Plan of attack

    phoenixcomm
    phoenixcomm
    Flash, Food For Thought: Ok, I have a Smart Display, driven by an MCP23017 16-bit I2C which requires a lot of glue, (quick count) 8 data lines, 5 address lines, and 8 control lines. If you count this on your fingers 8+5=13+8=21. Ouch. Oh yes and the ...
    • 22 Dec 2022
  • NexGen: Main Blog Index

    phoenixcomm
    phoenixcomm
    Main Index for NexGen's Blog. ATR Boxes Back to College: Simulator 101 CANaerospace, Adventures in Dream Boards Documents (Not NexGen) Hacking Other Things: Howto: Lab, TheLearning Center, The New Year: 2024 Polls, My Preface Random Things: Res...
    • 12 Dec 2022
  • NexGen: The Lab: Harbor Freight Cross Slide Vice

    phoenixcomm
    phoenixcomm
    Last month I picked up this beast at a garage sale for less than 20 bucks, it is missing one of the handles which I will have to replace. In the condition that it is somewhat less than 5 out of 10. Big wish. I wonder how I can change the stupid cheap...
    • 10 Dec 2022
  • Flight Simulator 101 or back to college - part 13: Two pi or not

    phoenixcomm
    phoenixcomm
    Flight Simulator 101 or back to college - part 13: Two Pi or not If you look in the Wiki and look for pi or π you get this,  where C/d is constant, regardless of a circle's size. π and it is an irrational number and a transcendental number...
    • 8 Dec 2022
  • NexGen: Component Documentation: Vertical Situation Indicator

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Vertical Situation Indicator Type: 329B-8U Manufacturer:  Collins Radio Type  329B-8U1 Part Number  787-6766-001 Power  115vac 400hz 26w 5v AC or DC Connector J1  771806 Mat...
    • 1 Dec 2022
  • NexGen: Component Documentation: Annunciator, SELCAL, Custom

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Annunciator, SELCAL, Custom SELCAL is a signaling method that can alert an individual aircraft that a ground station wishes to communicate with it even if the radios are muted. SELCAL signals can be transmitted over e...
    • 29 Nov 2022
  • NexGen: Component Documentation: Horizontal Situation Indicator

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Vertical Situation Indicator NexGen: Component Documentation: Horizontal Situation Indicator Type: 331A-7RA Manufacturer:  Collins Radio Type  331A-7RA Part Number  522-3138-004 Carr...
    • 29 Nov 2022
  • NexGen: Component Documentation: King Radio: ADF Panel

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Indicator, DME KI266 Manufacture King Radio Model Number KI266 Part Number 066-3047-00 Gorn Electronics  GM-14M Mate: Winchester MRA 14N7 "Gas-discharge displays are used to digitally display ran...
    • 23 Nov 2022
  • Where are we now, November 2022

    phoenixcomm
    phoenixcomm
    Ok, there has been a lot of movement in my design or should I say architecture? We have moved from my hatred of USBs where things never come up on the same address twice. A prime example is the Arduino IDEs virtual serial port. Oh, well I'm digressin...
    • 18 Nov 2022
  • NexGen: Hacking; Gray 2 BCD Encoder (using TTL)

    phoenixcomm
    phoenixcomm
    OK, I Have had it up to you know where with the GRAY CODE!! When I have written this decoder in software, it takes a loop or two, It just eats CPU time. This is ok if you can use interrupts. But the Ardunio does not return the interrupt value to you ...
    • 2 Nov 2022
  • NexGen: Component Documentation: Mode Selector

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Mode Selector Manufacture: PN A.R.C. 47968-0001EA.D.I. 84-101-1 Lamps: A247 Instrument Mount Lamp / Module: 4 Lamp Voltage Switches: On Bottom, Middle rows, and top left only Switch Arrangement: C...
    • 30 Oct 2022
  • NexGen: Component Documentation: Indicator, Marker Lights

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Indicator, ILS Marker Lights Manufacturer: TELLLITE Master Specialties Part Number 1943-4 Lamps: T1 3/4 Midget Flange Base  2 each display Lamp Voltage not sure yet Notes: 10.29.2022 - Upd...
    • 27 Oct 2022
  • NexGen: RSS Final Road Map! LAST CHANGE (Again???)

    phoenixcomm
    phoenixcomm
    The Road Map for the RSS has changed somewhat or here we go again. I have decided to implement CANaerospace on the Arduino Megas. This is kind of tough though.  The CANaerospace protocol has never been ported to the Arduino first, the endianness...
    • 16 Oct 2022
  • NexGen: Hacking a Processor Select Panel - Part 2

    phoenixcomm
    phoenixcomm
    The Processor Select Panel, 7-F511F00121-1 (NSN: 1290-01-438-6575), is from an Apache Longbow AH-64D. I only need 2 inputs and two outputs, as identified in the blog post "NexGen: Component Documentation: Panel, Processor Select". Just so we don't ne...
    • 10 Oct 2022
  • NexGen: Component Documentation: Indicator, Fan Speed, N1

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: Indicator, Fan Speed, N1 Manufacturer:  GE Aircraft Instrument Div purchased by AMETEK Part Number: 8DJ176LZD2 MODS: A, B, C, D Instrument Clamp: Marmon: MBG69239 Weight: Cable Weight: ...
    • 8 Oct 2022
  • NexGen: Component Documentation: Display, Multi-Purpose Color, MPCD, Prototype F-16

    phoenixcomm
    phoenixcomm
    Display, Multi-Purpose Color, MPCD, Prototype F-16 Manufacture Precision Display Technologies Part Number MPCDX-PROTO weight Cable weight Video Connectors Function R Video RED  B Video BLUE G Video&n...
    • 7 Oct 2022
<>