• Products and Partners
    Products and Partners
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
Autodesk EAGLE
  • Products and Partners
  • More
Autodesk EAGLE
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • what is the eagle free

    schmittalvin
    schmittalvin
    what is the eagle freeium code
    • 14 Nov 2023
  • Adding STEP models to libraries

    e14softwareuk
    e14softwareuk
    The way EAGLE treats libraries has recently changed. Users no long need to go login to library.io to map 3D Step models to their package to get a mechanical render in Fusion360. This process is still cloud base but it begins from within EAGLE. The fo...
    • 19 Jun 2018
  • EAGLE License Management Video

    e14softwareuk
    e14softwareuk
    For those new to EAGLE this short video by Autodesk overviews how their flexible license model works showing how you can assign licenses between users in an easy and intuitive manner. Setting User Permissions for Products, Services & Support...
    • 19 Jun 2018
  • EAGLE : Year End Review : 2017

    e14softwareuk
    e14softwareuk
    What a year! 2017 was a turning point in EAGLE's evolution with Autodesk releasing version 8, their take on a classic product with a pedigree going back over 30 years. What can one say but wow, what a deluge of changes and releases that have taken pl...
    • 23 Jan 2018
  • EAGLE v8: Taming the BGA Router

    rachaelp
    rachaelp
    1. Introduction I've recently started testing out the latest version (v8.3.1) of EAGLE Premium, and one of the features I was really interested to try out since I first saw v8 earlier in the year was the BGA Router. Breaking out BGA's is...
    • 29 Aug 2017
  • Enhancments to negasilk ULP for inverted silkscreen

    yahyatawil
    yahyatawil
    Hello I used negasilk.ulp for a while for inverted silkscreen, but I decided to enhance it a little and make it easier.  Steps:  1. First create your art work (Polygon in top layer with text inside it on layer 41 tRestrict with vector ...
    • 14 Apr 2017
  • Via parameters

    kk99
    kk99
    This is my submission for the EAGLE ULPs Contest originally posted at CadSoft EAGLE Design Competition (eagle-ulp). 1. Script description:This ULP script creates a list of all vias from top to bottom layers with additional data:- signal name,- d...
    • 4 Apr 2017
  • Board Outline Helper

    ipv1
    ipv1
    Introduction This is my submission for the EAGLE Workshop CadSoft EAGLE Design Competition EAGLE ULPs Contest at EAGLE ExchangeWith the Autodesk takeover of Eagle, a lot of new features have been introduced which make ULPs for panelisation, para...
    • 3 Apr 2017
  • LibIt.ulp make creating packages more easier (Eagle Contest Entry)

    yahyatawil
    yahyatawil
    LibIt ULPThis ULP makes creating packages for libraries much easier. You can use is to draw multiple SMDs/PADs, lines and rectanglesPAD Dialog has the following options:Select Shape: Select the shape of pad (Square-Round-Octagon-Long-Offset).Select ...
    • 31 Mar 2017
  • The Double Whammy - EAGLE Gets a New Update & New Pricing

    jwatson
    jwatson
    EAGLE has been making headlines these days after teaming up with Autodesk back in June 2016. And the question on everyone’s mind is the same - what is going to change?This popular PCB design tool has been around for nearly 25 years, and has gained a ...
    • 20 Jan 2017
  • PCB Land Patterns for Surface Mount Packages and Eagle Libraries

    e14 Contributor
    e14 Contributor
    Hi, If you look at the Interconnnecting and Packaging Electronic Circuits (IPC) document IPC-7351, it appears that the footprint (PCB land pattern) required for any given SMD component will depend on the soldering method used in the underlying P...
    • 8 Sep 2016
  • finding a component of S3LP307L and S3HP157L

    e14 Contributor
    e14 Contributor
    i cant  find this two component in the eagle library which is S3LP307L and S3HP157L can anyone help me thanks
    • 4 Jul 2016
  • ECAD-MCAD Integration in EAGLE by Jorge Garcia

    Jorge_Garcia
    Jorge_Garcia
         The electrical and the mechanical CAD industries belong together, but the communication between these two has been always difficult. Today's product design cycles benefit from close collaboration between the electronic engine...
    • 26 Apr 2016
  • from board to library part

    matrixgti
    matrixgti
    Hi All, this is my first post on this forum.I have a question about a board that i just design, is basically a breakout board for an Atmel 2560 with pin header.Now i have to embed this board into another board , is there a way to convert the board in...
    • 29 Feb 2016
  • Bridging the ECAD/MCAD gap with Fusion 360 and CadSoft EAGLE

    tapnair
    tapnair
    Today’s design engineers are facing unprecedented change and challenges as the products we design become more intelligent and more connected.  New manufacturing methods, distributed manufacturing and distributed design further create a need for ...
    • 16 Dec 2015
  • egale 7.3 gerber pour isocam

    e14 Contributor
    e14 Contributor
    BonjourJ'ai un problème depuis que je possède la dernière version d'eagle.Pour faire de la gravure séparative  je crée un fichier gerber + un fichier excellon. Puis j'utilise Isocam pour créer la gravure séparativeMais depuis la version 7.3 d'ea...
    • 19 Jun 2015
  • Are you better than the Autorouter?

    Jorge_Garcia
    Jorge_Garcia
    By Jorge Garcia, Cadsoft Computer     Few tools get as much slack as autorouters do. I've never seen anyone devalue a hammer or a screwdriver, but autorouters are usually seen as the crutch of beginners in PCB design; somethin...
    • 16 Jun 2015
  • EAGLE ULPs Every User Should Know

    DaveYoung
    DaveYoung
    A ULP (User Language Program) is a feature designed into EAGLE to allow users to generate their own processes to automate tasks that would otherwise be tedious and time consuming. While most users know that this functionality exists, very few want to...
    • 19 Jan 2015
  • The 10 Most Popular CadSoft EAGLE Libraries

    element14Dave
    element14Dave
    CadSoft EAGLE is our award-winning, easy-to-use PCB design tool solution used by tens of thousands of engineers, researchers and makers around the world. Voted "Product of the Year" over nine times by leading electronics publications, EAGLE offers us...
    • 15 Jan 2015
  • Building a library in Eagle

    Workshopshed
    Workshopshed
    My first thought is don't. There are lots of libraries at CadSoft EAGLE Libraries produced by others and by manfacturers. For example I found a Samtec library for some surface mount headers I was interested in using. If you can't find a part or ...
    • 1 Nov 2014
  • CUAUV uses EAGLE PCB tools, win big at RoboSub2014!

    e14 Contributor
    e14 Contributor
    Congrats to the Cornell University, Autonomous Underwater Vehicle team who submerged in success winning 1st place at RoboSub2014 competition! Team Leader Mark Lee speaks on how EAGLE PCB tools made the difference.  My name is Mark Lee and I am t...
    • 8 Sep 2014
  • Making a PCB in Eagle

    Workshopshed
    Workshopshed
    In my previous post on Starting out with Eagle I followed Jeremy Blum's tutorial to build a 555 timer circuit using Eagle's schematic editor. I've now followed the next video and put together a PCB. Before moving on from your schematic to PCB, I...
    • 8 Sep 2014
  • Starting out with Eagle

    Workshopshed
    Workshopshed
    A few projects have come up recently where it would have been useful to make my own PCBs. I've made do with breakout boards and stripboard to complete them. I also need to put together some schematics for things like my Topsy Turvy clock project. I h...
    • 11 Aug 2014
  • Eagle v7 Beta Review!

    e14 Contributor
    e14 Contributor
    By Sophi and Garrett The new version of Eagle is on out! The biggest changes coming are a new design feature and an improved autorouter. We are both veterans of Eagle and PCB board design so this blog is intended as both a review and a tutorial ...
    • 22 Jul 2014
  • Convertir un sheet en module

    e14 Contributor
    e14 Contributor
    Bonsoir, Je viens de migrer Eagle V6 vers V7 et je voulais savoir comment, dans un projet composé de 2 sheets, je peux convertir ces 2 sheets en 2 modules ?Dois-je créer 2 nouveaux module est ressaisir la schématique dans les 2 modules ou y-a-t-...
    • 22 Jul 2014
>