Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Renesas RX65 Envision Kit - part 2a: Blinky with GCC Toolchain
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Nov 2019 2:20 PM Date Created
  • Views 2514 views
  • Likes 5 likes
  • Comments 1 comment
  • rx65n
  • gcc
  • renesas
  • e2studio
Related
Recommended

Renesas RX65 Envision Kit - part 2a: Blinky with GCC Toolchain

Jan Cumps
Jan Cumps
23 Nov 2019

I'm evaluating the Renesas RX65N MCU EV Kit.

In this post: A Blinky, with the GCC toolchain.

image

It's not a real blinky - it's a switchy. The User LED is on when the User Button is pressed.

A Morse code trainer image.

 

 

Create the Project

 

In the previous post, I used the Renesas CCRX toolchain to create a project in e2 Studio. Many things are similar when using the GCC tools.

This post expects that you did the activities in the previous blog (e.g.: that you downloaded the evaluation board definition in the configurator's board tab).

 

File -> New C/C++ Project -> Renesas RX -> GCC for Renesas RC C/C++ Executable Project -> Next

image

 

Name your project -> Next.

Toolchain: GCC for Renesas RX, latest installed version

Select the correct tatget for this board (for navigation, see the previous post).

Set the E2 Lite (RX) debugger and create a release configuration too. -> Next

 

image

 

Enable Use Smart Configurator -> Finish.

 

Configure the Project

 

In the configurator window that opens, set the board to the Envision kit. Then open the Components tab.

The New Project wizard has created one compinent.

That's the upbringing module that brings you from power-up to main() with a correctly configured controller.

 

Now we add two modules. One to configure the GPIO pins, and one that gives us the pin definitions anf GPIO API.

 

On the Components tab, press the + button.

This brings up a list of available components.

The first time, we have to do two steps (Renesas gurus may chime in here to refine what needs to be selected/configured).

 

Change the IDE configuration to allow that blocked modules are shown.

Configure General Settings -> Enable Allow blocked FIT modules to be displayed -> Apply and Close

image

 

Then add all components . This takes a long time.

Download more software components -> Disable Show RX Driver Package only -> Select All -> Download.

Go for a coffee.

image

 

Once they are added, select these two:

  • Ports: to enable the ports and pins, and set the direction
  • r_gpio_rx: to add the pin header file and gpio APIs.

image

 

Cick Finish.

 

The user switch SW2 on the evaluation board is assigned to Port 0 bit 5, the LED2 blue led to Port 7 bit 0.

We'll set these pins as I/O functional inputs and outputs.

 

image

 

image

 

Select the Config_PORT module and enable PORT0 and PORT7. 2 new tabs appear.

image

Select tab PORT0 and set P05 to In.

image

Select PORT7 and set P00 to Out.

image

 

In the MCU package view, these pins have changed colour and definition:

image

 

In the Pin tab, they have also changed (here P70 (port 7 pin 0) as example):

image

 

image

 

That's it. The r_gpio_rx component does not need to be maintained.

Save the configuration file, then Generate Code.

 

Write the C Code

 

Activate the IDE's C/C++ perspective.

image

The configurator has created a project structure. Take some time to familiarise.

Then open the main file, RX65_blinky.c.

 

Let's add the header file for the driver code, and the pin definitions:

 

#include "r_gpio_rx_if.h"     /* Contains prototypes for the GPIO driver */

#define  SW_2    (GPIO_PORT_0_PIN_5)
#define  LED_2   (GPIO_PORT_7_PIN_0)

 

Then write a very simple main() loop.

It will check if the button state has changed, and if yes, update the LED state.

 

void main(void) {
    gpio_level_t lastLevel = GPIO_LEVEL_LOW;
    do {
        gpio_level_t level = R_GPIO_PinRead(SW_2);
        if (level != lastLevel) {user button on the lft of the board.


            lastLevel = level;
            R_GPIO_PinWrite ( LED_2, level);
        }
    } while (1);
}

 

Build and Debug

 

See the previous post for the instructions. It's identical for this project.

If you get a failure at startup, you mmay have skipped the step in that section to set the Power and Frequency options in the debug configuration.

Once the code is running, the blue led next to the USB connector will be on when you push the

 

image

 

 

Related blog
part 1: Create an Empty Project
part 2a: Blinky with GCC Toolchain
part 2b: Blinky with Timer and Interrupt
part 3: Port an example from Renesas toolchain to GCC
part 4a: Low Power - Sleep
part 4b: Low Power - Software Standby
4c todo: power mode 3
4d todo: power mode 4
part 5: DAC
part 6: Software SHA
part 7: Blinky with FreeRTOS
part 8: DMA
part 9: UART
part 10: Reserve LCD Frame Buffer in Expansion RAM with GCC
part 11: port emWIN to GCC and run an LCD Widget
Renesas RX65N MCU EV Kit - Review
Andrew Johnson's blog series
Renesas Envision Kit RPBRX65N Roadtest
Attachments:
RX65_blinky.zip
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    A new GCC version 8.3 is released for Renesas RX: https://gcc-renesas.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago

    A new GCC version 8.3 is released for Renesas RX: https://gcc-renesas.com/