Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Renesas RX65 Envision Kit - part 3: Port an example from Renesas toolchain to GCC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2019 10:10 PM Date Created
  • Views 2721 views
  • Likes 6 likes
  • Comments 5 comments
  • RoadTest
  • rt
  • renesas
  • e2studio
Related
Recommended

Renesas RX65 Envision Kit - part 3: Port an example from Renesas toolchain to GCC

Jan Cumps
Jan Cumps
24 Nov 2019

I'm evaluating the Renesas RX65N MCU EV Kit.

In this post,  I'll port the LCD driver example from the Renesas proprietary CC-RX

image

 

 

 

Renesas offers a GCC toolchain that can build firware for the RX65 family. I have been using it for most of my developments and it works .

The toolchain is nicely integrated in the e2 Studio IDE. The full cycle from project creation to debug is supported.

Let's see how you can port a project from CC-RX to GCC: the QE for Display [RX] Sample Program.

 

First, create a GCC project in e2 studio. Look at post 2a for  instructions.

Then, use the configurator to add the r_glcdc_rc component.

Enable LCD_CLK Pin and LCD_TCO0 -> 15.

Save and generate code.

 

Then copy the example sources from the Renesas project over from src to src:

main.c

r_image_config_RX65N_Envision.h

r_lcd_timing_RX65N_Envision.h

 

Also copy over the image folder. It contains the test pattern.image shown at the beginning of this post.

When you build the cde, it will fail for one source line:

 

#define FRAME_BUF_BASE_ADDR  (__sectop("FRAME_BUFFER"))

 

This is because __sectop() is a Renesas toolchain specific construct. It returns the address of the begin of the FRAME BUFFER section.

An other option is to read the documentation. It says that this address = 0x0800000.

 

image

That means I can get away by replacing the line with:

 

#define FRAME_BUF_BASE_ADDR   0x00800000

 

No other changes are needed. Build and debug.

Once this line in the main() function has been executed, we can manipulate the screen:

 

    /* ---- Initialization of frame buffer area ---- */
    frame_buffer_initialize();

    /* ---- Initialization of the GLCDC, and start display ---- */
    glcdc_initialize();

 

image

 

 

 

note: I was not successful in porting these Renesas components to GCC: the FAT and SHA1 modules.

These modules don't publish all sources. Part of the implementation comes in a pre-compiled .lib binary.

These libraries are specific for the Renesas rlink optimised linker. They aren't compatible with GCC linkers.

There is a tool available to convert Renesas .lib of type SH (fixed location libs) but the libs provided with the two modules above are not of that type.

 

That means that the default secure bootloader example (it uses SHA1 to validate new firmware and uses FAT to get the signed firmware from a USB stick) is not easy to port. I managed to port the soource compilation but haven't found a way to link in the FAT and SHA1 blobs.

 

If you plan to build the out-of-box example from source, do that within the first 60 days after you first used the Renesas toolchain, the archive those project with the build artifacts for later use. The toolchain is fully functional the first 60 days. After that, a few options are restricted. One of those options affects your ability to build those examples: a code size restriction of 128K (for the RX family). You need more for the default demo.

The price for a one year names STD licence for the CC-RX packet is a little over USD 300. That will give access to full-size binaries.

A one seat PRO license adds security and compliance related functionality (e.g.: MISRA-C rule validation) and costs approx. USD 350 / year.

For professional use, those are fair prices.

 

The e2 studio project is attached.

 

Related blog
part 1: Create an Empty Project
part 2a: Blinky with GCC Toolchain
part 2b: Blinky with Timer and Interrupt
part 3: Port an example from Renesas toolchain to GCC
part 4a: Low Power - Sleep
part 4b: Low Power - Software Standby
4c todo: power mode 3
4d todo: power mode 4
part 5: DAC
part 6: Software SHA
part 7: Blinky with FreeRTOS
part 8: DMA
part 9: UART
part 10: Reserve LCD Frame Buffer in Expansion RAM with GCC
part 11: port emWIN to GCC and run an LCD Widget
Renesas RX65N MCU EV Kit - Review
Andrew Johnson's blog series
Renesas Envision Kit RPBRX65N Roadtest
Attachments:
RX65N_GCC_QE_for_Display_sample_RX65N_Envision.zip
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    Here's a list of all Renesas examples, application notes and downloads for the RX65 family. There's a lot available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago

    Here's a list of all Renesas examples, application notes and downloads for the RX65 family. There's a lot available.