Sensors
  • Technologies
  • More
Sensors
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • NASA Used Optical Satellite Imagery to See the Long-Term Impact of the Megatsunami That Struck in 1958

    Catwell
    Catwell
    The largest tsunami ever recorded struck Lituya Bay in 1958. (Image Credit: NASA Earth Observatory) In 1958, a huge landslide caused 90 million tons of rock to slam into Alaska’s Lituya Bay. This impact produced a tsunami with a wave height o...
    • 24 Jul 2025
  • Texas Researchers Develop New Technique to Predict Underwater Landslides

    Catwell
    Catwell
    Underwater landslides can impact offshore infrastructure like wind turbines. (Image Credit: Nicholas Doherty/Unsplash) When underwater landslides hit, they can move huge amounts of sediment into the ocean, potentially damaging offshore infrastructur...
    • 22 Jul 2025
  • ASLM Uses a 3D Scanner to Replicate Vincent Van Gogh Paintings

    Catwell
    Catwell
    ASML gallery. (Image Credit: ASML/X) I would want a print from this tech, for sure. I fear the potential price. ASML and the Van Gogh Museum partnered to develop a 3D scanner capable of producing extremely detailed replicas of Vincent Van Gogh&rsquo...
    • 20 Jun 2025
  • Researchers Develop a New Device That Splits White Noise into an Acoustic Rainbow

    Catwell
    Catwell
    The ARE device uses scattering structures to split broadband white noise from a single source into an acoustic rainbow. The sound is mapped on a visible spectrum based on magnitude and frequency. (Image Credit: Science Advances) Researchers from the...
    • 18 Jun 2025
  • Researchers Introduce Metalens Microscope for Medical Applications

    Catwell
    Catwell
    The metalens-based microscope can address off-axis aberrations and achieve high-resolution wide-field imaging. (Image Credit: Tao Li and Jiacheng Sun (Nanjing University)) Optical technology could soon change thanks to the introduction of metalenses...
    • 10 Jun 2025
  • Open Bionics Launches the Hero Pro Bionic Arm For Amputees

    Catwell
    Catwell
    Open Bionics’ Hero Pro has a higher payload than other bionic arms. (Image Credit: Open Bionics) Bristol-based robotics company Open Bionics developed and launched Hero Pro, the world’s first wireless bionic arm for amputees. The company...
    • 28 May 2025
  • Earlier This Year, A Private Lander Touched Down on The Moon

    Catwell
    Catwell
    The Blue Ghost spacecraft touched down on the lunar surface, capturing an image of Earth on the horizon. (Image Credit: Firefly Aerospace) In March, Firefly Aerospace landed its Blue Ghost spacecraft on the Moon's surface, touching down "in...
    • 23 May 2025
  • China Fires Laser at a Moon-Orbiting Satellite in Daytime

    Catwell
    Catwell
    (Image Credit: marmixer/pixabay) Recently, China’s Deep Space Exploration Laboratory (DSEL) pointed, fired, and deflected a precision laser at a moon-orbiting satellite 80,000 miles away from Earth. This breakthrough with laser technology demo...
    • 8 May 2025
  • Researchers Believe Mosquito Antennas Could Help Unlock New Sensor Technology

    Catwell
    Catwell
    CT scan showing the structural antenna of a male mosquito. (Image Credit: Purdue University/Phani Saketh Dasika) Mosquitoes have unique sensory capabilities, and scientists believe they can use them as inspiration for developing new technology. Purd...
    • 30 Apr 2025
  • NASA Tracks a Large Anomaly in the Earth's Magnetic Field

    Catwell
    Catwell
    NASA tracks the South Atlantic Anomaly, a weakened region in the magnetic field that stretches 1,800 miles. (Image Credit: NASA Goddard/YouTube) For years, NASA researchers have been keeping a close eye on a weakened part of the magnetic field calle...
    • 17 Apr 2025
  • Scientists Develop 3D Holographic Display Where Objects Can be Touched and Manipulated

    Catwell
    Catwell
    The FlexiVol volumetric display does away with rigid diffusers in favor of elastic ones that can be touched and handled safely. (Image credit: Public University of Navarra) Scientists from the Public University of Navarra (UPNA) have developed Flexi...
    • 16 Apr 2025
  • Researchers Turn Light into a Supersolid State for the First Time

    Catwell
    Catwell
    System in reciprocal and coordinate space. (Image Credit: Nature (2025) An international team of engineers, nanotechnologists, and physicists has made it possible to transform laser light into a supersolid. This breakthrough could ultimately unlock ...
    • 12 Mar 2025
  • Researchers Put Mouse Brain Samples in Suspended Animation and Successfully Revived Them

    Catwell
    Catwell
    The brain slices underwent directional cooling via a copper cylinder immersed in liquid nitrogen. (Image Credit: bioRxiv) For the first time, scientists at the University of Erlangen-Nuremberg cryogenically froze and revived hippocampal slices of m...
    • 11 Mar 2025
  • Nasa’s Cone-Shaped Telescope to Unveil More About the Universe

    Catwell
    Catwell
    NASA’s SPHEREx telescope could give scientists a better understanding of the universe. (Image Credit: NASA/JPL-Caltech) We’re getting a better glimpse of the cosmos soon! The SPHEREx (Spectro-Photometer for the History of the Universe, E...
    • 28 Feb 2025
  • Canon Drops World’s First 410MP Image Sensor with 24K Resolution

    Catwell
    Catwell
    The CMOS sensor packs a staggering 24,592 x 16,704-pixel resolution, the largest ever achieved in a 35mm full-frame sensor. (Image credit: Canon) Canon recently unveiled the world’s first CMOS image sensor that packs 410MP, which is equivalent...
    • 19 Feb 2025
  • Upgrade Zigbee Devices and Turn Them into Motion Sensors with A Firmware Update

    Catwell
    Catwell
    Three or four Zigbee devices grouped within a room act as virtual sensors that detect human movement, turning the lights on/off. (Image Credit: Ivani) Zigbee bulbs and plugs have gotten a whole lot better. With a simple firmware update, these smart ...
    • 18 Feb 2025
  • China Develops Robot Inspired by Cats for Space Applications

    Catwell
    Catwell
    The robot lands on its feet like a cat, adjusting its position in mid-air. (Image Credit: Journal of Astronautics) Researchers at the Harbin Institute of Technology developed a cat-like robot that twists and lands on its feet while falling. Powered ...
    • 6 Feb 2025
  • Landing Zones Canada Unveils Stealthy New Drone

    Catwell
    Catwell
    The APDS can switch from supersonic to low loitering speeds. (Image Credit: Landing Zones Canada) Landing Zones Canada recently built an efficient, reliable payload delivery drone called the Eagle Advanced Payload Delivery System (APDS). This cuttin...
    • 5 Feb 2025
  • 10 Fun Innovations I liked at CES 2025

    Catwell
    Catwell
    The robot vacuum has an arm and a claw to help homeowners with tedious cleanups. (Image Credit: Roborock) We get tired of seeing socks on the floor and going through all that back-breaking work to pick them up. Thankfully, the Roborock Saros Z70 ro...
    • 22 Jan 2025
  • Lab on a Chip: From Humble Beginnings to the Latest Innovations

    Catwell
    Catwell
    The microfluidic chip is a lab-on-a-chip device that can be used to detect diseases or check the patient’s compatibility with drugs. Image credit: Wikipedia) Lab on a Chip (LOC) is described as a microfluidic device that integrates one or mor...
    • 2 Jan 2025
  • Drones Take Advantage of Next-Gen MEMS Technology for Modern Agriculture

    Catwell
    Catwell
    (Image credit: Pixabay) Drones are fast becoming an invaluable tool in the agriculture industry, undertaking multiple roles to ensure healthy and maximum crop yields. According to a recent report from DJI, over 300,000 drones operate globally, treat...
    • 31 Dec 2024
  • Time-of-Flight Imaging: Low-cost sensing with ams/OSRAM TMF8828 and Pi Pico

    shabaz
    shabaz
    Table of Contents Introduction Quick Overview How Does it Work? I2C Registers Overview Reading and Writing Registers Application Mode Pages USB UART Interface Browser Based App Summary Introduction Time-of-Flight sensors are fascinating. They...
    • 11 Dec 2024
  • Researchers Extracted Ancient DNA to Bring Back the Iberian Lynx from Extinction

    Catwell
    Catwell
    (Image Credit: Miller_Estzer/pixabay) Welcome to… Holocene Epoch park. The Iberian lynx went nearly extinct, and now it’s making a comeback. Thanks to conservation efforts, its population grew from 25 in 2002 to over 400 reproductive fe...
    • 29 Oct 2024
  • MIT Researchers Capture Images of Atoms Flowing In an Edge State

    Catwell
    Catwell
    A rending of the quantum fluid (gold) flowing along a laser light wall (green) and moving around obstacles. (Image Credit: Sampson Wilcox/MIT) MIT researchers recently observed edge states in a cloud of ultracold sodium atoms. They also captured ima...
    • 10 Oct 2024
  • Scientists Identify Unusual Signal that Reverberated Around the World for Nine Days

    Catwell
    Catwell
    The seismic activity was the result of a massive landslide in Greenland's Dickson Fjord, which caused a 200-meter-high mega-tsunami that sloshed back and forth roughly 10,000 times in nine days. (Image credit: Wikipedia) On September 16, 2020, ...
    • 24 Sep 2024
<>