Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Blog
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Super Smart Home #3 Designing the Control Center

    balearicdynamics
    balearicdynamics
    Proof of Concept The UI Development Lifecycle Qt for the UI design What is in the "mainwindow.ui" File? Making the Interface Design Usable in Python Integrating the Python UI Class Into the Application Full Content Already Posted (until...
    • 23 Apr 2020
  • Super Smart Home #2 The Door Opener

    balearicdynamics
    balearicdynamics
    Components Developing on the ESP8266-01 A Simple Programmer Board Testing the ESP8266-01 The Software Full Content Already Posted (until now) Sources, Circuits, and Documentation Thanks to ComponentsA short foreword that will remain...
    • 22 Apr 2020
  • Super Smart Home #1 The project

    balearicdynamics
    balearicdynamics
    Introduction The Project The Nodes Node 1 - Door Bell Node 2 - Door Opener Node 3 - Environmental Control Node 4 - Lighting Control Node 5 - Appliances Node 6 - Alarms Node 7 – Cloud Full Content Already Posted (until now) Sou...
    • 21 Apr 2020
  • SmartCage: Overview of AWS (Blog #2)

    neuromodulator
    neuromodulator
    Overview of AWS While waiting for the Cypress PSOC to arrive I began studying how to use the AWS platform. AWS as the name implies is a set (actually a full ecosystem) of web services provided by Amazon to perform a wide variety of tasks such as...
    • 21 Apr 2020
  • The Bio Highway – Exploring ADC with Cypress ModusToolbox and Device Configurator

    vlasov01
    vlasov01
    Plan for The Week My plan for this week was pretty simple - enable reading of analog data from on-board thermistor using ModusToolbox. It is an important step to convert Arduinio code for heart beat sensor to PSoC 6 and specifically to my board ...
    • 20 Apr 2020
  • Connected Cloud Challenge - Smart Backup Sump Pump #3

    cmelement14
    cmelement14
    In my previous blog, I showed what the local console messages look like when the AWS demo application has been successfully run on the PSoC®︎ 6 WiFi-BT Pioneer Kit. How can you quickly prove that the transmitted messages have actually arrived on AWS s...
    • 19 Apr 2020
  • Sense the mail, Send to cloud #5

    saicheong
    saicheong
    We are working on sense the mail inside the mailbox, In Pioneer kits TFT shield, we have a motion sensor and a Ambient Light Sensor, we could like to use those to sense the mail, so no additional sensor need to use. BMI160 The BMI160 is connecte...
    • 18 Apr 2020
  • Connected Cloud Challenge -  IoT based Advertisement BillBoards/Hordings - Summary

    sami9974
    sami9974
    It won’t be a bigger problem to find one digital hoarding in your area. Since the introduction of Digital Advertisements.As project plan I have decided to divide this project into 4 parts as below :1) User Interface (Website)2) AWS IoT3) DataBase4) ...
    • 14 Apr 2020
  • Study of AWS shadow sync between iOS and the Cypress IoT device #4

    saicheong
    saicheong
    www.youtube.com/watchIn our project, which require synchronise the state between two or more devices, one is located onsite for monitoring and control physical environment (the things), another is the remote devices may virtually such as APP or the h...
    • 14 Apr 2020
  • The Bio Highway – Getting Started with Heartbeat Sensor

    vlasov01
    vlasov01
    AD8232 ECG Measurement Heart Monitor Sensor ModuleMy initial plan was to use AD8232 ECG Measurement Heart Monitor Sensor Module. The AD8232 is a low cost integrated front end for signal conditioning of cardiac bio electrical signals to monitor heart ...
    • 12 Apr 2020
  • Getting Started with Cypress PSoC®︎ 6 WiFi-BT Pioneer Kit - #1

    weiwei2
    weiwei2
    Details about this contest is at Connected Cloud Challenge with Cypress and AWS IoT and it contains useful information and technical resources link.for convenience, i also copy and paste some of these urls at the references section of this blogIt is ...
    • 11 Apr 2020
  • Mbed RTOS thread: Send CapSense Data to AWS #3

    saicheong
    saicheong
    Working for framework of RTOS threadingwww.youtube.com/watchIntroductionIn order to send of data without blocking and improve the smooth  of user interface and background monitoring/tracking, the system required running under thread control prov...
    • 8 Apr 2020
  • Connected Cloud Challenge - IoT Gaming Table - Summary

    brianchilders
    brianchilders
    Connected Cloud Challenge - IoT Gaming Table - SummaryBy Brian Childers - April 2020 Summary Brief / Intended AudienceAbout Me / Connected Cloud Challenge InterestConnected Cloud Challenge - IoT Gaming TableWhat's in the boxAbout the PSoC 6 ...
    • 5 Apr 2020
  • The Bio Highway – Finishing the First Mile

    vlasov01
    vlasov01
    Which platform should I use - Amazon FreeRTOS or Mbed OS? It is a good question to think about before investing a lot of time into a new platform as at the end our time is our most precious resource, It requires some analysis. I've googled Inter...
    • 5 Apr 2020
  • Mbed connect to AWS iOT, OS, driver, security ..  #2

    saicheong
    saicheong
    Developing Framework for the Project www.youtube.com/watch How i choose platform I am try to build the framework which is the foundation of this project. In Cypress PSOC 6, we can choose three main OS 1. PSOC ModusToolbox App, whi...
    • 3 Apr 2020
  • Connected Cloud Challenge - Smart Backup Sump Pump #2

    cmelement14
    cmelement14
    Set up AWS After some struggling, I finally got the AWS IoT account setup. However, I have problem to connect the PSoC®︎ 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WIFI-BT) to the cloud. I found Cypress' start guide Getting Started with Amazon FreeR...
    • 3 Apr 2020
  • SmartCage: Introduction and plan (Blog #1)

    neuromodulator
    neuromodulator
    Introduction In this design challenge I will build a system that will track small rodents activity and their environmental conditions. The system will use AWS and make the captured sensor data available (probably through a dashboard) to the pet ...
    • 31 Mar 2020
  • The Bio Highway – Getting Started or the First Mile

    vlasov01
    vlasov01
    I’ve done a couple of personal projects on AWS building simple Alexa skills, but I’m not an expert in AWS. And I’ve used different MCUs, but never used Cypress PSoCs. After I’ve listen to a couple of AWS podcasts on AWS IoT I’ve decided to start my ...
    • 30 Mar 2020
  • Connected Cloud Challenge - Smart Backup Sump Pump #1

    cmelement14
    cmelement14
    Project Introduction I am going to use this design challenge to design a backup sump pump for my house. The following diagram depicts my design idea. When the power grid is off, the true sine wave UPS will power the sump pump when it needs to ki...
    • 29 Mar 2020
  • Begin the journey : Hello the World by PSoC6 Kits

    saicheong
    saicheong
    An Intellectual MailboxBriefing of ProjectOur project is build a mailbox which can detect the mail arrived and inform owner which the mail coming though cloud services, the prototype based on PSoC 6 WiFI-BT Pioneer Kit and try to minimum the BOM, the...
    • 27 Mar 2020
  • The Bio Highway - Introduction

    vlasov01
    vlasov01
    The problemSport exercises can generate significant stress for human body. It may be difficult for many to realize where is their limit. There is a high risk of going over the limit. At the same time it may be not very efficient to perform workout fa...
    • 21 Mar 2020
<