PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Art-a-Tronic Episode 2
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
  • Author Author: balearicdynamics
  • Date Created: 17 Mar 2019 11:57 AM Date Created
  • Views 3623 views
  • Likes 14 likes
  • Comments 17 comments
  • exhibition
  • depot09
  • cage
  • animatronic
  • mannequin
  • elegoo
  • pi-casso
  • gods
  • hackster.io
  • raspberry pi
  • cenciurio wines
  • lorenzo p merlo
  • technology in cage
  • challenge
  • art
  • digital painting
  • Making
  • pi face
  • ptron
  • mars 3d printer
  • hacking
  • neptune 3d printer
  • art-a-tronic
Related
Recommended

Art-a-Tronic Episode 2

balearicdynamics
balearicdynamics
17 Mar 2019

  • Introduction
  • Moving the Mannequin
    • Thinking on How to Move the Torso
    • The Most Affordable Solution
  • Previous Episodes
  • Next Episodes

Introduction

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have already received the notification from UPS that the challenge kit will arrive next Tuesday 19; in the meantime, the exhibition installation goes ahead. Lorenzo's operas will create a path for visitors. As there are many different points of view you can read Art-a-Tronic, as well there are different paths you can follow visiting the exhibition.

Moving the Mannequin

An almost complex part is adding the motion to the mannequin. The problem is that it has been designed and build more than half a century ago so integrating some sort of movement in it sounds very difficult. Unfortunately, the head is fixed; probably it is possible to cut the neck in the middle adding some rotation but I think that this will penalize too much the aesthetics so the head will remain fixed. There are five points that can be moved corresponding to the articulated parts of the mannequin: wrists, shoulders, and torso.

I have also considered that all the motion interventions will include some kind of alteration in the form of the joints but this can be easily masked properly dressing the parts.

There is also another important consideration; to control the motion I expect to interface a dedicated microcontroller able to manage the low-level motor motion part autonomously and in part receiving orders from the brain, the Raspberry PI 3B+

 

Thinking on How to Move the Torso

image

Torso - or, better, the upper part of the body - is fixed through an axle screwed on the upper plane of the legs (that can't move). The first ides was using a couple of motors pushing vertically from the torso with threaded bars but this implied a lot of mechanical problems, including fixing the motors on the upper part and the thread bars attach to the bottom parts.

image

Excluding the possibility to have the torso oscillating I decided for a single-motor solution acting as a linear transducer as shown in the stepper parts positioned approximately in their asset shown in the image below.

image

Using this Stepper motor just makes the body taller some cm so it is acceptable without losing the aesthetical body proportions.

The two images below show the legs upper surface by the plant. I will start from this point to design the parts that must fit inside this space.

imageimage

 

The Most Affordable Solution

Update

I have reviewed in detail the possible solutions to move the torso. The initial idea - very similar to those suggested by beacon_dave (Dave Ingels_ - sounds attracting but reviewing in depth how the two parts mannequin is joined arise a lot of difficulties, with the risk to be not feasible in a good way. The images below show how the central joint is an essential part of the entire torso support and can't be avoided. the lock nut is part of the system keeping together the two legs, as a matter of fact, the bottom half of the body.

imageimageimage

Changing this part means to replace is rebuilding one in a different way and in my opinion it is not the worth as the same result can be reached in an easiest way, apparently more complex but that requires definitely less extra 3D printed parts.

image

As shown in the above image, the shaft is not just a bar but includes a turnable spring to keep the torso in the desired orientation. This sounds good to fine-tune the upper part when there is the motor with the linear transducer. Following this proof of concept I have drafted a quoted sketch to fix the ideas before proceeding to model the parts that should be 3D printed.

image

I should make only two parts for the bottom: the stepper support that should be fixed to the plane and the back side support. To make it working without attrite, I will use a free fall bearing, part of the same 3D printing. Note that in the sketch I have designed only the bottom guide for the back of the torso but in reality, there is a counterpart that will be fixed to the bottom of the torso; both together will be thick like the motor. The threaded bar is oriented horizontally to the longitudinal (the longest side) of the torso in correspondence to the mannequin belly to be completely hidden.

 

So, don't lose the next episode.

 

Previous Episodes

  • Art-a-Tronic Episode 1

 

Next Episodes

  • Art-a-Tronic Episode 3
  • Art-a-Tronic Episode 4
  • Art-a-Tronic Episode 5
  • Art-a-Tronic Episode 6
  • Art-a-Tronic Episode 7
  • Art-a-Tronic Episode 8
  • Art-a-Tronic Episode 9
  • Art-a-Tronic Episode 10
  • Art-a-Tronic Episode 11
  • Art-a-Tronic Episode 12
  • Art-a-Tronic Episode 13
  • Art-a-Tronic Episode 14
  • Art-a-Tronic Episode 15
  • Art-a-Tronic Episode 16
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago +7
    A small slewing ring bearing with gear teeth might be worth considering ? https://en.wikipedia.org/wiki/Slewing_bearing Insert the motor vertically into that existing hole with a pinion on the end of its…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave +7
    Hello Dave, thank you for the suggestion. The idea just as you mention, unfortunately, is not reliable. The torso should have a larger base to rotate( not so many degrees) But in theory - I have already…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to beacon_dave +6
    Hello Dave (bis) I have reviewed again your idea. Take a look to the video below, I have already applied it in the past to make the camera pan prototype: www.youtube.com/watch I worked fine in this case…
Parents
  • mcb1
    mcb1 over 7 years ago

    Enrico

    Depending on the hole in the upper body, you should be able to add a normal bearing that resides on the top of the threaded bolt

    image

    The inner race will sit on this, while the outer supports the body.

    It may require a small spacer or 3D printed part to go between the bearing and other parts.

     

     

    I'd also replace the spherical bottom bolt with a fixed version so that the torso and legs are in the same plane.

    image

     

    I'd then use a wooden ring attached to the upper body, and a rubber wheel pressing against the inside (or outside) of the ring to make it rotate.

    You should be able to mount the motor through the leg.

    I you make the motor and wheel sprung loaded, it would allow for any off centre issues and allow the tension to be adjusted.

     

    There are plenty of geared motors, or a geared stepper motor should give enough torque and be much smaller than the one above.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to mcb1

    Hi Mark,

     

    thank you for your contribution. I am happy that this project is creating attention stimulating suggestions and criticism.

    Well, I have checked again the details but this solution is not viable. This is a mannequin of the mid of the '60s: heavy, well done and most of the parts are really well refined by hand. Advantages and disadvantages...

     

    The legs are two and the bottom part of the body is divided in two parts, joined inside (the hole is just to close the joint nut. The same joint is the support for the shaft bottom M4 screw with the blockage nut. The problem of the spherical support is meaningless as the top regulation of the shaft act to the inside spring and metal cylinder to lock the shaft in the desired position. It is very robust when locked (if should support in the original design, both the torso and the dressing). This is fundamental as the body planes separating the two halves are not perfectly plane, just well refined. The entire shaft length (25 mm diameter) will fit inside the body to keep in position at the right azimuth but it is fundamental that the torso is based on something almost large.

    You mention geared motors (excluded as I should make specific movements so the choice is for a stepper). But probably not evident in the images, this stuff is a 1.80 tall real size person build without material economy in mind. The torso, empty as it is now, is about 5.5 Kg that will probably reach 6.5 with the stuff I will add. So the Nema 17 stepper motor and the reduction of the pulley is the minimum essential to be able to move it without too much effort.

    Mixing the various ideas I have discussed until now the solution I am trying to design for now is Lazy Susan bearing on the peripheral, the motor inside the base of the legs (not exactly in-axis with the shaft), and a reduction pulley of 150 mm diameter. As the rotation angle should be about +30 / -30 Deg, I will try to use a 2 mm tooth belt to join the big pulley (fixed to the dorso bottom) together with the small (20 teeth) pulley on the motor shaft.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to mcb1

    Hi Mark,

     

    thank you for your contribution. I am happy that this project is creating attention stimulating suggestions and criticism.

    Well, I have checked again the details but this solution is not viable. This is a mannequin of the mid of the '60s: heavy, well done and most of the parts are really well refined by hand. Advantages and disadvantages...

     

    The legs are two and the bottom part of the body is divided in two parts, joined inside (the hole is just to close the joint nut. The same joint is the support for the shaft bottom M4 screw with the blockage nut. The problem of the spherical support is meaningless as the top regulation of the shaft act to the inside spring and metal cylinder to lock the shaft in the desired position. It is very robust when locked (if should support in the original design, both the torso and the dressing). This is fundamental as the body planes separating the two halves are not perfectly plane, just well refined. The entire shaft length (25 mm diameter) will fit inside the body to keep in position at the right azimuth but it is fundamental that the torso is based on something almost large.

    You mention geared motors (excluded as I should make specific movements so the choice is for a stepper). But probably not evident in the images, this stuff is a 1.80 tall real size person build without material economy in mind. The torso, empty as it is now, is about 5.5 Kg that will probably reach 6.5 with the stuff I will add. So the Nema 17 stepper motor and the reduction of the pulley is the minimum essential to be able to move it without too much effort.

    Mixing the various ideas I have discussed until now the solution I am trying to design for now is Lazy Susan bearing on the peripheral, the motor inside the base of the legs (not exactly in-axis with the shaft), and a reduction pulley of 150 mm diameter. As the rotation angle should be about +30 / -30 Deg, I will try to use a 2 mm tooth belt to join the big pulley (fixed to the dorso bottom) together with the small (20 teeth) pulley on the motor shaft.

     

    Enrico