Products
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
Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Wireless charging - Success!
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hlipka
  • Date Created: 26 Jun 2014 11:46 PM Date Created
  • Views 1236 views
  • Likes 1 like
  • Comments 4 comments
  • beyond_the_phone
Related
Recommended

Wireless charging - Success!

hlipka
hlipka
26 Jun 2014

Its now about 1:30 in the morning, so this post might be too late for the contest. But I finally finished my wireless charged snow groomer. After doing the final reworks and bodges on the PCB, I added the needed connectors and put everything together.

Receiver

For the wireless receiver, I added a small support board that holds the receiver PCB with the coil attached to it. I put the coil on the back side of the receiver PCB, and fixed it with two layers of Test Power Strips. That helped in leveling out the solder joints from the PCB:

image

I then mounted that PCB on an acrylic plate, and used standoffs and spacers to get it to the right height.

PCB reworks

Nearly all parts of my circuit needed some form of touching and reworks. What once was a nice board now looks quite patchy:

image

(Top side, with most of the reworks for the end-of-charge circuit)

image

(Backside, where the wires are for the differential amplifier)

On the right side on the back one can see the PCB areas designated as heat sinks for the balancer FETs.

Connector puzzle

After finishing the PCB (and verifying that everything works as it should) I added connectors to put everything together:

image

Here the base plate is visible. It also holds the PCB, which gets half-hidden under the receiver board. To allow that, I removed the test points and the programming header from the receiver.

The battery is a 11.1V, 1300mAh race car battery (an extron X1), which comes with both a balancer connector (for charging) and power leads. I added a screw terminal to them, so I can remove it easily.

The final step

As final step I just needed to fit everything in the battery compartment of the snow groomer. Since I measured quite carefully, I knew how large all the stuff was allowed to be. So it was not a surprise that everything did fit in snugly:

image

The battery and the acrylic plate span together the whole length, to they hold quite tight. On the side there is enough room for the connectors. It was a welcome surprise, after all these set-backs in the last few days, that it did indeed work on the first try.

When putting it on the charger base station, I found out that it fit a little bit too tight - I should have save some millimeters there... But the charging notification on the transmitter turned on, and also my current sense notification. Even though its a little bit hidden:

image

I also should put the USB power cable entry not to the side, but to the front, since its now to close to the driving chain.

image

But the status LEDs from the transmitter a visible, so I consider this as OK.

Wrapup

Thanks to Element14, Texas Instruments and especially Würth for this contest, all the parts and the support given to all the contestants! Many thanks especially to Christian and Simon!

Even though it has been stressful at some times, this was a fun project. My son was delighted when he discovered (today in the afternoon...) what I did build for him. And for me it means there are now two toys less where the batteries are empty at the wrong moment, and I don't need to keep charge of them. I also learned a great deal, not only about wireless charging.

This won't be my last post on this project. I still need to come up with the final schematic. And I also will need to do some more verifications and tests before I hand this project over to my son. So I will report about that also, but give me a short break to catch up with my sleep...

All the blog posts

In chronological order (more or less):

Beyond the phone - ein Plan muss her!

Wireless power demo board - Ein erster Eindruck

Wer misst, misst Mist - or measuring the performance of the wireless demo kit

Besser zweimal messen - update to my performance evaluations

Wireless Power - Pläne schmieden

Wireless power - Wie lade ich einen Akku-Pack?

Wireless power - charging a battery pack part 2

Wireless power - charging a battery pack part 3

Two times is not enough - Measuring the performance of the wireless power demo kit part 3

Wireless power - battery undervoltage lockout with multiple cells

Wireless charging - status update

Wireless charging - complete schematic walkthrough

Wireless charging - status update 2

Wireless charging - status update 3

Wireless charging - proof of work

Wow, 16 articles. Thats nearly one article per week. I did not remember to write that much...

  • Sign in to reply
Parents
  • waelect
    waelect over 12 years ago

    Well Done Hendrik, glad you have it all completed now you can relax.

     

    Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • waelect
    waelect over 12 years ago

    Well Done Hendrik, glad you have it all completed now you can relax.

     

    Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hlipka
    hlipka over 12 years ago in reply to waelect

    My plan for today is not to touch anything about this project, clean up my work bench, and go to bed early image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    Funnily I also wanted to go to bed at a decent hour.

    Luckily its the weekend tomorrow and I can sleep in......image