Arduino

An open-source platform platform that makes hardware and software accessible for rapid prototyping, learning, experimenting, and tinkering. Discuss topics and share knowledge on the entire range of Arduino compatible boards and accessories, from Classic to MKR boards, and more.

Featured Content
image tile

How to Program the Arduino Opta PLC

This article explores how Arduino-based Opta® PLC can mitigate PLC programming challenges. It also introduces the Arduino PLC programming environment, highlighting its benefits and applications in automation

Read Blog

image tile

Exploring Arduino Pro's Role in Industry 4.0

This webinar highlights how edge computing technology can drive efficiency in applications related to Industry 4.0.

image tile

Arduino Giga R1 WiFi

Buy Now    Tech Specs

The Giga R1 packs BLE and the power of the STM32H7, the processor used in the Portenta H7, into the accessible Mega form factor.

Read Blog
image tile

Nicla Sense

Buy Now

An intelligent board that features industrial-grade sensors, including a Bosch Sensortec BHI260AP motion sensor system with embedded AI.

image tile

Nano 33 BLE Sense

Buy Now

A low-power board with built-in BLE and Bluetooth 5, featuring temperature, pressure, humidity, light, and gestures sensors.

design challenge tile

Arduino Edge Control Board

Buy Now

Designed for precision farming applications, this control board is well suited for irrigation with modular connectivity.

Recent Discussions
Arduino Day Content
More
Recent Blogs
  • Bluetooth Terminal for HC-05, HC-06 on android devices

    Hello community. I was developed my own application for Arduino developers and today i had published it on Google Play. This app bring you flexible and configurable remote for your arduino devices via bluetooth modules HC-05, HC-06. This is free appl…
  • Atmega Pinout and Conflicts

    I'm writing this as a "Blog Post", because I did not see a way to make it a document: Which I would have preferred. I ran into a problem on the Intel Edison board, that stuck me for a while on coding, until I finally found the issue was with…
  • Am I using the 2N2222 correctly?

    This is my first use of transistors in a project. I need to control a SainSmart 16-Channel Relay Module using an Arduino 101(3v3 GPIOs). This Relay Module uses 5 vdc through Opto couplers to power the relays. The input pins on the relay board are at …
  • BMP180 Interfacing with Arduino in Depth

    This video is all about interfacing BMP180 module with Arduino. BMP180 will help us to measure environmental temperature  and pressure and by using that we can calculate the altitude which can be used in various applications like weather monitor...
Related Projects