• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Pico C/C++ Development with Visual Studio Code (VS Code): A Development Container Approach!

    shabaz
    shabaz
    Table of Contents Introduction Software Installation Configure Visual Studio Code Open a Dev Containers Project Building a Dev Containers Project Examining Project Code Revisiting the Project Running the Pi Pico project Opening Projects in a C...
    • 13 Jan 2024
  • Sounds & Visions - The Multimedia Wishlist for Arduino/Raspberry Pi

    dychen
    dychen
    Let's get creative!  In this wishlist, we're looking at multimedia accessories for the Arduino, Raspberry Pi, and other single board computers and controllers.  We're interested in anything that has to do with graphics, music, v...
    • 9 Jan 2024
  • Working with Pi Pico C/C++ Projects Easily: A Docker Approach!

    Working with Pi Pico C/C++ Projects Easily: A Docker Approach!

    shabaz
    shabaz
    Table of Contents Introduction What Is Docker? How Does It Work? What’s Required? Commands Overview Installing Docker Installing and Running the Pi Pico Ready Container Start-Up and Access the Container Download Pi Pico Project Source Code to...
    • 8 Jan 2024
  • C++ gpio library for Raspberry Pi - Pt 3: Blinky!

    C++ gpio library for Raspberry Pi - Pt 3: Blinky!

    Jan Cumps
    Jan Cumps
    An exercise to build a C++ library for the GPIO pins. The programmer can decide what underlying mechanism is used to talk to the pins. In this 3rd post, finally, a Blinky! #include "memmapdevice.h"typedef dgpio::pin<dgpio::memmapdevice> pin...
    • 7 Jan 2024
  • Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico

    Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico

    shabaz
    shabaz
    Table of Contents Introduction How Does it Work? Using the Ready-Built Code Source Code Changing the Sounds Summary Introduction This short project can be used to output WAV format sound effects for animatronic displays (such as at model train ex...
    • 5 Jan 2024
  • C++ gpio library for Raspberry Pi - Pt 2: Plug In drivers for direct register GPIO, or file system based GPIO

    C++ gpio library for Raspberry Pi - Pt 2: Plug In drivers for direct register GPIO, or file system based GPIO

    Jan Cumps
    Jan Cumps
    An exercise to build a C++ library for the GPIO pins. The programmer can decide what underlying mechanism is used to talk to the pins. In this second post, 3 mechanism are supported: register access via memmap the sysfs inter...
    • 5 Jan 2024
  • C++ gpio library for Raspberry Pi - Pt 1: Design and How To Use

    C++ gpio library for Raspberry Pi - Pt 1: Design and How To Use

    Jan Cumps
    Jan Cumps
    An exercise to build a C++ library for the GPIO pins. The programmer can decide what underlying mechanism is used to talk to the pins. In this initial release, one mechanism is supported: the sysfs interface. typedef dgpio::pin<dgpio::sysfsdev...
    • 5 Jan 2024
  • Raspberry Pico - Timers in multi-core FreeRTOS SMP ("also a double blinky")

    Jan Cumps
    Jan Cumps
    FreeRTOS Symmetric Multiprocessing (SMP) is a version of the RTOS that can schedule tasks across multiple controller cores. It has just been promoted to the main release, and supports the RP2040. In this blog post, revisit&nbs...
    • 19 Nov 2023
  • Raspberry Pico - Play with multi-core FreeRTOS SMP ("the double blinky")

    Jan Cumps
    Jan Cumps
    FreeRTOS Symmetric Multiprocessing (SMP) is a version of the RTOS that can schedule tasks across multiple controller cores. It has just been promoted to the main release, and supports the RP2040. In this blog post, I design a doubl...
    • 17 Nov 2023
  • Raspberry Pico - multi-core FreeRTOS SMP now integrated in main package

    Raspberry Pico - multi-core FreeRTOS SMP now integrated in main package

    Jan Cumps
    Jan Cumps
    Trying out multi-core FreeRTOS has now become very simple. The SMP functionality, and the Raspberry PICO example !! became part of the standard download.The organisation hasn't released a new version yet, but everything is submitted to...
    • 21 Oct 2023
  • Introducing The New Raspberry Pi 5 - 3x Faster, 2.4GHz, VideoCore VII GPU, RTC, Gigabit Ethernet, 1GB, 2GB, 4GB, 8GB RAM

    e14phil
    e14phil
    Introducing the Raspberry Pi 5 Meet the New Raspberry Pi 5! It represents a leap in performance, with many widely-requested quality of life features, including an RTC battery connector and an onboard power button!  Pre-order the R...
    • 28 Sep 2023
  • Win a Raspberry Pi 5 from the element14 Community!

    e14phil
    e14phil
    Win a Raspberry Pi 5! We have just announced the release of the amazing Raspberry Pi 5, with its 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, VideoCore VII GPU, LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch), 2.4 GHz a...
    • 28 Sep 2023
  • Raspberry Pi 5 Technical Specifications and Mechanical Drawings

    e14phil
    e14phil
    Raspberry Pi 5 Key Features: Here are the tech specs for the brand new Raspberry Pi 5: • 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache• VideoCore VII GPU• LPDDR4X-4267 SDRAM (4GB and ...
    • 28 Sep 2023
  • Raspberry Pi 5 FAQ - Frequently Asked Questions about the Raspberry Pi 5

    e14phil
    e14phil
    Raspberry Pi 5 FAQ Learn more about the Raspberry Pi 5! Will my existing case fit the new board? Do I need a new charger for the Raspberry Pi 5? What is a Real-Time Clock? What Are the Specifications for the Raspberry Pi 5?  • 2.4GHz quad-...
    • 28 Sep 2023
  • Can you run PalmOS on the Raspberry Pi RP2040?

    dychen
    dychen
    How do you run an obsolete OS on modern hardware? Figure 1: Palm TX (Source: Brusselsshrek/Wikipedia) Remember the PalmPilot? PalmPilots came out in the 90's and were one of the earliest PDAs (personal digital assistants). They were basical...
    • 21 Sep 2023
  • Your browser is slowing you down! Raspberry Pi Browsers Finding the Best performance on 32bit and 64bit Raspberry Pi OS

    gam3t3ch
    gam3t3ch
    When it comes to our browser its one of the few things we often over look. We might just be comfortable with Google Chrome or Firefox and think well I just have to deal with the slowness and random quirks with them on the Raspberry Pi.  But what...
    • 2 Sep 2023
  • Raspberry Pico C SDK: reserve a Flash memory block for persistent storage

    Raspberry Pico C SDK: reserve a Flash memory block for persistent storage

    Jan Cumps
    Jan Cumps
    When you develop firmware for a Raspberry Pico, there are cases where you want to store user data in Flash. Data that needs to survive a power-down. E.g: calibration data, user preferences, display Celsius/Fahrenheit …&...
    • 30 Aug 2023
  • Raspberry Pi Zero W to Telegram Photo Using Bot

    meera_hussien
    meera_hussien
    In this blog, I would like to share my latest tutorial or project video on the Raspberry Pi Zero W. https://youtu.be/2DAU0SU0IL8
    • 5 Aug 2023
  • Going bare metal on Raspberry Pi

    Going bare metal on Raspberry Pi

    ggabe
    ggabe
    Introduction: If you're an avid Raspberry Pi enthusiast and have explored the world of traditional Linux-based development on the platform, it's time to embark on a new adventure. In this blog post, we'll delve into the exciting realm of ...
    • 25 Jun 2023
  • Ploopy's Open Source Headphones with the RP2040

    dychen
    dychen
    Open source software is all the rage; open collaboration with every software developer on the planet has led to more secure and innovative code. But what about on the hardware side? Traditionally, hardware has been more proprietary and closed off, b...
    • 8 Jun 2023
  • How to improve my brachioGraph project - add something special

    samiboutgoulla
    samiboutgoulla
    hello everyone I made a project https://www.brachiograph.art/tutorial/construct.html brachioGraph with three servo motors and a raspberry pi, I need help to improve it, add something design thing, add something else that will make it better
    • 20 May 2023
  • 11+ Years of Raspberry Pi and the element14 Community @ Embedded World Exhibitor Forum with e14Phil and MAYERMAKES

    e14phil
    e14phil
    11+ Years of Raspberry Pi and the element14 Community @ Embedded World Exhibitor Forum Its been 11+ Years of Raspberry Pi and element14 Community, and we have had an amazing ride since this first post in 2012:  "It’s been a long time...
    • 25 Apr 2023
  • Add external SPI Flash Memory to Raspberry Pico - 5: pass STL containers as read-only parameters

    Add external SPI Flash Memory to Raspberry Pico - 5: pass STL containers as read-only parameters

    Jan Cumps
    Jan Cumps
    A projects to learn the SPI API of the RP2040 C SDK, and to use it to control an external Flash IC. In this post, I refine the m25 c++ class again. take care that an STL container is read-only when passing it to a member. Pass...
    • 9 Apr 2023
  • Trying to set my USB interface as the default using a Pi 4 and Balena Sound

    AlterKind
    AlterKind
    I see that BalenaOS detects my Komplete Audio 6 when I lsusb to check. How do I change the default output from the AUX to my KA6? Mind you, I know alsamixer is usually the answer but for some reason, I can go into alsamixer and pul up my KA6 as a sou...
    • 23 Mar 2023
  • Pi Global Shutter Camera: What's Inside the Box?

    shabaz
    shabaz
    The new Pi Global Shutter Camera (see the announcement) may be suitable for AI experimentation, so I decided to get one! I believe it should be electrically compatible with both the Pi as well as the NVIDIA Jetson Nano, so I think I can get...
    • 11 Mar 2023
<>