Code Exchange
  • Technologies
  • More
Code Exchange
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Encoders work! i2c bus operational

    SensoredHacker0
    SensoredHacker0
    Yesterday I learned that j1939 is Canbus, and that our FC6A Plus PLCs support this. Today I learned that when I plug in the PLC to the network the arduino looses control over the HMI, and the PLC doesnt have it. ..so theres some unknown networki...
    • 15 May 2026
  • Omega 5SRTC hack, and basic IO on arduino to HMI is operational.

    SensoredHacker0
    SensoredHacker0
    Im doing my on the Line challenge figured out the issues with the HMI Coms,geting readdy to write the helper functions to make the arduino PLC Server respond with the IO of the arduino.6% memory use on a Mega!well anyway all I have for pots are these...
    • 13 May 2026
  • Now possible to deploy IDEC PLC code from server of choice.

    SensoredHacker0
    SensoredHacker0
    Ok The Docs arent great, and I literally just figured this out 2 days ago. but if you have a ZLD file (the raw instruction files for IDEC PLC Code)it is now possible to deploy native instructions from the server of your choice.This includes Linu...
    • 25 Feb 2026
  • More FC6A library uses

    SensoredHacker0
    SensoredHacker0
    Yesterday I wanted to reconfigure all the PLCs in my lab with settings for a specific use case. This involves changing the values of 3 registers to make the PLCs listen to a server over DHCP. my lab has 12 FC6A plcs. and loading windLDR on ...
    • 23 Jan 2026
  • Conditional breakpoint in VSCode

    Jan Cumps
    Jan Cumps
    Sometimes, you want to have a breakpoint that only halts execution (breaks ) if a certain condition is true. My user story: I have a GPS design that receives data from satellites. Sometimes, that radio receives "not guaranteed" data. The dat...
    • 15 Dec 2025
  • modern C++: write my own function that returns true / false, and a value, part 2 (embedded friendly)

    Jan Cumps
    Jan Cumps
    what came before:  modern C++: function returns true / false, and a value or error message   modern C++: write my own function that returns true / false, and a value or error message  C++ has released a new feature: return ...
    • 4 Dec 2025
  • modern C++: initialise a static array inside a class

    Jan Cumps
    Jan Cumps
    Pre C++17 In traditional C++, if you have a class that has a static array as data member, you have to initialise that array outside of the class.  class myclass { protected: static uint myarray[4]; }; uint myclass::myarray[4]; You will typi...
    • 24 Nov 2025
  • Monitor your IDEC PLC with Maintenance Protocol using the open source library FC6A

    SensoredHacker0
    SensoredHacker0
    Maybe you work with IDEC PLCs, or maybe you have to monitor a process using them. Well, from WindLDR, that process might suck, having to monitor trends, or open multiple instances of WindLDR just to look at some select registers, there is now a ...
    • 23 Nov 2025
  • Generate Awesome ASCII ART with QAAA.py

    SensoredHacker0
    SensoredHacker0
    Hello All from rural Maine. QAAA.py is a novel drawing app, which uses  text to draw pictures. Some of y'all might have been around at a time when ASCII text was more prevalent. Well anyway, this app is designed to be cross platform tho...
    • 22 Nov 2025
  • C++ write your own stream class - part 1a: the cost of objects can be zero (embedded friendly C++)

    Jan Cumps
    Jan Cumps
    I wrote a little output stream class in a previous post:  C++ write your own stream class - part 1: output stream initial design (embedded friendly C++) . In this post, I'm adding an input stream, and an input / output stream that's su...
    • 12 Nov 2025
  • C++ write your own stream class - part 1: output stream initial design (embedded friendly C++)

    Jan Cumps
    Jan Cumps
    In C++ it's common to stream data. You write to a file using the << operator. example:  cout << "hello, world! << endl; In this blog I'm making my own minimal output stream class. Just enough code to show that it works. This co...
    • 11 Nov 2025
  • modern C++ for loop, but you still want an index

    Jan Cumps
    Jan Cumps
    C++ has a range loop. A for loop that will run over all elements in the range you give it: std::vector<int> v = {0, 1, 2, 3, 4, 5}; // ... for (auto i : v) std::cout << i << ' '; std::cout << '\n&#...
    • 5 Nov 2025
  • Reflections on Using AI in Software Development

    AngelSoto
    AngelSoto
    Context: A Practical Project Over the past days, I have been developing a Python Qt application to generate weekly meal plans for my baby and family.The project itself is not overly complex, but it has provided a valuable opportunity to reflect on so...
    • 11 Sep 2025
  • C++ moving and returning objects part 2: move and copy (embedded friendly C++)

    Jan Cumps
    Jan Cumps
    In object oriented designs, there are times when you replace an object by another. Example: when you store an object into an STL container. In a lot of those cases, you create an object, and add it. The object in the container is a cop...
    • 20 Jul 2025
  • C++ moving and returning objects part 1: object as return value (embedded friendly C++)

    Jan Cumps
    Jan Cumps
    You may read guidelines that say: "never use an object as return value of a function. Because of performance reasons". Because the object is copied into the receiving variable when returning from the function call. That was true in C++...
    • 19 Jul 2025
  • C++ 3 way compare

    Jan Cumps
    Jan Cumps
    task: Let's say that you are writing a C++ class, where the objects have to be sorted or compared. In classic C++, you 'd write an operator overload for <, <=, == , !=, >= and >. In modern C++, you can get all that fun...
    • 15 Jul 2025
  • GCC 15.1 for Windows is available

    Jan Cumps
    Jan Cumps
    If you're interested to try out the latest C++26 options: The Windows port for GCC 15.1 is available for download.I installed GCC 15.1.0 (with POSIX threads) + MinGW-w64 13.0.0 UCRT - release 2. To install, download the zip file, ...
    • 30 Jun 2025
  • C++ friend functions

    Jan Cumps
    Jan Cumps
    For an embedded design, I made a featherweight class. A C++ construct that used no more data or code size than a traditional C design. class command { public: inline command(uint32_t steps, bool reverse) : cmd_(steps << 1 |...
    • 18 May 2025
  • New CMake library link option $<COMPILE_ONLY:LIB>

    Jan Cumps
    Jan Cumps
    CMake has an easy way to get access to libraries headers and source: target_link_libraries(your_lib, some_lib). Where your_lib is the library you are developing, and some_lib is a library you depend on. Ideal if you are using a library, and...
    • 19 Apr 2025
  • embedded C++: manage a resource with a tiny* object

    Jan Cumps
    Jan Cumps
    *tiny like in: 0 bits of data, 0 code instructions added, 0 clock ticks scenario: you have a resource that needs to be initialised before use, and deactivated when done. We usually do that by calling some code before the actions, and some code after ...
    • 5 Apr 2025
  • embedded C++: add cheap bitwise conversion to a register structure

    Jan Cumps
    Jan Cumps
    This blog is based on real world work. I'm controlling a TI DRV8711 stepper motor controller via SPI. I need to modify 16-bit registers of that IC. TI provided a header file with register definitions, and code to convert that struct to a 16 bit ...
    • 30 Mar 2025
  • modern C++: restrict templated types with concept

    Jan Cumps
    Jan Cumps
    In C++, templates allow you to write generic code, that can handle many types. But almost always, there will be types you can't handle. In my case, I have a callback manager that supports functions that return a void, a number, a bool or a class...
    • 10 Mar 2025
  • C++ classes and operators

    Jan Cumps
    Jan Cumps
    This is a "classic C++" post, something that's been part of the language since conception: How to use an operator in your class design. I developed a callback class. Your "gizmo that needs to callback something" would hold an instance of that class (...
    • 9 Mar 2025
  • let CMake fetch your build dependencies

    Jan Cumps
    Jan Cumps
    When you work on a project, you often rely on external libraries and source code. If you use CMake as your build tool: it can download the artifacts for you. And make them available during build. By using FetchContent. use case: your pro...
    • 9 Mar 2025
  • modern C++: write my own function that returns true / false, and a value or error message - part 1 (embedded friendly)

    Jan Cumps
    Jan Cumps
    I'm experimenting with new C++ constructs. GCC 15 implements an interesting concept of the C++26 standard: A function can return a status, and either a value or an error message. In a previous post I tested one of C++ standard function...
    • 1 Mar 2025
>