Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • What can you do with a 500 MHz MCU? – Join the Crossover Code Challenge today!

    kjachim
    kjachim
    Launched in October, the i.MX RT1010 crossover MCU further expands NXP’s popular i.MX RT series and introduces the world to the next generation of low-cost, high-performance MCUs.  With features such as Flex PWM for motor control, S/PDIF fo...
    • 9 Dec 2019
  • Renesas RX65 Envision Kit - part 9: UART

    Jan Cumps
    Jan Cumps
    Preface: It seems that it's not possible to use the debug USB port as debugger and serial port at the same time. I'm evaluating the Renesas RX65N MCU EV Kit.In this post: Serial communication - UART - SCI. The RX family has 12 serial periph...
    • 8 Dec 2019
  • Renesas RX65 Envision Kit - part 8: DMA

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post: A Direct Memory Access example.source: application  note R01AN2063EJ0220 DMAC Module Using Firmware Integration Technology  The Example - DMA and ADC The Renesas DMA exampl...
    • 7 Dec 2019
  • Renesas RX65 Envision Kit - part 7: Blinky with FreeRTOS

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post: A Blinky, with the FreeRTOS managing the clock. Create the Project As usual, use Blog #1 to create the project.The only extra action is to select FreeRTOS while going through the pro...
    • 1 Dec 2019
  • Renesas RX65 Envision Kit - part 6: Software SHA

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post,  I'm reviewing the SHA options.source: Renesas SHA package documentation SHA Hardware Accelerated vs Software The RX family has models that come with a hardware accelerator for ...
    • 1 Dec 2019
  • Renesas RX65 Envision Kit - part 5: DAC

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post,  I'm reviewing the Digital Analog Converter Adapt the Envision Kit The RX65N has two DAC channels. On the controller, they are PO3 and P05. source: Renesas datasheet T...
    • 30 Nov 2019
  • Datasheets, Schematics and Application Notes in Eclipse

    Jan Cumps
    Jan Cumps
    When you're developing for a microcontroller or IC, it's handy to have the documentation available at your fingertips.Many manufacturers give strange names to these documents. The Renesas RX65N that I'm currently working with has a datash...
    • 29 Nov 2019
  • Renesas RX65 Envision Kit - part 4b: Low Power - Software Standby

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post,  I'm reviewing the Software Standby power save mode  Software Standby Mode This is a lower consumption mode than the Sleep mode in post 4a.I'm doing the blogs a little out ...
    • 28 Nov 2019
  • Renesas RX65 Envision Kit - part 4a: Low Power - Sleep

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post,  I'm reviewing the Sleep power save modesource: application note R01AN4347EJ011: Examples of Transitioning to RX651 Groups Low Power Consumption Modes  Evaluation Kit Power Doma...
    • 27 Nov 2019
  • Renesas RX65 Envision Kit - part 3: Port an example from Renesas toolchain to GCC

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post,  I'll port the LCD driver example from the Renesas proprietary CC-RX   Renesas offers a GCC toolchain that can build firware for the RX65 family. I have been using it for m...
    • 24 Nov 2019
  • Renesas RX65 Envision Kit - part 2b: Blinky with Timer and Interrupt

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post: Expand the Blinky example with a timer and interrupt.This time it's a real blinky. The code to poll the user button is removed and the led is controlled by one of the onboard timers. &nbs...
    • 23 Nov 2019
  • Renesas RX65 Envision Kit - part 2a: Blinky with GCC Toolchain

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post: A Blinky, with the GCC toolchain.It's not a real blinky - it's a switchy. The User LED is on when the User Button is pressed.A Morse code trainer .  Create the Project In the pr...
    • 23 Nov 2019
  • Renesas RX65 Envision Kit - part 1: Create an Empty Project

    Jan Cumps
    Jan Cumps
    I'm evaluating the Renesas RX65N MCU EV Kit.In this post: how to start a project in the Renesas IDE e2 Studio.I'll use the Renesas CCRX toolchain.  Start a Project File -> New C/C++ Project -> Renesas RX -> Renesas CC-RX C/C++...
    • 23 Nov 2019
  • Port an MBED design to non-MBED - Phase 3: InterruptIn Class and example

    Jan Cumps
    Jan Cumps
    The port of the MBED InterruptIn is complete.In this blog you can see the internals of this class and how to set up configuration and handling. My port is for a Hercules TMS570LC43. I use the HAL utility and api for that controller where possibl...
    • 16 Nov 2019
  • Storage Insights #7 - SD Card Technology Advantages

    drozwood90
    drozwood90
    In Storage Insights #6 we dove deeper into SATA (Serial ATA), discussing layering and compatibility. In Storage Insights #7 we have a link to a video presentation that details several technology advantages of industrial SD cards.SD cards, or Secure D...
    • 15 Nov 2019
  • Port an MBED design to non-MBED - Phase 2b: DigitalOut Class and Blinky example

    Jan Cumps
    Jan Cumps
    The port of the MBED DigitalOut is complete.In this blog you can see the internals of this class and how to create a blinky. Blinky #include "includes.h" // this is the include that replaces MBED.h for ported applications. // st...
    • 12 Nov 2019
  • Port an MBED design to non-MBED - Phase 2a: DigitalOut Class Constructor

    Jan Cumps
    Jan Cumps
    I've ported the MBED DigitalOut class to the Hercules controller that I'll be using.It could be any controller or SBC, but having one example makes it tangible. I've try to do this with as limited as possible impact to the SemTech library. That ...
    • 11 Nov 2019
  • Port an MBED design to non-MBED - Phase 1: compile without errors

    Jan Cumps
    Jan Cumps
    There are many good MBED examples. It's a popular platform, supported by many manufacturers.Here's my story on how to port one of those excellent MBED example program to another platform. The program I want to port is the SemTech LoRa Ping-Pong ...
    • 9 Nov 2019
  • Hercules Safety Microcontroller: Use C++ with HALCoGen C Projects

    Jan Cumps
    Jan Cumps
    TI Hercules microcontrollers are "functional safety" devices for automotive, industrial and medical use.When you create a new firmware project for this family, you use the TI HALCoGen tool to configure the peripherals and create the source....
    • 9 Nov 2019
  • Microsoft’s Project Silica can Store Data on Glass for Hundreds of Years

    Catwell
    Catwell
    The new storage technology stores data in quartz glass using laser light, which burns voxels into the medium that hold multiple bits of information. (Image credit: Microsoft)  A recent collaboration by Microsoft and Warner Brothers resulted in s...
    • 7 Nov 2019
  • Newly Developed Electroadhesive Stamp Could Push Miniaturization to New Levels

    CharlesGantt
    CharlesGantt
    If you have ever populated a PCB with lots of SMD components by hand, you know how frustrating and time-consuming it can be. Thankfully, when its time to move into production we employ special robots called “pick and place” machines to do the job for...
    • 29 Oct 2019
  • Arm Provides Custom Instruction Support for Their Embedded CPUs

    Catwell
    Catwell
    Arm will offer support for custom instructions for their ARMv8-M embedded CPUs targeted at embedded and IoT applications. (Image credit: Arm)  During this year’s TechCon event in Santa Fe, Arm announced it would start supporting custom instructi...
    • 22 Oct 2019
  • Graphene Turns 15 and Promises to Change the Future

    Catwell
    Catwell
    (Image credit: AlexanderAIUS via Wikipedia)  Graphene is one of the world’s most robust materials even though its only 1-atom thick, and coupled with its highly conductive nature, one of the most sought out materials for a myriad of applications...
    • 15 Oct 2019
  • Engineers From MIT Develop New Advanced Microprocessor Using Carbon Nanotubes

    CharlesGantt
    CharlesGantt
    For several years now, the microprocessor manufacturing world has been coming to grips with the fact that Moore’s law no longer governs the rate at which we are able to shrink transistors in size. This has led to researchers worldwide rushing to find...
    • 26 Sep 2019
  • Cortex-M debugging and automated testing using Rasp-Pi

    kamtar
    kamtar
    I have decided to write about the usage of Raspberry pi as both wireless programmer/debugger and tool for automated testing for Cortex-M MCUs. There are few articles and tutorials but still, this topic's online coverage is rather poor considering its...
    • 12 Sep 2019
<>