Eye On Intelligence Challenge
  • Challenges & Projects
  • Design Challenges
  • Eye On Intelligence Challenge
  • More
  • Cancel
Eye On Intelligence Challenge
Blog
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Eye On Intelligence Challenge to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • ADAS and Vehicle Monitoring System – Training YOLOv3 and inference on DPU

    vmate
    vmate
    With a sufficiently large dataset created, the next step is training a model to run on the DPU. I couldn’t find a full list of supported models for the DPU and its corresponding toolchain, but YOLOv3 is confirmed to be working, so I will be usi...
    • 16 Nov 2024
  • Z7_Color_AID Blog #4: Architecture Discussion of Z7_Color_AID

    flyingbean
    flyingbean
    Table of Contents Z7_Color_AID Project Background Z7_Color_AID Project Introduction Next Step of the Design Challenge References Z7_Color_AID Project Background Detecting color is important for a lot of applications.  In self-driving cars, A...
    • 16 Nov 2024
  • ADAS and Vehicle Monitoring System – Object Recognition, Neural Network Training, DPU

    vmate
    vmate
    The core of the ADAS system will be an Object Recognition model, detecting traffic signs, lights, and speed limits. The two main features the blogs will be focusing on are traffic light change notifications and speeding warnings. The Dataset For tra...
    • 15 Nov 2024
  • Blog #5: Third Eye for Blind - Training and Optimizing YOLOv3 Model for Object Detection

    Blog #5: Third Eye for Blind - Training and Optimizing YOLOv3 Model for Object Detection

    taifur
    taifur
    This blog aims to create a custom YOLOv3 model for object detection. But before going into the details I wish to check the web camera that came with the kit using the Arty Z7 board to confirm everything is working as expected. I created a Python note...
    • 15 Nov 2024
  • Person Detection with yolo #5 Eye on With USB Camera in Pynq Virtual Environment

    fyaocn
    fyaocn
    #5 Eye on With USB Camera in Pynq Virtual Environment Table of Contents 1 Image Process and Video Capture with USB camera 2 Test Pynq I2C overlay with Pmod ALS light sensor 3 USB camera for Video and Image 4 Yolo and Person Detection 5 Summary 1 ...
    • 15 Nov 2024
  • Person Detection with yolo #4 Pynq Virtural Environment

    fyaocn
    fyaocn
    #4 Pynq Virtural Environment  Table of Contents 1 Pynq is virtual environment 2 Arty Z7 and pynq overlay 3 Pynq setup in Arty Z7 4 iPython and coding 5 Summary 1 Pynq is virtual environment Pynq is clever designed to support&nbsp...
    • 14 Nov 2024
  • Person Detection with yolo #3 Vitis AI and DPU behind Arty Z7

    fyaocn
    fyaocn
    #3 Vitis AI and DPU behind Arty Z7 Table of Contents 1 DPU behind Arty Z7 2 Vitis AI to DPU 3 Go deep into DPU  4 Model for DPU  5 Summary  1 DPU behind Arty Z7 Vitis AI is Integrated Development Environment that fasilating ML deve...
    • 13 Nov 2024
  • Person Detection with yolo #2 Software-->from Vivado to Vitis to Petalinux

    fyaocn
    fyaocn
    #2  Software-->from Vivado to Vitis to Petalinux Table of Contents 1 Diversity software toolsets 2 Getting start with Vivado 3  Getting to Vitis 4 Build Petalinux Projects 5 Three Pathway to Eye Intelligence in Arty...
    • 7 Nov 2024
  • Person Detection with yolo #1 Vision AI with Arty Z7 for Person Detection

    fyaocn
    fyaocn
    #1  Vision AI with Arty Z7 for Person Detection Table of Contents 1 Description of Person Detection with yolo 2 Vision AI with Arty Z7  3  Arty Z7 and USB camera 4 Unboxing with out-of-factory Image 5 Challenges and O...
    • 6 Nov 2024
  • Eye On Intelligence Challenge - a Birds-Eye view - Tensorflow and Hummingbirds

    rsc
    rsc
    Tensorflow: After spending many hours trying to shuffle and reformat the bird database into something that Tensorflow would be happy with, I gave up.  I found another bird database that already had each .jpg file sized the same, and all the imag...
    • 4 Nov 2024
  • Blog #4: CNN HW Accelerator for Handwriting Recognition - Neural Network Architecture for Handwritten Digit Recognition

    yesha98
    yesha98
    Hardware Architecture of the Neural Network A DMA feeds the neural network's input using the AXI Stream protocol. This protocol is very efficient in handling large data using a simple handshake, as depicted below. The figure above shows the ba...
    • 4 Nov 2024
  • Z7_Color_AID Blog #3: PYNQ Framework: Library and Overlay

    flyingbean
    flyingbean
    Table of Contents PYNQ Framework Brief Learning PYNQ Overlay from Supported IPs, PS/PL Interface and PL Control A Simple PYNQ Overlay Project Journey Future Path on PYNQ/Z7_Color_AID Project References PYNQ Framework Brief PYNQ includes major com...
    • 4 Nov 2024
  • FruitVision Scale - FPGA HX711 driver

    Blog 4 - FruitVision Scale - FPGA-Based HX711 Driver for Precision Weighing with AMD PYNQ

    javagoza
    javagoza
    Introduction In my previous blog for the Eye On Intelligence Design Challenge, I used the Zynq analog-to-digital converter (XADC) to sample the analog signal from a Wheatstone bridge load cell, amplified with an AD8226 instrumentation amplifier. The ...
    • 1 Nov 2024
  • Blog #3: CNN HW Accelerator for Handwriting Recognition - Defining the Neuron for Handwritten Digit Recognition

    yesha98
    yesha98
    Defining the Neuron Weighted Sum and Bias For a neuron in a given layer, the output before activation (also known as the pre-activation value) is calculated as follows: Activation Function Application After computing the weighted sum z, the neuron a...
    • 1 Nov 2024
  • ADAS and Vehicle Monitoring System - 4G, Video Streaming, Canbus Integration

    vmate
    vmate
    In this blog, I'll go through setting up the communications hardware, and software setup for video streaming and data logging. Internet Connectivity I decided on using an EM7455 WWAN card, typically used in laptops, to provide the system with in...
    • 31 Oct 2024
  • Blog #2: CNN HW Accelerator for Handwriting Recognition - Introduction to CNN for Handwritten Digit Recognition

    yesha98
    yesha98
    Background For handwritten digit recognition, Convolutional Neural Networks (CNNs) are the most effective type of neural network, as they excel at identifying patterns and spatial hierarchies in image data. CNNs have become the standard approach, esp...
    • 30 Oct 2024
  • Blog 5 - Petalinux base implementation.

    pandoramc
    pandoramc
    A good way to work is to use of an Operating System. In this case, the platform provided by AMD is a distribution called Petalinux. For a general purpose computing systems there are no problems selecting distributions or wide range of processors avai...
    • 27 Oct 2024
  • Blog 4 - Async processing

    pandoramc
    pandoramc
    Many computer architectures contains more than a processor, consequently, the developer must change the programming perspective in order to use each available resource in the platform. This time, the XC7Z020 SoC has a Dual-core ARM Cortex-A9 in the H...
    • 22 Oct 2024
  • Z7_Color_AID Blog #2: Reproduce PYNQ Image on Ubuntu 20.04

    flyingbean
    flyingbean
    Table of Contents Motivation to Rebuild Pynq_Z1 Image Rebuild Pynq_Z1 image Test Rebuilt Pynq_Z1_v3.0.1 Image Future Path on PYNQ/Z7_Color_AID Project References Motivation to Rebuild Pynq_Z1 Image Porting a supported PYNQ platform from PYNQ gith...
    • 21 Oct 2024
  • Sign Language Interpreter Blog 1: Project Overview and Kit Unboxing

    cbohra00627
    cbohra00627
    IntroductionI participated in The Eye on Intelligence challenge hosted by Element14 and luckily got selected as an official challenger. I have background in VLSI and like to play with Electronics items and boards in my free time. For this chall...
    • 19 Oct 2024
  • Blog #4: Third Eye for Blind - Object Detection using ZYNQ DPU and YOLOv3

    Blog #4: Third Eye for Blind - Object Detection using ZYNQ DPU and YOLOv3

    taifur
    taifur
    My project "Third Eye for Blind" is based on object detection. So, what is object detection? Object detection is a computer vision technique that allows us to identify and locate objects in an image or video. With this kind of identificatio...
    • 16 Oct 2024
  • FruitVision Scale

    Blog 3 - FruitVision Scale - Weighing strategies with load cells using the Digilent Arty Z7

    javagoza
    javagoza
    Introduction This is my third entry in The Eye on Intelligence design challenge. In the previous two, I introduced the Digilent Arty Z7 development board and the PYNQ development framework. PYNQ enables the creation of designs in adaptive computing e...
    • 16 Oct 2024
  • Blog Post 1 : Eye On Intelligence Challenge - The Problem Statement

    aswinvenu
    aswinvenu
    Introduction     Running is one of the world most popular and favorite activity for maintaining fitness. The sport involves both aerobic and anaerobic metabolism in different proportions. It is estimated that total of 621Million people...
    • 15 Oct 2024
  • Z7_Color_AID-Blog#01: First Impression of PYNQ on Arty-Z7-20

    flyingbean
    flyingbean
    Table of Contents Arty-Z7-20 OOB Resources to Learn PYNQ Framework Bring Arty-Z7-20 Up into Running References Arty-Z7-20 OOB It is my first time to use PYNQ on AMD® FPGA platform.  I did try to deploy PYNQ on Digilent MiniZed last year....
    • 13 Oct 2024
  • Eye On Intelligence Challenge - a Birds-Eye view - Bird Database

    rsc
    rsc
    I missed some time on this project because of travel for work, but I'm back and ready to proceed.... There are several bird databases available for training the ML model so I'm not going to try and make my own. These are some of the ones I fo...
    • 11 Oct 2024
<>