Project14
  • Challenges & Projects
  • More
Project14
Show and Tell!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Show and Tell, Share a project you previously created or you are building right now
Show & Tell, share a project you previously created or you are building right now
  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Audio transmission using LED light

    Audio transmission using LED light

    strb
    strb
    This project dates back to the last year of my bachelor degree. The professor for the "Electronic laboratory" course decided to give a twist to final examination allowing two options: standard examination or a project contest. Rules were si...
    • 23 Aug 2026
  • Ink Bot the Vertical Pen Plotter

    Ink Bot the Vertical Pen Plotter

    nimion_art
    nimion_art
    Check out this drawing machine that I built and programmed from scratch using an Arduino Uno, stepper motors, and more!
    • 21 Aug 2026
  • Electronic vintage weather station

    Electronic vintage weather station

    Spain_mtg
    Spain_mtg
    Electronic vintage weather station    In the past, some houses had small weather stations that showed the data of humidity, atmospheric pressure and temperature that were in that area by means of spheres, these spheres were framed in tables...
    • 18 Aug 2026
  • Building the Brains of a Home Beer Canning Machine

    Building the Brains of a Home Beer Canning Machine

    Drodbar
    Drodbar
    From a spare Arduino and a breadboard to a custom PCB controlling valves, sensors and the full canning cycle Project at a glance • Controller: Arduino Nano • Outputs: four Airtac 4V210-08 electro-pneumatic valves • Sensor: Baumer...
    • 18 Aug 2026
  • Q-Aid enclosure 3D render designed in Autodesk Fusion, showing camera cutout, ultrasonic sensor holes, OLED window and touch zone

    Q-Aid: The Clip-On AI Badge That Runs Fully Offline

    ElleX
    ElleX
    Q-Aid is a clip-on wearable AI companion badge built entirely around the Arduino UNO Q's dual-brain architecture — the Qualcomm QRB2210 running local AI on Linux, paired with the STM32U585 MCU for real-time sensor control. Everything runs f...
    • 18 Aug 2026
  • Eco Classroom

    Eco Classroom

    redcharly
    redcharly
    Eco Classroom Table of Contents Eco Classroom Introduction UNIHIKER K10 Programming K10 The project Introduction Hi, I'm Carlo, and I'd like to share my experience with a very interesting board, the UNIHIKER K10. I'm a middle school teacher an...
    • 17 Aug 2026
  • pcb_round_watch

    LumiDial: a 72-LED Analog Wristwatch Powered by ATmega328

    taifur
    taifur
    Introduction LumiDial is a custom-built wristwatch that blends classic analog style with modern LED technology. Instead of using physical hands, it uses 72 SMD LEDs arranged in a circular layout — 60 LEDs to indicate seconds and minutes, a...
    • 14 Aug 2026
  • Diagno V1 in action

    Diagno — The Four-Probe Handheld That Measures, Generates, and Sniffs Almost Anything

    thegrgelectric
    thegrgelectric
    I would like to proudly present my battery-powered, RP2040-based handheld with a color screen and four reconfigurable test probes that measures voltage, resistance, frequency, and logic signals — and can just as easily generate PWM, drive ...
    • 10 Aug 2026
  • ESP32+NRF24 based walkie talkie

    ESP32+NRF24 based walkie talkie

    Nanucek
    Nanucek
    ESP32 nRF24 Walkie-Talkie (Main Description) This project is a wireless communication terminal built on the ESP32 microcontroller, utilizing the nRF24L01 2.4GHz transceiver module for data transmission. The system features a 0.96" I2C OLED display to...
    • 8 Aug 2026
  • Journey of an Autonomous hunter robot and a Stygian Witch Eye

    robogary
    robogary
    For interesting STEM demonstrations at schools, I had built a small hobby robot called the Orange Giraffe Hunter. Its job was to look around , lock in, and chase down a plastic Orange Giraffe     The prototype build used an Arduino Uno...
    • 8 Aug 2026
  • Analog Soul, Digital Heart: A World-War II Emergency Phone

    Analog Soul, Digital Heart: A World-War II Emergency Phone

    saturn_rings
    saturn_rings
    The inspiration Let's be honest, our grandparents hate smartphones. They find it hard to navigate through menus, forget where the emergency button is, and often want nothing to do with modern technology. On top of that, the world is full of electroni...
    • 5 Aug 2026
  • Compact RPi CM4 based Home Assistant System

    ralphjy
    ralphjy
    Introduction I'm currently waiting to receive the hardware for the Raspberry Pi Compute Module 5 Development Kit RoadTest.  My motivation for applying for that roadtest is to replace a Home Assistant (HAOS) home automation system that I have...
    • 4 Aug 2026
  • PLC with PSoC

    PLC with PSoC

    Em0ke
    Em0ke
    This PLC board is designed using a Cypress System-on-Chip (SoC) microcontroller for industrial automation and embedded control applications. The Cypress SoC integrates a microcontroller with programmable analog and digital peripherals on a single chi...
    • 28 Jul 2026
  • A.E.G.I.S. Advanced Engineering Gear for Intelligent Support. A Robotic Arm!

    A.E.G.I.S. Advanced Engineering Gear for Intelligent Support. A Robotic Arm!

    AwesomeApple1
    AwesomeApple1
    AEGIS is a fully custom-designed robotic arm that I designed, 3D printed, assembled, and programmed from the ground up over the past month. My inspiration came from JARVIS in Iron Man—the idea of building an intelligent robotic assistant that c...
    • 25 Jul 2026
  • Green pixelated camera output from a Raspberry Pi

    Station 202: a camera that throws the image away

    apn201
    apn201
    A Raspberry Pi 3 and a broken camera become a generative monitor that renders my desk as green pixels - and never lets a real image leave the device.
    • 29 Jun 2026
  • Too-slow-to-load-img:(

    CuteBit Robot

    arjunkulkarni
    arjunkulkarni
    The Expressive AI Desktop Robot CuteBit is an open-source, voice-controlled AI robot that combines a powerful Local LLM "Brain" (running on a host PC) with an expressive ESP32 "Body". Unlike standard voice assistants, CuteBit has ...
    • 25 Jun 2026
<