Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Connect to AVNET iotconnect.io with Node-RED - part 10: Trusted Platform Module (TPM) Security
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 22 May 2021 1:46 PM Date Created
  • Views 3338 views
  • Likes 8 likes
  • Comments 6 comments
  • raspberry
  • security
  • avnet
  • smartedge
  • trusted_platform_module
  • iot
  • tpm
Related
Recommended

Connect to AVNET iotconnect.io with Node-RED - part 10: Trusted Platform Module (TPM) Security

Jan Cumps
Jan Cumps
22 May 2021

AVNET's iotconnect.io cloud platform is an online service that you can use to send data to, and then show it on a dashboard. In this blog series I'm learning how to talk to it with Node-RED.

In this post: authentication with a hardware support: Trusted Platform Module (TPM) sign-on.

image

Several of the previous posts work on generic Raspberry Pi, BB, ... . This one is different.

You need hardware that supports TPM. I'm using the Avnet SmartEdge IIOTGateWay. It has an Infineon SLB9670SLB9670 (datasheet) IC on the pcb. This TPM module has a unique ID (+Endorsement Key (EK) and EK certificate). And it's supported by Linux kernel. See here for a breakout post: Infineon SLx9670 Trusted Platform Module (TPM) for IoT Security.

 

In essence, what happens in this post, for hardware and software, is identical to this post on GitHub, but on the SmartEdge, this is part of the out-of-box setup. Infineon has a module for Raspberry Pi that gives the same experience.

 

This is recent functionality. TPM is supported in the Python SDK since the first release of the SmartEdge.

I'm using a pre-release of the Node-RED modules here. Production release is imminent.

 

Scenario:

 

Register a TPM enabled device on IoTConnect portal, and let it connect and share sensor data.

 

Together with part 8b and later of this series (CA signed certificates), TPM authentication is a decent choice for industrial applications.

And the scenario isn't very different. CA Signed and TPM security both rely on certificates. CA Signed via software, TPM via a hardware module.

 

The TPM approach uses 3 functions of the Infineon chip:

  • get the unique identification
  • retrieve an endorsement key (EK, equivalent to public key), that can be used to register the device on IoTConnect cloud.
  • use the on-silicon key to validate sign-on.

 

Why TPM?

CA Signed and TPM are both strong solutions.

An advantage of TPM is that you can't accidently share the private key because it can't be retrieved from the IC.

An advantage of CA based authentication is that it doesn't need additional components to the BOM (this may become less of an issue when microcontrollers and processors come with on-board TPM).

Provisioning can be automated for both solutions.

This is one intrusion vector less. Software attacks to retrieve the private key will not work.

 

Steps:

 

I am assuming at this point that you have a Linux box with TPM support. See the header block of this post for details.

Like the previous solution, you can script the provisioning via an REST API, but I'm doing the steps manually here.

 

Create a template that supports TPM authentication

 

image

I've created a number of templates in this series. Everything is the same, except that this time I select TPM as Authentication Type.

Like the other examples, I create the attribute.

 

image

I've also created a longitude and latitude attribute. That's for later, when I'm going to show the portal's capability to show a device on a map.

 

Provision a device

 

The keys to register a TPM on IoTConnect, are ihe unique ID of the hardware TPM and the Endorsement key of that module.

IoTConnect cloud runs on Azure, and the Azure utility tpm_device_provision is used to get that data.

Source code is available on GitHub. On the SmartEdge, it's installed out of box.

 

The utility uses the Linux TPM driver to get the info, and can be executed from the command line:

 

yes 2>/dev/null|/opt/avnet-iot/iotservices/tpm_device_provision

 

image

The output has all info I need. Not in a friendly way to collect from a command line, but the Avnet Python samples show how you can retrieve the relevant data.

 

id_ek = cmdline("yes 2>/dev/null|/opt/avnet-iot/iotservices/tpm_device_provision")
# ...
            lines = id_ek.splitlines()
            uniqueId = mystr(lines[3], 'utf-8')
            EndorsementKey = mystr(lines[6], 'utf-8')

 

The Avnet example then uses the REST api to provision the device. Here's the same process via the portal:

image

 

Node-RED Config and Test

 

image

 

On the device's Node-RED flow, you have to set the Registration Id from the previous step as unique id.

Like all previous posts, the CPID is retrieved from the IoTConnect portal.

The Scope ID is a value you also get from Avnet when registering. For trial subscriptions, you can usually find it back in the IoTConnectSDK.conf.default they provide.

That is it. The rest of the flow is exactly the same as in all previous posts.

 

When you enable the flow, you should see the green embelishment and Connected label under the IoTConnect node.

image

 

As usual with security, the end result doesn't look spectacular.

The real power is behind the scenes: hardware based authentication.

 

 

The Python SDK with On Semiconductor RSL10 BLE article seriesIndustry
part 1: overview and goal
part 2: WiFi Provisioning
part 3: Adding a Module (RSL10)
part 4: Talk BLE to the On Semi RSL10 Sensor Kit
part 5: A Cloud User Experience Example
part 6: Register as a Gateway Device
part 7: Register a Gateway and Client Devices
part 8: Get BLE Image from Camera and Send to Cloud
The NODE-Red SDK article seriesIndustry
part 1: overview and goal
register a Thing and connect to IoTConnect.io cloud
part 2: create an account and log on to the portal
part 3: set up the thing and its interface in the cloud
part 4: set up Node-RED and first exchange
interact with IoTConnect.io cloud
part 5: online dashboard
part 6: rules and alerts
part 7: messages and commands from the cloud
safer connections with certificates
part 8a: safer connect with Self Signed Certificates
part 8b: safer connect with CA certificatesY
commercial and industrial scale: outsource certificate generation and programming to subcontractors and suppliers
part 9a: Outsource Certificate Signing in IIoT Supply ChainY
part 9b: IIoT supply chain and Certificates - Create Ca Root certificate, Load to IoTConnect Cloud and ValidateY
part 9c: IIoT supply chain and Certificates - Create an Intermediate CA Certificate for your SubcontractorY
part 9d: IIoT supply chain and Certificates - Subcontractor Generates a Thing Certificate for Your DeviceY
part 9e: IIoT supply chain and Certificates - Test!Y
commercial and industrial scale: Trusted Platform Module (TPM) Authentication
part 10: Trusted Platform Module (TPM) SecurityY
Infineon SLx9670 Trusted Platform Module (TPM) for IoT SecurityY
Infineon Trust Platform Module + Raspberry Pi 3 B - Review
part 11: Act as Gateway with Clients
The Automate Device Provisioning and Cloud Configuration article seriesIndustry
Automatic Provisioning with REST APIY
  • Sign in to reply
Parents
  • scottiebabe
    scottiebabe over 2 years ago

    Nice work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 2 years ago

    Nice work!