Project14
  • Challenges & Projects
  • More
Project14
Make a Connection
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Show and Tell, Share a project you previously created or you are building right now
Show & Tell, share a project you previously created or you are building right now
  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Using LoRa for remote communication

    redcharly
    redcharly
    Introduction The project I wish to propose stems from my curiosity about the LoRa protocol, which has always fascinated me due to its ultra-low power consumption and long-range capabilities. I built a communication system consisting of several compon...
    • 28 Sep 2026
  • Car Racing Gaming Console

    misaz
    misaz
    Hello Element14 community. As part of “Make a Connection” Project14 competition I made a SuperTuxKart racing console using Arduino Uno Q, Meccano like building set, my own gyroscope and accelerator shield, Linux driver and bunch of python...
    • 27 Sep 2026
  • Today's Adventure

    Today's Adventure

    PlatypiMaster
    PlatypiMaster
    I developed Today's Adventure to maximize the simple but elegant nature of e-ink displays. It turns weather, time and seasonal context into a plan for the day. What started as a need for accurate local weather evolved into a system that hel...
    • 27 Sep 2026
  • Thumbnail Image

    MorseMatrix - Simple Morse Code Machine

    Shishir
    Shishir
    Project Overview MorseMatrix is a standalone, real-time hardware Morse code decoder built on an Arduino Uno Q Single Board Computer with a built-in LED matrix. It turns the morse code entered through physical button presses into readable text by...
    • 27 Sep 2026
  • Two Handoff wristbands side by side

    Handoff: shake hands, share contacts

    rahuljeyaraj
    rahuljeyaraj
    Shake hands and swap contacts. The card goes from one wristband, through the two people holding hands, to the other band, and into their phone.
    • 27 Sep 2026
  • Send some water to your plants from anywhere in the world

    Send some water to your plants from anywhere in the world

    embeddedguy
    embeddedguy
      Table of Contents   Introduction and Motivation Hardware Requirements  Camera Remote access ESP-Rainmaker configurations Rainmaker Software Automation HaT mini  Automation HaT Wiring Raspberry Pi Configurations Remote a...
    • 27 Sep 2026
  • thumbnail

    EyeLink — A Wheelchair You Drive by Blinking

    khadri
    khadri
    https://youtu.be/VDHrHypaC9s Head Tilt + Eye Blink + Wireless Control I built EyeLink, a working prototype of a hands-free wheelchair control system that combines head movement and eye-blink confirmation to control a small motorized wheelchair platfo...
    • 27 Sep 2026
  • Greenhouse monitoring and controlling system

    Greenhouse monitoring and controlling system

    jelektro
    jelektro
    Introduction and Project Concept Modern agriculture and smart horticulture face constant challenges: optimizing resource utilization, maintaining precise environmental parameters, and minimizing human intervention in repetitive tasks. Greenhouses req...
    • 26 Sep 2026
  • Health and Activity Monitor

    Health and Activity Monitor

    jelektro
    jelektro
    This project presents the design and implementation of an intelligent wearable health assistant built around the Nordic Semiconductor nRF5340-DK development platform. The system integrates the MAX30100 pulse oximeter and heart-rate sensor together wi...
    • 26 Sep 2026
  • 446MHz Tape Measure Yagi

    shreaypatel2
    shreaypatel2
    The Concept When I saw the Make a Connection theme, I noticed many projects were utilizing Wi-Fi, Bluetooth, and IoT clouds. As an electrical engineering student currently exploring different domains of the field, I’ve recently found myself f...
    • 25 Sep 2026
  • MorseDecoder

    Full Duplex Morse Code Decoder

    VK2EJH
    VK2EJH
    Morse Code is not dead. Here is my project to use 2 BBC micro:bits and a laptop to send Morse Code in both directions whilst also decoding Morse Code sent from both ends using button A or a proper key. Step 1 upload the code using the Python Programm...
    • 25 Sep 2026
  • Energy Harvesting from low temperature waste heat via Thermoelectric generators

    Energy Harvesting from low temperature waste heat via Thermoelectric generators

    soumyabrata
    soumyabrata
    This work develops an integrated thermoelectric energy-harvesting system for low-grade waste heat. Because a thermoelectric generator (TEG) operating at a small temperature difference (approximately 15 K) produces a low voltage (below 100 mV), the s...
    • 24 Sep 2026
  • Final STM32 autonomous canister recovery robot, angled front view

    AWR: The Signals Behind an Autonomous Canister Recovery Robot

    paolorobillos
    paolorobillos
    An STM32 robot uses distance, encoder and IR sensor signals to find a canister, capture it, and return to a tape-marked home zone.
    • 24 Sep 2026
  • Gestu: Gesture communication with Arduino UNO Q

    shogunx
    shogunx
    .                                    Project 14: Smart Gesture Communication establishes an advanced, low-latency bridge between human movement and digital expr...
    • 23 Sep 2026
  • A 4-voice Arduino synthesizer, AM radio transmitter, and educational platform that transforms emotions into music and broadcasts them through the air.

    Musical Emotions Emitter- Broadcasting Feelings Over Medium-Wave Radio

    javagoza
    javagoza
    Musical Emotions Emitter Broadcasting Feelings Over Medium-Wave Radio A 4-voice Arduino synthesizer, AM radio transmitter, and educational platform that transforms emotions into music and broadcasts them through the air. Project Video players.brightc...
    • 18 Sep 2026
  • lora messenger

    RescueLink: A LoRa-Based Emergency Messenger for Disaster Communication

    taifur
    taifur
    Introduction  When a major disaster strikes, communication can become as important as food, water, and medical supplies. During cyclones, floods, earthquakes, and other emergencies, cellular networks and Internet connectivity may become unavaila...
    • 18 Sep 2026
  • AgriScout: A Smart Agricultural Rover Connecting Farmers to Their Fields

    Shreyas.chaurasia
    Shreyas.chaurasia
    Introduction Agriculture often requires farmers to regularly monitor different areas of a field. Soil conditions can vary from one area to another, making continuous manual monitoring time-consuming. To address this, I developed AgriScout, a low-cos...
    • 16 Sep 2026
  • R2D2 Copilot For an E-Bike

    dougw
    dougw
    Intro I have been converting my e-bike into a cargo bike so I can use it for grocery runs or trips to the Dollar store. The bike is a step-through folding bike so I can put a large cargo container on the back without having to worry about having to s...
    • 14 Sep 2026
  • Antarctic Beacon: Bridging 130 Years of Wireless History with IoT & 20m RF

    doctoriot
    doctoriot
    CWbeacon 14 MHz - An IoT Morse Code Beacon from the IoT Lab to Antarctica A 3 W HF radio beacon that keys its RF carrier with Morse code, reports its own transmissions over Telegram, authenticates every message with a CRC seeded by Marconi'...
    • 13 Sep 2026
  • Full Duplex Morse Code using the BBC micro:bit V 2.2

    Erik.H
    Erik.H
    Hey, If you are going to "Make a Connection", why not make the communication "Full duplex" or both directions at once. So that it has at least 2 paths, no waiting and real time speed. This is a project I created this year for an O...
    • 13 Sep 2026
  • Spoon Box — My First 3D Print Became an ESP32 Media Player

    ThingToo
    ThingToo
    I don’t own a 3D printer. My public library does. That’s how my first-ever 3D print became Spoon Box: a translucent ESP32 media player with an OLED display, addressable LEDs, network audio, Home Assistant integration, and a giant spoon on...
    • 12 Sep 2026
  • EM Signal detection and transmission

    Hoytman
    Hoytman
    A sea of electromagnetic noise surrounds humanity, coming from countless electrical devices. Have you ever been curious about that noise? For my competition entry, I’ll show you how to build a simple EM detector so that you can listen...
    • 10 Sep 2026
  • Barbie watching Blink

    Blinking at a webcam: a one-way optical data link with an M5Stack Atom Matrix

    apn201
    apn201
    An M5Stack Atom Matrix blinks colour at a webcam. A CRC-verified one-way optical link decodes the text. No radio, nothing to jam. Project14 entry.
    • 10 Sep 2026
  • OrderUp - Turning a Spoken Order Into a Signal the Kitchen Can Hear

    arvindsa
    arvindsa
    Since the time I learnt that the next project14 theme was going to be "Make a Connection" - Build a project that sends a message or Signal, I have been racking my mind for something unique. I blasted through the usual suspects, nearly fina...
    • 6 Sep 2026
  • Meshtastic Solar Hat Node

    ralphjy
    ralphjy
    Meshtastic Solar Hat Node Introduction Back in July, cstanton  posted The world's on fire - embrace solar punk in the Design Challenges Forum about the Meshtastic network and communicating "off grid".  I just di...
    • 5 Sep 2026
>