IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Arduino MKR 10xx, ETH Shield and Amazon Web Services: Safe MQTT with SSL and Certificate

    Jan Cumps
    Jan Cumps
    We'll connect an Arduino MKR to AWS IoT with an Ethernet cable and the MKR ETH shield.I've done this before on a MKR1010 with WiFi. This post uses the same example, with a wired Ethernet solution.With this example, you can safely connect to AWS and i...
    • 8 Sep 2019
  • Flex Suppressor Sheets Can Solve Your Noise Problems!

    nikhilstephen
    nikhilstephen
    After breaking something, how many times have you wished a band aid or duct tape could fix the issue? When I was in college, my classmates and I had an inside joke saying, “If it can’t be fixed with duct tape then you’re not using enough duct tape.” ...
    • 28 May 2019
  • The Windchillator - Reducing the sleep current of the Arduino MKR WIFI 1010 to 800 uA

    bernhardmayer
    bernhardmayer
    In an IoT sensor application the sensor usually sleeps most of the time and wakes in regular periods for a very short time to send its measurements to the cloud. This should reduce the average current consumption to 10 - 100 uA and enable a long batt...
    • 27 May 2019
  • The Windchillator - Arduino IoT Cloud and visualization

    bernhardmayer
    bernhardmayer
    Arduino IoT cloud Connecting a Arduino to the Arduino IoT Cloud is very simple and straight forward. As long as you have the right Arduino board. At the moment there are only Arduino MKR 1000, Arduino MKR WIFI 1010 and Arduino MKR GSM 1400 suppo...
    • 25 May 2019
  • The Windchillator - Introduction and Project Plan

    bernhardmayer
    bernhardmayer
    It seems like I am a little bit late for the IoT: In the Cloud challenge. Nevertheless since I received a Arduino MKR WIFI 1010 board from element14 and that my project is now almost I finished I will present it anyway. Introduction and IdeaFor ...
    • 23 May 2019
  • THING FINDER

    aabhas
    aabhas
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 14 May 2019
  • The Drawing Machine Part 2. The Arducycloid

    balearicdynamics
    balearicdynamics
    The Project: Evolution of an Idea Show Figuring Out the Design Wiring the Hardware Controlling the Motors With Only Two PWM Signals Connecting the Drawing Machine to the Cloud Registering and Setting Up the Cloud Writing the Software An Add...
    • 14 May 2019
  • Irrigation Sprinkler Control - Finishing Up

    ralphjy
    ralphjy
    This will be my final blog in the IoT: In the Cloud project.  I have finished programming the controller logic and have modified the enclosure to mount the relay module and drilled out the wiring access hole. Controller LogicFor this first ...
    • 12 May 2019
  • Traffic Management System

    crisdeodates
    crisdeodates
    A compact stand-alone system which allows transport providers and law enforcers to manage transport systems efficiently.This project focus to build a complete system for Traffic Evaluation, Management and Monitoring that is capable of relaying the re...
    • 9 May 2019
  • Basic IoT switches - flashing  SONOFF’s with Arduino IDE

    carmelito
    carmelito
    About a couple of months back a work buddy of mine, moved back to Canada and  gave me 4 Sonoff switches, he was using the Sonoff to control his lamps using the default sonoff mobile app. I dint want to use the mobile app, to send data to the clo...
    • 8 May 2019
  • Irrigation Sprinkler Control - Cayenne Dashboard and MQTT messaging

    ralphjy
    ralphjy
    I have used the myDevices Cayenne IoT platform on a couple of previous projects and I like its capability but I've discovered that for the Sprinkler Control that it has a number of shortcomings.  One of the major differences is that because I a...
    • 2 May 2019
  • Irrigation Sprinkler Control - Testing the Relay Interface

    ralphjy
    ralphjy
    I've been distracted and just realized that the deadline for the IoT: In the Cloud project is fast approaching.   Time to get back to work to connect and test the relay module.   Here are pictures of the RPi 3B and 5 inch touchscreen displ...
    • 29 Apr 2019
  • IOT and RFID based medicine prescription

    nishanchettri
    nishanchettri
    Story behind the project:I believe that a project without a story is stale and tasteless and doesnot have a vivid connection with the author/maker.Last year I was diagonsed with measles and jaundice at the same time.I was taken to a hospital nearby w...
    • 27 Apr 2019
  • Arduino IoT Cloud controlled MKR Robot ARM: We have Movement

    jomoenginer
    jomoenginer
    Month of RobotsEnter Your Project for a chance to win robot prizes for your robot builds and a $200 shopping cart!  The Birthday Special: Robot Prizes for Robot Projects!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Po...
    • 15 Apr 2019
  • Irrigation Sprinkler Controller - GUI Design

    ralphjy
    ralphjy
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 27 Mar 2019
  • Irrigation Sprinkler Control - HDMI Display Test with tkinter GUI

    ralphjy
    ralphjy
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 25 Mar 2019
  • Home Automation Using Raspberry Pi Matrix Voice and Snips

    ruchir1674
    ruchir1674
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 24 Mar 2019
  • Irrigation Sprinkler Controller - Hardware Interface Design

    ralphjy
    ralphjy
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 24 Mar 2019
  • IOT Reflow Oven with Arduino MKR WiFi 1010

    fmilburn
    fmilburn
    UPDATE  8 May 2019:  New documentation at the end of the blog on replacing thermocouple amplifier with the Arduino MKR THERM SHIELD, the Arduino MKR RGB SHIELD, and further automation experiments.    Introduction   Element ...
    • 23 Mar 2019
  • Irrigation Sprinkler Controller - Project Plan

    ralphjy
    ralphjy
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 22 Mar 2019
  • Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - AWS, Graphs and Alerts

    Jan Cumps
    Jan Cumps
    My project for Arduino Day 2019 is an autonomous sensor device that reports its battery status to Amazon Web Services. It uses AWS for data insight, graphs and to indicate how long it's expected to continue living without charging. It raises an ...
    • 22 Mar 2019
  • Arduino IoT in the Cloud - Door Alarm

    rsc
    rsc
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 22 Mar 2019
  • Arduino IoT Cloud controlled MKR Robot ARM: Das Blinken LED

    jomoenginer
    jomoenginer
    IoT: In the Cloud - Arduino IoT Cloud controlled MKR Robot ARM   Introduction   The Internet of Things is still a hot marketing topic covering everything from Voice Assistants, and Smart Lights, to connected Refrigerators that can order gr...
    • 22 Mar 2019
  • Temperature measurement with Arduino MKR WIFI 1010 and Cloud

    kk99
    kk99
    The basic idea was to create a temperature monitor based on DS18B20 sensors with support for remote access. I have used a kit called AVT-1705 which allows to read data from two DS18B20 sensors via RS485 protocol. As master controller I have used a ...
    • 21 Mar 2019
  • Irrigation Sprinkler Controller - Design Considerations

    ralphjy
    ralphjy
    IoT: In the CloudEnter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme ...
    • 21 Mar 2019
>