Arduino

An open-source platform platform that makes hardware and software accessible for rapid prototyping, learning, experimenting, and tinkering. Discuss topics and share knowledge on the entire range of Arduino compatible boards and accessories, from Classic to MKR boards, and more.

Featured Content
image tile

How to Program the Arduino Opta PLC

This article explores how Arduino-based Opta® PLC can mitigate PLC programming challenges. It also introduces the Arduino PLC programming environment, highlighting its benefits and applications in automation

Read Blog

image tile

Exploring Arduino Pro's Role in Industry 4.0

This webinar highlights how edge computing technology can drive efficiency in applications related to Industry 4.0.

image tile

Arduino Giga R1 WiFi

Buy Now    Tech Specs

The Giga R1 packs BLE and the power of the STM32H7, the processor used in the Portenta H7, into the accessible Mega form factor.

Read Blog
image tile

Nicla Sense

Buy Now

An intelligent board that features industrial-grade sensors, including a Bosch Sensortec BHI260AP motion sensor system with embedded AI.

image tile

Nano 33 BLE Sense

Buy Now

A low-power board with built-in BLE and Bluetooth 5, featuring temperature, pressure, humidity, light, and gestures sensors.

design challenge tile

Arduino Edge Control Board

Buy Now

Designed for precision farming applications, this control board is well suited for irrigation with modular connectivity.

Recent Discussions
Arduino Day Content
More
Recent Blogs
  • Using DFRobot_LIDAR07 with Arduino Uno

    I've used ST microLIDAR Time-of-Flight sensors previously to measure short distances.  A VL6180X to focus my laser cutter laser-focus-assembly-completed and VL53L0/1X sensors for distances up to 4 meters in projects whose...
  • Adding Analog RC Control to an Arduino

    I want to use analog RC control to do stuff wirelessly with an ArduinoMy method up until now for controlling penguins that flap their wings and tell jokes, rude Bender robots, and the Tin Man has been to use WiFi.  This works but I thought I wou...
  • Arduino Portenta - Person Detection

    I recently virtually attended the Arm DevSummit 2021.  One of the workshops was hosted by Edge Impulse and used the Arduino Portenta H7 with the Vision Shield to do Object Classification.  That got me interested in trying to do Object Detec...
  • Porting NeoPixels to the Arduino Portenta

    Part of my project with the Arduino Portenta requires some lighting and I wanted to be able to individually control them. I asked a model railroad mate and he suggested NeoPixels. They only require 3 wires, run on 5v and can be controlled from a rang…
Related Projects
  • 5. AardEnergy – ADE7753 Meter Chip Circuit

    At last a chance to catch up with my Energy Monitor Arduino Project. Here is the circuit I will build to work with my Arduino Uno via the SPI interface: It is a design that was informed by discussions from this question: How to Use Cur...
  • UNO R4 on the big screen

    element14 sent me an Arduino UNO R4 MINIMA, so I though I would show that it is compatible with the original UNO in addition to being way more powerful. To do this demo, I just plugged in a display shield designed for an original UNO and presto - it …
  • CAPACITANCE METER PROTOTYPE

    CAPACITANCE METER PROTOTYPE    This is my first proyect, a capacitance meter prototype of capacitors with Arduino. As we know, the Arduino digital pins have an output voltage of 5 volts, we are going to take advantage of this voltage and th...
  • 10 Best ideas for Easy Arduino Projects

    The Arduino platform has become quite popular with people just starting out with electronics. It is an open-source hardware design, based on microcontroller board designs and provide sets of digital and analog I/O pins that can be interfaced to vario…
  • Arduino-Based Automatic Guitar Tuner

     One of the most important things when playing guitar is making sure that the instrument is in tune. Even the best guitar player will not sound any good with an out-of-tune guitar. Tuning guitars by hand using a standard tuner has always been co...