Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Introduction to OM13077 Dual processor cores NXP LPCXpresso development board and demonstrating the existing project using LPCXpresso tool [Importing the example project and executing on NXP LPC54102  board]

    bheemarao
    bheemarao
    The LPCXpresso family of boards provides a powerful and flexible development system for NXP's Cortex M MCUs The LPCXpresso54102 board has been developed by NXP to enable evaluation of and prototyping with the LPC54100 family of MCUs and features the ...
    • 27 May 2016
  • Getting Started with FRDM-KW40Z NXP Freedom Development Platform [Importing existing project using KSDK1.3.0 tool chain and demonstrating DAC ADC Demo]

    bheemarao
    bheemarao
    This document shows how to import the existing project of Kinetis SDK v1.3 using the kinetis Design Studio version 3.2.0 implemented using  FRDM-KW40ZFRDM-KW40Z The  FRDM-KW40ZFRDM-KW40Z development board is an evaluation environment suppor...
    • 20 May 2016
  • Out-of-Box demo for FRDM-KW40Z NXP Freedom development platform [demonstrating wireless point-to-point out of the box connectivity based on SMAC]

    bheemarao
    bheemarao
    This blog brings you a short out-of box demo Wireless Connectivity Example Demos on the  FRDM-KW40ZFRDM-KW40Z for newly introduced freedom board  FRDM-KW40ZFRDM-KW40Z which is a low-cost development platform enabled by the Kinetis W series ...
    • 15 May 2016
  • Interfacing / Porting SDcard using MBED-OS[yotta] on Freedom board FRDM-K64F

    bheemarao
    bheemarao
    In continuation to my earlier blog on demonstration of porting MBED-OS here is another blog on interfacing sdcard using mbed os yotta modules using frdm-k64f freedom board  Refer to my earlier blog HEREIntroduction and demonstration of porting M...
    • 10 May 2016
  • Merging NXP LPCXpresso IDE with the Kinetis Design Studio, Processor Expert and Kinetis SDK [working with KSDK1.3 on LPCXpresso using FRDM-K64F freedom development board]

    bheemarao
    bheemarao
    This document tutorial show the steps how to use LPCXpresso NXP IDE with KDS processor expert and kinetis SDK1.3 implementing using  FRDM-K64FFRDM-K64F freedom board  NXP LPCXpresso IDE LPCXpresso is a low-cost microcontroller (MCU) de...
    • 22 Apr 2016
  • Getting Started with FreeRTOS and KSDK 2.0: [Creating a new FreeRTOS with KSDK V2.0 application using FRDM-K64F freedom board]

    bheemarao
    bheemarao
    The purpose of this document is to provide information that enables developers to start their first application using FreeRTOS and KSDK v2.0. FreeRTOS is integrated with the Kinetis SDK and FreeRTOS which is a Very Popular Open Source RTOS FreeR...
    • 15 Apr 2016
  • Importing project from kinetis SDK2.0: [How to import the existing project from Kinetis SDK and execute using FRDM-K64F ]

    bheemarao
    bheemarao
    This document shows how to import the existing project of Kinetis SDK v2 using the kinetis Design Studio version: 3.2.0 KSDK V2.0 Kinetis SDK v2 is a collection of comprehensive software enablement for NXP Kinetis Microcontrollers that includes ...
    • 29 Mar 2016
  • Getting Started with KSDK 2.0: [How to use the SDK with Kinetis Design Studio using FRDM-K64F freedom board]

    bheemarao
    bheemarao
    This document / tutorial show the steps how to use the SDK2.0 with Kinetis Design Studio v3.0.0 implementation using FRDM-K64F freedom board.Unlike previous SDK's, with the SDK v2.0 it only needs a generic 'new project wizard' inside KDS. KSDK V...
    • 17 Mar 2016
  • Introduction and demonstration of porting MBED-OS [yotta]on FRDM-K64F Freedom board

    bheemarao
    bheemarao
    The content of this Tutorial has been extracted from mbed.com Introduction to mbed OS mbed OS is the operating system created for mbed-enabled boards. It allows C++ applications to run on these boards by providing APIs that you can use from...
    • 1 Mar 2016
  • Kinetis Design Studio 3.0 Kinetis SDK 1.3 Processor-Expert using FRDM-KL43Z: Part-2: Displaying Timer value on SLCD and Hyperterminal

    bheemarao
    bheemarao
    This is in continuation to part-1 (for details click here), In this tutorial Here we are adding fsl_tpm and Debug UART to display the timer on Slcd and to hyperterminal. Tutorial instructions to demonstrate the projectCreate a new project as exp...
    • 9 Dec 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.3 Processor-Expert using FRDM-KL43Z: Setup configuration for KSDK1.3 and Exploring on Segment LCD using KL43Z Freedom board: Part-1

    bheemarao
    bheemarao
    This tutorial brings you on getting working with 4-digit (4X8) segment LCD present in KL43Z freedom board.   Installing the Kinetis SDK v1.3.0 / Eclipse Update Download SDK1.3.0 from below link and install it. By default it gets instal...
    • 26 Nov 2015
  • SOMNIUM DRT Freescale Kinetis IDE 2.4 Released

    e14 Contributor
    e14 Contributor
    SOMNIUM is pleased to announce the general availability release of SOMNIUM DRT Freescale Kinetis IDE, version 2.4 for ARM Cortex-M based Kinetis MCUs. DRT 2.4 introduces some key features and product enhancements to improve development productiv...
    • 10 Nov 2015
  • Interfacing HC-SR501 pyroelectric infrared PIR motion sensor detector module and FRDM-STBC-AGM01 sensor board to FRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert

    bheemarao
    bheemarao
    This is a project for interfacing PIR sensor module to FRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert The module contains 3 pins for connection with system. The two of them are vcc 5v and Gnd. The third one is output...
    • 16 Oct 2015
  • Interfacing HC-SR501 pyroelectric infrared PIR motion sensor detector module to FRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert

    bheemarao
    bheemarao
    This is a project for interfacing PIR sensor module to  FRDM-KL43ZFRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert  The module contains 3 pins for connection with system. The two of them are vcc 5v and Gnd. The th...
    • 7 Oct 2015
  • Interfacing Freescale’s FRDM-STBC-AGM01 sensor module to FRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert

    bheemarao
    bheemarao
    This is a project for interfacing FRDM-STBC-AGM01 sensor module to FRDM-KL43Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert. This board is 9-axis Sensor Toolbox Development Board Enabled for sensor fusion with FXAS21002C 3-axis gyr...
    • 22 Sep 2015
  • Interfacing Freescale’s FRDM-STBC-AGM01 sensor module to FRDM-KL46Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert

    bheemarao
    bheemarao
    This is a project for interfacing FRDM-STBC-AGM01 sensor module to FRDM-KL46Z using Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert. This board is 9-axis Sensor Toolbox Development Board Enabled for sensor fusion with FXAS21002C 3-axis gyr...
    • 16 Sep 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Quick tutorial on dimming control (varying PWM duty cycle) using user push buttons

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project controls the brightness of LED i.e varying the duty cycle using two user push button, one button to increase the b...
    • 28 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert Using FRDM-KL46Z:   Toggle Green Led using PIT (Periodic Timer Interrupt)

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This is a project for Toggle a Green LED using PIT module of PE implemented using freedom board FRDM-KL46Z.  RequirementsT...
    • 26 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL46Z: Quick tutorial on GPIO Interrupt (Toggling LED using button with Interrupt logic)

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project Toggles the RED and Green LED by pressing the push buttons SW-1 and SW-2 implemented using Interrupt function on K...
    • 24 Aug 2015
  • Build a musical EKG with the Freescale FRDM-KL05

    ciorga
    ciorga
    Short Introduction: I have been following the Battle of the DreamBoards Championship with interest and I enjoyed the variation of functionality features put together in each of the dreamboards.  I especially had my attention attracted by th...
    • 22 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Quick tutorial on GPIO Interrupt (Toggling LED using button with Interrupt logic)

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project Toggles the RED and Green LED by pressing the push buttons SW-1 and SW-2 implemented using Interrupt function on K...
    • 21 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Quick tutorial on dimming control (varying PWM duty cycle) using UART-Console communication

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project controls the brightness of LED i.e varying the duty cycle using UART console communication using debug_console and...
    • 18 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Quick tutorial on GPIO control using UART-Console communication

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project controls the GPIO (LED toggle/set/clear) using command over UART console communication using debug_console and fsl...
    • 12 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: UART communication with a console on the host through OpenSDA

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This project explores function of debug_console component interfaces to OpenSDA uart port of the KL43Z freedom board Requi...
    • 11 Aug 2015
  • Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Dimming Red Led with TPM (varying duty cycle)

    bheemarao
    bheemarao
    Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This is a project for dimming an RED LED using TPM module (i.e varying the duty cycle of the PWM pulse)  implemented on fr...
    • 31 Jul 2015
<>