RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in Writing a Tutorial How To On a Renesas MCU Board?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 2748 subscribers
  • Views 5737 views
  • Users 0 members are here
  • EK-RA6M3
Related

Would You Be Interested in Writing a Tutorial How To On a Renesas MCU Board?

rscasny
rscasny over 3 years ago

ek-ra6m3I would like to get more Renesas content on element14. I have a Renesas EK-RA6M 3 evaluation kit. If you are interested in writing a tutorial for it, I'll send it to you. 

Leave a comment below with what you would like to do with it. 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • misaz
    misaz over 3 years ago

    I already wrote it Slight smile. As part of EK-RA2L1 RoadTest I wrote step-by-step tutorial how to use basic and advanced peripherals of the MCU and shown practical development of simple application with this MCU.

     Using I2C, SPI and DMA on Renesas RA2L1 (part 1) 

     Using I2C, SPI and DMA on Renesas RA2L1 (part 2) 

    Later as part of Summer of Senors I wrote how to very easily use Renesas ZMOD4510 Air Quality Sensor on their MCU platform:

     Blog #4: Tutorial: Using ZMOD4510 with Renesas EK-RA2L1 and FSP 

    RA6M3 is more advanced MCU than RA2L1 but Renesas design MCU in very nice compatible way, so everything which works on lower platform (RA2L1) work on higher family (RA6M3) also.

    Maybe someone else can provide tutorials showing other peripherals or some different approach of using RA MCUs.

    Except RA2L1 I already own RA6M4 which I used in some projects like  Duratool Cabinet Storage Box Upgrade . RA6M4 is slightly more advanced than RA6M3 but M3 have display driver in advanced to newer M4. Do you want to provide standard EK-RA6M3 kit or kit with display (EK-RA6M3G)?

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to misaz

    I've been busy too Slight smile

    part 1: Create an Empty Project
    part 2a: Blinky with GCC Toolchain
    part 2b: Blinky with Timer and Interrupt
    part 3: Port an example from Renesas toolchain to GCC
    part 4a: Low Power - Sleep
    part 4b: Low Power - Software Standby
    part 5: DAC
    part 6: Software SHA
    part 7: Blinky with FreeRTOS
    part 8: DMA
    part 9: UART
    part 10: Reserve LCD Frame Buffer in Expansion RAM with GCC
    part 11: port emWIN to GCC and run an LCD Widget
    Renesas RX65N MCU EV Kit - Review

    So has Andrew J : Renesas Envision Kit RPBRX65N Roadtest

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    You Have!   And Andrew as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    You Have!   And Andrew as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    Thanks for pointing this out. I have to check into it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to Jan Cumps

    This issue apply for RX family only. RA have standard ARM Core and I have not seen any time limitation. So feel free to apply if you want to play with Renesas MCU which you can program and develop firmware anytime including support for crypto engine.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Jan Cumps

    Agreed, Jan.  I still have the board but don’t really know what to do with it because of the licenses.  It should be really useful given it’s built in LCD but I don’t want to fork out for a licence until I’ve got a genuine use for it, rather than just a play around.  It’s a shame because in many ways it was a useful board for learning embedded computing, something I have to get to grips with.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neerajrd82
    neerajrd82 over 3 years ago in reply to Jan Cumps

    Understood, But i forgotten one thing that RX65 series of microcontrollers contains propriety core of Renesas instead of  ARM core. That is why GCC ARM doesn't support your encryption and FS modules & it would also will not Core also. Sorry, i would have given support, if Core would would have been of  ARM. 

    THANKS    

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to neerajrd82

    The GCC arm compiler, when I roadtested a Renesas compiler, did not support the encryption and FS modules. Those were only available as a library precompiled for the Renesas toolchain.

    I documented it in this blog: 

     Renesas RX65 Envision Kit - part 3: Port an example from Renesas toolchain to GCC 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neerajrd82
    neerajrd82 over 3 years ago in reply to Jan Cumps

    Dear Jan, i can help you in this. You can use Keil MDK ARM or Segger Embedded Studio. If you have licensing issues with you existing cross compiler. By the way which cross compiler you are using? Anyhow, You can still use Segger Embedded Studio without any license issues.

    Please! note carefully: Free version of  Segger Embedded Studio will access to GCC ARM ( this is open source) & paid version of same will give access to Professional version of Segger cross-compiler.

    i sincerely think that this should be able to solve your licensing issues. In your case,Free version of  Segger Embedded Studio should be good enough. 

    THANKS

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to rscasny

    The reason why I stopped blogging about the Renesas kit, is that the license is time limited. I still have the hardware, but ran out of software license.
    Renesas is an outlier here. Their license runs out for everyone. Side effect is that community bloggers have to stop blogging.

    They are an exception. Most microcontroller manufacturers don't end date the development suite after a few months. You can keep on investigating and blogging.
    Maybe that explains why Renesas bloggers stop after a road test finished.

    • Cancel
    • Vote Up +4 Vote Down