• Products and Partners
    Products and Partners
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
Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog VenTTracker #08 - Trying to make a measuring device with the accelerometer
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 25 Apr 2021 5:18 PM Date Created
  • Views 1918 views
  • Likes 8 likes
  • Comments 1 comment
  • venttracker
  • acceleromenter
  • arduino_nano_33_iot
  • distance measurement
  • covid-19
  • integration
  • design_for_a_cause_2021
  • natural ventilation
Related
Recommended

VenTTracker #08 - Trying to make a measuring device with the accelerometer

javagoza
javagoza
25 Apr 2021

This week we have tried that our sensor measures the opening of the window using only the accelerometer, without using the magnetic linear encoder that we have used in the previous blog.

The measurement is carried out by making a double integration of the acceleration values.

We have developed a small python script to obtain the data from the Arduino through the serial port and be able to graph it.

 

image

  Design for A Cause 2021 the VenTTracker project

  01 - Intro and motivation. | 02 - Analyzing Window Types (I) | 03 - Analyzing Window Types (II) | 04 - Playing with the IMU | 05-Sliding Window Mock-up | 06 -  Window Sensor Prototype | 07 - Adjusting the window sensor | 08 - Trying to make a measuring device with the accelerometer | 09 - Checking and updating WiFiNINA Firmware | 10 - Ventilation Monitor on Arduino IoT Cloud | 11 - Wireless Environmental Monitor on Arduino Nano 33 IoT | 12 - Window Anomaly Detection. Edge Impulse & Arduino Nano 33 IoT | 14 - Environmental Monitor Revisited - Version 2 | 13 - Project wrap-up and Lessons learned

 

Tracking System for Classroom Ventilation Routines

A STEM project for classrooms

the VenTTracker project - Blog #08 - Trying to make a measuring device with the accelerometer

 

image

 

The measuring device

We have converted our window sensor into a distance measuring device. This will allow us to know the opening status of a window for our project to monitor the ventilation routines that we are doing with the Arduino Nano 33 IoT.

We use the LSM6DS3, iNEMO inertial module sensor, from the the Arduino Nano 33 IoTArduino Nano 33 IoT, to estimate the distance from the window closed position.

More information about the sensor in our past blog: VenTTracker #04 -  Playing with the IMU

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The theory

We will try to get the positioning of the window using only the accelerometer and magnetic reed switch used to detect that the window is open or closed as described in our second blog VenTTracker #02 -  Analyzing window types.

 

An acceleration sensor measures the acceleration applied to the device, including the force of gravity. The accelerometer returns acceleration force data for all three coordinate axes,

Motion sensors are useful for monitoring device movement, such as tilt, shake, rotate, or roll. Movement is usually a reflection of direct input from the user (for example, a user driving a car in a game or a user controlling a ball in a game), but it can also be a reflection of the physical environment in which it is find the device. (for example, moving with you while driving your car) In the first case, you are monitoring the movement in relation to the reference frame of the device or the reference frame of your application; in the second case, you are monitoring movement relative to the world's frame of reference. Motion sensors by themselves are not normally used to monitor the position of the device but as our requirements are not very demanding we are going to give it a try.

 

To obtain the position we must perform a double integral on the acceleration data. We apply a simple algorithm to implement a double integration of the data obtained from the sensor. The double integration consists of making a first integration to obtain the velocity and then another on the latter to obtain the position.

 

image

 

Graphic visualization of the double integration that we have obtained with the small python script that we include at the end of the blog

 

image

 

Calibrating the device

The signal is not noise-free, so it must be digitally filtered. The filter that we are going to use calculates an average of the acceleration; the value will be the result of averaging a certain number of samples.

We found that filtering only by averaging the acceleration is not enough. There is also environmental noise such as small vibrations caused by noise or air movement, so we carry out an extra filtering to discriminate the real acceleration that affects the movement of our window.

 

A "stopped" state is essential to obtain correct data. A calibration routine is needed when booting our sensor. This calibration value should be as accurate as possible. We have found that it is best to calibrate at various points on the window because the window may not be level properly. The actual value of the acceleration is the sample minus the calibration value.

 

In the calibration routine we eliminate static acceleration due to gravity. In this routine, we average the samples when the accelerometer is in a state of standstill. The more samples we have taken, the more accurate the calibration result.

 

image

 

 

Getting started

Initially we started taking samples with the official arduino library to see the behavior of our sensor by doing the double integral and applying an initial filter. The results are not very exact but they are valid for our purpose, which is to determine the position of the window without much precision. From this moment we decided to use the SparkFun library to have more control over the working parameters of the IMU.

 

Graphics made with the Arduino library. AccX in m/s^2, VelX in m/s, PosX in cm

 

imageimage

imageimage

 

imageimage

Filtering Chain

To eliminate mechanical noise we use a low pass filter. We have to eliminate as much noise as possible to prevent errors from accumulating when integrating. Being a double integral the one that we are going to make, the errors grow quadratically.

An easy way to perform a low pass filter is to perform a moving average. We have simplified filtering and consists of obtaining the average of a set of samples. It is important to obtain the average of a balanced number of samples. If we take too many samples we can end up losing too much information and if we take too few we end up with an incorrect value.

We have carried out many tests to reach an adequate value. However, we observe that the number of samples required also depends on the average speed at which we move the window, so we have had to reach a compromise in which the sensor no longer acts correctly below a velocity threshold.

 

When we are in the stop condition, minor errors in acceleration can be interpreted as constant velocity due to the fact that non-zero samples are added. In the ideal case for a stopped state, all samples should be zero. If we do not zero these samples they will accumulate on the velocity producing a virtual continuous movement and, therefore, an unstable position.

Even with the above filtering, some data may be wrong, so we need a discrimination window between valid data and invalid data for the stopped state.

 

This is our filtering chain:

 

image

 

After filtering:

 

image

 

Motion completion detection.

Looking at the graph below, there is an initial acceleration or deceleration at maximum speed. So that acceleration changes direction to zero again. At this point we can consider that a complete displacement has been made and a new position has been reached.

 

image

 

In a real scenario, the area under the positive part should be equal to the area of the negative part, reaching zero velocity when the window stops. If we don't force that velocity to zero, the position will be in an unstable state. To force the steady state if we have several acceleration samples to zero or the velocity changes sign, we force the velocity to zero.

 

User interface

Our final version of the sensor will not have a graphic display to reduce power consumption and increase battery life.

For taking samples we have included the same graphic display that we used for the previous prototype of the sensor that used a linear magnetic encoder to determine the position of the moving part of the window.

The display shows the filtered data of the acceleration, speed and position. The last position data is shown in centimeters.

 

image

 

image

Absolute reference

 

We need a way to force an origin to our measurements. We use a magnetic reed switch to zero our sensor.

Resetting position to zero. Absolute reference.

 

image

 

Estimating distance from origin

image

 

Adjusting the LSM6DS3 sensor

 

With the LSM6DS3 we can adjust:

  • the Linear acceleration measurement range

image

  • the sample rate

image

 

  • the antialiasing filter bandwidth

image

After taking many samples we decided to adjust the settings as shown in the following images.

 

image

 

The circuit

 

The circuit is similar to the window sensor prototype from the previous blog, VenTTracker #06 -  Window Sensor Prototype, from which we have removed the indicator lods and the two magnetic reed switches that made up our magnetic linear encoder.

 

image

The code

 

Python Code

 

############################################################################
#  This is an example for testing the VenTTracker Window Sensor
#  The sensor measures the opening of the window using only the accelerometer
#  When the device detects a complete movement it sends a stream of data
#  with the following structure. 
#  This scrtp parse the data a graph it.
#
#  START,accelSampleRate,accelRange,accelBandWidth, lpfSamples<LF>
#  accData,velData,posData,timestamp<LF>
#  accData,velData,posData,timestamp<LF>
#  ...
#  ...
#  ...
#  accData,velData,posData,timestamp<LF>
#  END<LF>
#  
#
#  Author: Enrique Albertos
#  Date: 2021-04-23
############################################################################




import serial
import time
import pandas as pd
import matplotlib.pyplot as plt
# if using a Jupyter notebook include
%matplotlib inline
# set up the serial line
ser = serial.Serial('COM17', 9600)
time.sleep(2)
while True:
    # Read and record the data
    accData =[]                       # empty list to store the data
    velData =[]                       # empty list to store the data
    posData =[]                       # empty list to store the data
    accelSampleRate = ""
    accelRange = ""
    accelBandWidth =""
    lpfSamples = ""
    timeStampData = []
    readings = 0
    while True:
        b = ser.readline()         # read a byte string
        string_n = b.decode()  # decode byte string into Unicode  
        string = string_n.rstrip() # remove \n and \r
        datalist = string.split(",")
        if (datalist[0] == "START"):
            accelSampleRate = datalist[1]
            accelRange = datalist[2]
            accelBandWidth = datalist[3]
            lpfSamples = datalist[4]
            break
    csvData = []
    while True:
        b = ser.readline()         # read a byte string
        csvData.append(b)
        string_n = b.decode()  # decode byte string into Unicode  
        string = string_n.rstrip() # remove \n and \r
        if (string == "END"):
            break
        readings = readings + 1
        datalist = string.split(",")
        accData.append(float(datalist[0]))           # add to the end of data list
        velData.append(float(datalist[1]))           # add to the end of data list
        posData.append(float(datalist[2]))           # add to the end of data list
        timeStampData.append(int(datalist[3]))           # add to the end of data list
    print(readings)
    if readings > 5:
        df = pd.DataFrame(csvData)
        df.to_csv("C:/Arduino/" + str(time.time()) + ".log")
        fig, axs = plt.subplots(1, 3, figsize=(14, 6), sharey=False)
        axs[0].plot(timeStampData, accData, label="Acceleration")
        axs[0].set_title('Acceleration')
        axs[0].set_xlabel('Time (ms)')            
        axs[0].set_ylabel('Acceleration (m/s^2)')
        axs[0].grid( True, color='0.95')
        axs[1].plot(timeStampData,velData, label="Velocity")
        axs[1].set_title('Velocity')
        axs[1].set_xlabel('Time (ms)')
        axs[1].set_ylabel('Velocity (m/s)')
        axs[1].grid( True, color='0.95')
        axs[2].plot(timeStampData,posData, label= "Distance") 
        axs[2].set_xlabel('Time (ms)')
        axs[2].set_ylabel('Distance (m)')
        axs[2].set_title('Distance')
        axs[2].grid(True, color='0.95')
        fig.suptitle('Distance. Sample Rate = ' + accelSampleRate + " Hz, Range +-" + accelRange + " G, Bandwidth " + accelBandWidth + " Hz" )
        plt.show()

 

Arduino Code

Obtaining data in real time from the PC is not feasible due to the time it takes to send through the serial port and the speed at which we want to take samples from the accelerometer. Therefore, the log data is buffered and sent to the serial port when a complete movement is detected.

 

/**************************************************************************
  This is an example for testing the VenTTracker Window Sensor
  The sensor measures the opening of the window using only the accelerometer
  The measurement is carried out by making a double integration of the acceleration values. 
  
  This example is for a 128x32 pixel display using I2C to communicate
  3 pins are required to interface (two I2C and one reset).


  Hardware. Pinout
    8 A4/SDA Analog ADC in; I2C SDA; SDA to SDA OLED Display
    9 A5/SCL Analog ADC in; I2C SCL to SCK OLED Display
    13 RST Digital In Active low reset input  RESET to push button. Other end to ground.
    14 GND Power Power Ground to Battery (-)
    15 VIN Power In Vin Power input VIN to Baterry (+)
    20 D2 Digital GPIO - to Open/Closed Reed Switches
    27 D9/PWM Digital GPIO to  Right Reed Switch. Other end to ground.
    28 D10/PWM Digital GPIO;  to Left Reed Switch. Other end to ground.


  Author: Enrique Albertos
  Date: 2021-04-23
 **************************************************************************/
#include "SparkFunLSM6DS3.h"


#include "SPI.h"
#include "Wire.h"
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#include <Fonts/FreeMonoBold18pt7b.h>


#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 32 // OLED display height, in pixels


#define G_CONSTANT  9.80665 // m/s^2 adjust to your location


// Declaration for an SSD1306 display connected to I2C (SDA, SCL pins)
#define OLED_RESET -1 // Reset pin # (or -1 if sharing Arduino reset pin)
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, OLED_RESET);


long lastMillis = millis();


#define DISRIMINATION_WINDOW_X 0.019
#define DISRIMINATION_WINDOW_Y 0.019
#define DISRIMINATION_WINDOW_Z 0.1
#define LPF_SAMPLES 16.0  //16


LSM6DS3 IMU(I2C_MODE, 0x6A);


uint16_t errorsAndWarnings = 0;
float maximumX = 0;
// last accelerometer reading
float lastAccXsample;
float lastAccYsample;
float lastAccZsample;
// buffer for logging
float accSamples[1000];
float velSamples[1000];
float posSamples[1000];
long timestampSamples[1000];
int rawSamplesCount = 0;
// last two readings for integration
unsigned char countx;
float accelerationX[2];
float velocityX[2];
float positionX[2];
float accelerationY[2];
float velocityY[2];
float positionY[2];
float accelerationZ[2];
float velocityZ[2];
float positionZ[2];
unsigned char direction;
float stationaryReadingX;
float stationaryReadingY;
float stationaryReadingZ;
// let's assume we are in closed position and window opens from left to right
volatile bool openCloseChangePending = true;
unsigned long lastLeftSwitchDebounceTime = 0; // the last time the input left encoder pin was toggled
unsigned long OpenClosedSwitchDebounceDelay = 150; // the debounce time
unsigned long lastDebouncingMeterMillis= 0; // last time the meter is stopped
unsigned long accelerometerDebounceDelay = 300; // the debounce time
enum WindowStateType {OPEN = HIGH, CLOSED = LOW};
int windowState = CLOSED;
bool directionChanged = false;
int openClosedSwitchPort = 2; // switch to ground + internal pull-up resistor.
                              // Negative logic LOW when switch is closed


void calibrateAccelerometer(void);
void movementEndCheck(void);
void position(void);
void resetPosition(void);
void displayPosition(void);
void isrChangeOpenClosedSwitchPort() ;


void setup() {
  setupSerialPort();
  setupAccelerometer();
  setupDisplay();
  calibrateAccelerometer();
  setUpOpenCLoseSwitch();
}


void loop() {
  int16_t temp;
  windowState = digitalRead(openClosedSwitchPort);
  if(windowState == OPEN && openCloseChangePending ) {
    openCloseChangePending = false;
    if (rawSamplesCount > 3) {
      logDataToSerial();
    }
    rawSamplesCount = 0;
  }
  if(windowState == CLOSED || openCloseChangePending ) {
    openCloseChangePending = false;
    rawSamplesCount = 0;
    resetPosition();
    displayPosition();
  }  else {
    position();
  }
}


void setupSerialPort() {
  Serial.begin(9600);
  delay(1000); 
}


void setupDisplay() {
  if (!display.begin(SSD1306_SWITCHCAPVCC, 0x3C)) { // Address 0x3C for 128x32
    for (;;)
      ; // Don't proceed, loop forever
  }
}


void setUpOpenCLoseSwitch() {
  pinMode(openClosedSwitchPort, INPUT_PULLUP);
  delay(20);
  // detect switch chages from open to closed. It is negative logic
  attachInterrupt(digitalPinToInterrupt(openClosedSwitchPort),
                  isrChangeOpenClosedSwitchPort, CHANGE);
}


void setupAccelerometer() {
  IMU.settings.gyroEnabled = 0; 
  IMU.settings.accelEnabled = 1;
  IMU.settings.accelRange = 2;      //Max G force readable.  Can be: 2, 4, 8, 16
  IMU.settings.accelSampleRate = 416;  //Hz.  Can be: 13, 26, 52, 104, 208, 416, 833, 1666, 3332, 6664, 13330
  IMU.settings.accelBandWidth = 100;  //Hz.  Can be: 50, 100, 200, 400;
  IMU.settings.accelFifoEnabled = 0;  //Set to include accelerometer in the FIFO
  IMU.settings.tempEnabled = 0;
  IMU.settings.fifoModeWord = 0; 
  if (!IMU.begin() ) {
    Serial.print("Error at begin().\n");
  }
}


void displayPosition(void) {
  display.setFont();
  display.clearDisplay();
  display.setCursor(0, 0);
  display.setTextColor(SSD1306_WHITE);
  display.print(accelerationX[1], 4);
  display.setCursor(0, 8);
  display.print(velocityX[1], 4);
  // show distance in cm
  float distance = sqrt(positionX[1]*positionX[1] + positionY[1] * positionY[1]+ positionZ[1] * positionZ[1]) * 100.0;
  display.setCursor(0, 16);
  display.print(distance, 4);
  display.setFont(&FreeMonoBold18pt7b);
  display.setCursor(64, 24);
  display.print((int)distance);
  display.setFont();
  display.print("cm");
  display.display();
}


/**
  Interrupt Service Routine for Changing Edge in Open Close Switches
*/
void isrChangeOpenClosedSwitchPort() {
  windowState = digitalRead(openClosedSwitchPort);
  if ((millis() - lastLeftSwitchDebounceTime) > OpenClosedSwitchDebounceDelay) {
    openCloseChangePending = true;
    lastLeftSwitchDebounceTime = millis();
  }
}


void resetPosition(void) {
  accelerationX[1] = 0;
  accelerationX[0] = 0;
  velocityX[1] = 0;
  velocityX[0] = 0;
  positionX[0] = 0;
  positionX[1] = 0;


  accelerationY[1] = 0;
  accelerationY[0] = 0;
  velocityY[1] = 0;
  velocityY[0] = 0;
  positionY[1] = 0;
  positionY[0] = 0;


  accelerationZ[1] = 0;
  accelerationZ[0] = 0;
  velocityZ[1] = 0;
  velocityZ[0] = 0;
  positionZ[1] = 0;
  positionZ[0] = 0;


  lastMillis = millis();
}


// read accelerometer data
void readAccelerometerData() {
  lastAccXsample = -IMU.readFloatAccelX();
  lastAccYsample = IMU.readFloatAccelY();
  lastAccZsample = IMU.readFloatAccelZ();
}


void displayCalibrationInfo() {
  display.clearDisplay();
  display.setCursor(10,10);
  display.fillScreen(BLACK);
  display.setTextColor(WHITE);
  display.println(F("Calibrating IMU..."));
  display.print(F("Sample rate: "));
  display.print(IMU.settings.accelSampleRate);
  display.print(F(" Hz"));
  display.display();
  delay(20);
}


/*******************************************************************************
  The purpose of the calibration routine is to obtain the value of the reference
threshold. It consists on a 1024 samples average in no-movement condition.
********************************************************************************/
void calibrateAccelerometer(void) {
  unsigned int count1 =0;
  displayCalibrationInfo();
  stationaryReadingX = 0.0;
  stationaryReadingY = 0.0;
  stationaryReadingZ = 0.0;
  // calculate mean stationary value
  do {
      readAccelerometerData();
      stationaryReadingX = stationaryReadingX + lastAccXsample; // Accumulate Samples
      stationaryReadingY = stationaryReadingY + lastAccYsample; 
      stationaryReadingZ = stationaryReadingZ + lastAccZsample; 
      count1++;    
  } while (count1 != 1024); // 1024 times
  stationaryReadingX = stationaryReadingX / 1024.0;
  stationaryReadingY = stationaryReadingY / 1024.0;
  stationaryReadingZ = stationaryReadingZ / 1024.0; 
}


/*
Send data buffers to serial
*/
void logDataToSerial() {
  Serial.print("START");
  Serial.print(",");
  Serial.print(IMU.settings.accelSampleRate);
  Serial.print(",");
  Serial.print(IMU.settings.accelRange);
  Serial.print(",");
  Serial.print(IMU.settings.accelBandWidth);
  Serial.print(",");
  Serial.println(LPF_SAMPLES);


  for (int i = 0; i < rawSamplesCount; ++i) {
    Serial.print(accSamples[i], 8);
    Serial.print(",");
    Serial.print(velSamples[i], 8);
    Serial.print(",");
    Serial.print(posSamples[i], 8);
    Serial.print(",");
    Serial.print(timestampSamples[i]-timestampSamples[0]);
    Serial.println();
  }
  Serial.println("END");
}


/*
  This function allows movement end detection. If a certain number of
acceleration samples are equal to zero or velocity direction has changed the sign 
we can assume movement has stopped.
Velocity variables are reseted, this stops position increment and eliminates position error.
*/
void movementEndCheck(void) {
  
if ( accelerationX[1] == 0 )// we can assume that velocity is cero
 // we count the number of acceleration samples that equals cero
  {
    countx++;
  } else {
    countx = 0;
  }


if (countx > 2 || directionChanged ) 
   {
    displayPosition();
   
    countx = 0;
    resetAccelerationBuffer();
    resetVelocityBuffer();
    directionChanged = false;


    if (rawSamplesCount > 4) {
      logDataToSerial();
    }
    rawSamplesCount = 0;
    lastDebouncingMeterMillis = millis();
   }
  displayPosition();
}


void resetAccelerationBuffer() {
    accelerationX[0] = 0.0;
    accelerationX[1] = 0.0;
    accelerationY[0] = 0.0;
    accelerationY[1] = 0.0;
    accelerationZ[0] = 0.0;
    accelerationZ[1] = 0.0;
}
void resetVelocityBuffer() {
    velocityX[0] = 0.0;
    velocityX[1] = 0.0;
    velocityY[0] = 0.0;
    velocityY[1] = 0.0;
    velocityZ[0] = 0.0;
    velocityZ[1] = 0.0;
}


void debounceAccelerometer() {
  while (millis() < lastDebouncingMeterMillis + accelerometerDebounceDelay){
    readAccelerometerData();
    resetAccelerationBuffer();
    resetVelocityBuffer();
  }
}


/*****************************************************************************************/
/******************************************************************************************
  This function transforms acceleration to a proportional position by
integrating  the acceleration data  twice. It also adjusts sensibility by
multiplying the "positionX"  and "positionY" variables. This integration
algorithm carries error, which is compensated in the "movenemt_end_check"
  subroutine. Faster  sampling frequency implies less error  but requires more
memory. Keep  in mind that the same process is applied to the X and Y axis.
*****************************************************************************************/


void position(void) {

  unsigned int count2;
  count2 = 0;
  debounceAccelerometer(); 
  // filtering routine for noise attenuation average represents the acceleration of an instant
  do {    
    readAccelerometerData();
    accelerationX[1] = accelerationX[1] + lastAccXsample;
    accelerationY[1] = accelerationY[1] + lastAccYsample;
    accelerationZ[1] = accelerationZ[1] + lastAccZsample;
    count2++;


  } while (count2 != LPF_SAMPLES); // 64 sums of the acceleration sample


  // Low pass band filter
  accelerationX[1] = accelerationX[1] / LPF_SAMPLES; // division by 64
  accelerationX[1] = accelerationX[1] - stationaryReadingX; // eliminating zero reference
  
  accelerationY[1] = accelerationY[1] / LPF_SAMPLES; // division by 64
  accelerationY[1] = accelerationY[1] - stationaryReadingY; // eliminating zero reference


  accelerationZ[1] = accelerationZ[1] / LPF_SAMPLES; // division by 64
  accelerationZ[1] = accelerationZ[1] - stationaryReadingZ; // eliminating zero reference
  // offset of the acceleration data


  // mechanical filter
  if ((accelerationX[1] <= DISRIMINATION_WINDOW_X) &&
      (accelerationX[1] >=-DISRIMINATION_WINDOW_X)) // Discrimination window applied
  {
    accelerationX[1] = 0; // to the X axis acceleration
  }


  if ((accelerationY[1] <= DISRIMINATION_WINDOW_Y) &&
      (accelerationY[1] >=-DISRIMINATION_WINDOW_Y)) // Discrimination window applied
  {
    accelerationY[1] = 0; // to the Y axis acceleration
  }


  if ((accelerationZ[1] <= DISRIMINATION_WINDOW_Z) &&
      (accelerationZ[1] >=-DISRIMINATION_WINDOW_Z)) // Discrimination window applied
  {
    accelerationZ[1] = 0; // to the Z axis acceleration
  }


  // variable
  long actualTime = millis();
  long ellapsedTime = actualTime - lastMillis;
  lastMillis = actualTime;


  // first X integration:
  velocityX[1] = velocityX[0] + (accelerationX[0]  + ((accelerationX[1] - accelerationX[0]) / 2.0)) *  G_CONSTANT * ellapsedTime /1000.0 ;
  velocityY[1] = velocityY[0] + (accelerationY[0]  + ((accelerationY[1] - accelerationY[0]) / 2.0)) *  G_CONSTANT * ellapsedTime /1000.0;
  velocityZ[1] = velocityZ[0] + (accelerationZ[0]  + ((accelerationZ[1] - accelerationZ[0]) / 2.0)) *  G_CONSTANT * ellapsedTime /1000.0;


  // second X integration:
  if ( (velocityX[0] * velocityX[1]) > 0) {
    positionX[1] = positionX[0] + (velocityX[0] + ((velocityX[1] - velocityX[0]) / 2.0)) * ellapsedTime/1000.0;
    positionY[1] = positionY[0] + (velocityY[0] + ((velocityY[1] - velocityY[0]) / 2.0)) * ellapsedTime/1000.0;
    positionZ[1] = positionZ[0] + (velocityZ[0] + ((velocityZ[1] - velocityZ[0]) / 2.0)) * ellapsedTime/1000.0;
  }


  if (rawSamplesCount == 0 ) {
    accSamples[rawSamplesCount] = accelerationX[0];
    velSamples[rawSamplesCount] = velocityX[0];
    posSamples[rawSamplesCount] = positionX[0];
    timestampSamples[rawSamplesCount] = millis()-ellapsedTime;
    rawSamplesCount++;
  }
  
  accelerationX[0] =  accelerationX[1]; // The current acceleration value must be sent to the previous acceleration
  directionChanged = (velocityX[0] * velocityX[1]) < 0;
  velocityX[0] = velocityX[1]; // Same done for the velocity variable
  positionX[0] = positionX[1]; // actual position data must be sent to the


  accelerationY[0] =  accelerationY[1]; // The current acceleration value must be sent to the previous acceleration
  velocityY[0] = velocityY[1]; // Same done for the velocity variable
  positionY[0] = positionY[1]; // actual position data must be sent to the


  accelerationZ[0] =  accelerationZ[1]; // The current acceleration value must be sent to the previous acceleration
  velocityZ[0] = velocityZ[1]; // Same done for the velocity variable
  positionZ[0] = positionZ[1]; // actual position data must be sent to the




  accSamples[rawSamplesCount] = accelerationX[1];
  velSamples[rawSamplesCount] = velocityX[1];
  posSamples[rawSamplesCount] = positionX[1];
  timestampSamples[rawSamplesCount] = millis();
  rawSamplesCount++;


  movementEndCheck();


  direction = 0; // data variable to direction variable reset
}

 

 

Next Steps

  • Prepare our sensor to share your data in the cloud.
  • Prepare our sensor to be able to configure it via bluetooth
  • Train a Machine learning model that allows us to detect anomalies in the movement of the window to warn of the need for window maintenance.
  • Get started with the design of our environmental sensor.

 

VenTTracker Blogs
VenTTracker #01 - Intro and motivation.
VenTTracker #02 - Analyzing window types.
VenTTracker #03 - Analyzing window types II
VenTTracker #04 - Playing with the IMU
VenTTracker #05 - Sliding Window Mock-up
VenTTracker #06 - Window Sensor Prototype
VenTTracker #07 - Adjusting the window sensor
VenTTracker #08 - Trying to make a measuring device with the accelerometer
VenTTracker #09 - Checking and updating WiFiNINA Firmware
VenTTracker #10 - Ventilation Monitor on Arduino IoT Cloud
VenTTracker #11 - Wireless Environmental Monitor on Arduino Nano 33 IoT
VenTTracker #12 - Window Anomaly Detection. Edge Impulse & Arduino Nano 33 IoT
VenTTracker #14 (aka #11 bis) - Environmental Monitor Revisited - Version 2
VenTTracker #13 - Project wrap-up and Lessons learned

 

 

<< Previous VenTTracker BlogNext VenTTracker Blog  >>
VenTTracker #07 - Adjusting the window sensorVenTTracker #09 - Checking and updating WiFiNINA Firmware
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +1
    Very good post. You did a great job of analyzing your data and applying filters to smooth the data without losing accuracy. Well done. DAB
Parents
  • DAB
    DAB over 5 years ago

    Very good post.

    You did a great job of analyzing your data and applying filters to smooth the data without losing accuracy.

     

    Well done.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Very good post.

    You did a great job of analyzing your data and applying filters to smooth the data without losing accuracy.

     

    Well done.

     

    DAB