In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Dust, Temperature and Humidity Monitor Chapter 7

    engswee
    engswee
    (Best view 1920 x 1200)This chapter only discuss about PCB design and PCB prototype. Sorry guys have a bad cough and fever this weeks.Get an 4 days MC. PCB:Look like I need to have 2 design PCB for this project for now. Fan have a big internal cutout...
    • 16 Dec 2014
  • AirMobile - 13 - AirVantage binding

    amgalbu
    amgalbu
    Previous postsAirMobile - 11 - MQTT Java ClientAirMobile - 12 - AirVantage REST API AirVantage OpenHAB bindingAfter creating an helper class for accessing the data stored in AirVantage, I am now ready to implement an OpenHAB binding. With such a...
    • 16 Dec 2014
  • Carbon Footprint Monitoring - Hardware Design

    xever
    xever
    Over the past few days, I have been contemplating about the hardware for this particular project and ended up with a PCB design as rendered below.  Initial Thoughts How I came into this design was a result of a thought process that att...
    • 16 Dec 2014
  • ITO - In the Air Degign Challenge - Portable Field Tester #5

    dwinhold
    dwinhold
    Hello to everyone!! So, my update last week didn't get posted due to a drastic change in our project. With the focus on clean air, water and soil sensing, I was creating sensor boards for.. well sensors. This was starting to work well until my d...
    • 16 Dec 2014
  • AirMobile - 12 - AirVantage REST API

    amgalbu
    amgalbu
    AirVantage REST API In the previous post, I created a Java MQTT client to push data into the AirVantage cloud platform.Next step is to read it out and make it available to OpenHAB. In this post I will talk about the AirVantage REST API, whereas ...
    • 15 Dec 2014
  • In the Air Design Challenge, Auto Greenhouse Blog Post #3

    dimonic
    dimonic
    Apologies folks for the long gap between posts! Things have been moving forward, although not as fast as I would like, and not ion all the areas I would like them to. Things Achieved Assembled a frame for the project - Ikea Gorm frame,...
    • 12 Dec 2014
  • Blog Summary #003 : In The Air Challenge 2014

    cstanton
    cstanton
    The In The Air Challenge is running from September 22nd to February 27th.Previous Activity:Blog Summary #000 : In The Air Challenge 2014Blog Summary #001 : In The Air Challenge 2014Blog Summary #002 : In The Air Challenge 2014Current Activity:Blog Su...
    • 12 Dec 2014
  • [AirCare] InTheAir - Week 7: Dust sensor

    fvan
    fvan
    Previous posts for this project:[AirCare] InTheAir - Project Description[AirCare] InTheAir - Week 1: Getting a Launchpad to Blink[AirCare] InTheAir - Week 2: Preparing the Beaglebone Black[AirCare] InTheAir - Week 3: Fuel Tank Testing[AirCare] InTheA...
    • 12 Dec 2014
  • AirMobile - 11 - MQTT Java Client

    amgalbu
    amgalbu
    MQTT Java ClientMQTT is a light-weight protocol initially developed by IBM for transferring telemetry data. It' based on the publisher-subscriber paradigm: a device can publish data into the system and many receivers can subscribe to get data changes...
    • 11 Dec 2014
  • [Firecracker Analyzer] Making the Power PCB with Eagle, TI BQ25504, TPS62740 and TPS61200

    ipv1
    ipv1
    Previous Posts[Firecracker Analyser] [week 0] Project Description[Firecracker Analyser] [week 0] Sensor Research[Firecracker Analyzer] [week 1] System Design and ReDesign[Firecracker Analyzer]Brief update[Firecracker Analyzer] Messing with an I2C LCD...
    • 11 Dec 2014
  • [Firecracker Analyzer] Another small update

    ipv1
    ipv1
    Previous Posts[Firecracker Analyser] [week 0] Project Description[Firecracker Analyser] [week 0] Sensor Research[Firecracker Analyzer] [week 1] System Design and ReDesign[Firecracker Analyzer]Brief update[Firecracker Analyzer] Messing with an I2C LCD...
    • 11 Dec 2014
  • In The Air: Episode 6 - Getting Ready For PCBs

    michaelwylie
    michaelwylie
    Previous Posts:In The Air: Epidose 1: IntroductionIn The Air: Episode 2 - Preparing for Surface Mount WorkIn The Air: Episode 3 - Surface Mount BeginningsIn The Air: Episode 4 - InductorsIn The Air: Episode 5 - PCB Design UpdateThis week involve...
    • 11 Dec 2014
  • HAB monitoring Post#6 ( Sensor node enclosure design )

    rmlab
    rmlab
    The image below shows my sensor node enclosure. The enclosure is an air-tight box where all electronics ( MSP430FR5969, batteries, C110L tranceiver) will be fixed inside. A total of four PVC elbows with 12 inches pipes are mounted on two longer sides...
    • 11 Dec 2014
  • In the Air Design Challenge - Pollen & Allergen Sensing – Post 4 (Preparing the InTheAir Power Board)

    tomaja
    tomaja
    Previous posts:In the Air Design Challenge - Pollen & Allergen SensingIn the Air Design Challenge - Pollen & Allergen Sensing – Post 1 (Pollen Sensor)In the Air Design Challenge - Pollen & Allergen Sensing – Post 2In the Air Design Challe...
    • 7 Dec 2014
  • In-the-Air-Challenge: Dust counting with Beagle Bone Black and a webcam

    janisalnis
    janisalnis
    Previous post: In-the-Air-Challenge: Air Quality Sensor BoxNext post: In-the-Air-Challenge: A sheet of laser light for 2D visualization of dust flow Roadtesters for In-the-Air-Challenge received fom Element14 a free Beaglebone Black (BBB) microc...
    • 7 Dec 2014
  • [Firecracker Analyzer] Messing with an I2C LCD and using the BUS PIRATE

    ipv1
    ipv1
    The LCD itself First things first... The bus pirate. On to the bus! Conclusion I got one of these (The LCD!The LCD!) LCDs from the budget and the motive is to use them to display air quality. Low and behold I got them and these things are t...
    • 6 Dec 2014
  • Carbon Footprint Monitoring - Emission Sensor Firmware

    xever
    xever
    This week's update is going to be short but sweet, as I have been working most on the firmware architecture and device driver development.  So far, the code flow as below.   The intention is that the emission sensor board will be ...
    • 6 Dec 2014
  • Dust, Temperature and Humidity Monitor Chapter 6

    engswee
    engswee
    (Best view 1920 x 1200) This chapter I will share about PCB design.This PCB design in under progress. I will talk about the design, problem, solution and related issue.It simply straight forward since we have dedicated hardware and all the relat...
    • 6 Dec 2014
  • In-the-Air-Challenge:   Air Quality Sensor Box

    janisalnis
    janisalnis
    Previous: In-the-Air Challenge:  Texas Instruments MSP 430 FR5969 launchpadNext post: In-the-Air-Challenge: Dust counting with Beagle Bone Black and a webcamI bought three CO2 sensors and Arduino-nanos and gave one to high school students and o...
    • 5 Dec 2014
  • [AirCare] InTheAir - Week 6: Accessing Fuel Tank's Data

    fvan
    fvan
    Previous posts for this project:[AirCare] InTheAir - Project Description[AirCare] InTheAir - Week 1: Getting a Launchpad to Blink[AirCare] InTheAir - Week 2: Preparing the Beaglebone Black[AirCare] InTheAir - Week 3: Fuel Tank Testing[AirCare] InTheA...
    • 5 Dec 2014
  • Blog Summary #002 : In The Air Challenge 2014

    cstanton
    cstanton
    The In The Air Challenge is running from September 22nd to February 27th.Previous Activity:Blog Summary #000 : In The Air Challenge 2014Blog Summary #001 : In The Air Challenge 2014Current Activity:Blog Summary #003 : In The Air Challenge 2014Blog Su...
    • 5 Dec 2014
  • AirWise #5 - Preliminary Schematic

    e14 Contributor
    e14 Contributor
    Just a quick post with my preliminary schematic.My plan is to prototype this circuit on a shield first and then to order a custom PCB board. Finalized schematic, BOM and layout to follow.
    • 5 Dec 2014
  • AirMobile - 10 - Switching to "Plan B"

    amgalbu
    amgalbu
    While creating the board layout, I realized (too late!) that the package I choose for the MSP430 was not available. I selected the MSP430FR5947 MSU because it has the same features of the MSP4305969 mounted on the LaunchPad but in a more handy TSSOP3...
    • 3 Dec 2014
  • In The Air: Episode 5 - PCB Design

    michaelwylie
    michaelwylie
    UpdateA Riddle: How many times in three weeks can a 1 year old child catch sick? The correct answer seems to be 3 times ... Previous PostsIn The Air: Epidose 1: IntroductionIn The Air: Episode 2 - Preparing for Surface Mount WorkIn The Air: Epis...
    • 2 Dec 2014
  • [Firecracker Analyzer]Brief update

    ipv1
    ipv1
    Its been a hectic couple of weeks and progress has been slow. I will be posting a series of smaller posts to cover work done and my "evil plans". One of the factors that contributed to my slow progress was sensor selection and I am still a ...
    • 29 Nov 2014
<>