Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Blog
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Path to Programmable 3 - Winner's Announcement

    rscasny
    rscasny
    What is Path to Programmable III? Path III is the third session in the element14 Community’s structured FPGA-based SoC training. The first Path training program was held in 2018 and focused on programmable logic devices PLDs and featured the AV...
    • 27 Sep 2023
  • Demonstration and Outcome - Blog 6

    Demonstration and Outcome - Blog 6

    rahulkhanna
    rahulkhanna
    Welcome to the final blog on building a Bottle Cap Inspection System using Machine Vision. In this project, we plan to create an automated visual inspection system that can detect defects in bottle caps, such as cracks, deformation, and missing parts...
    • 10 Sep 2023
  • LCD click interface on Ultra96-V2 - Blog 5

    LCD click interface on Ultra96-V2 - Blog 5

    rahulkhanna
    rahulkhanna
    Welcome to blog 5 for the Ultra96-V2 development board. In this blog, we'll dive into interfacing an LCD Click board with the Ultra96-V2, allowing you to display information, messages, or graphics on an LCD screen. Let's get started...
    • 8 Sep 2023
  • Path to Programmable III Final Project Blog: CarSafety Device using Xilinx ZYNQ FPGA

    taifur
    taifur
    Introduction This is the final project blog for Path to Programmable III using the MiniZed Xilinx ZYNQ FPGA board. In this project blog, I will show how I made an internal car safety device using some Grove sensors and the MiniZed FPGA board. From a ...
    • 6 Sep 2023
  • Final Project - Process of medical images

    cghaba
    cghaba
    The project was developed in the Health part of the Market path though the application is related also to Vision path. The project is intended to allow the process of medical images in order to improve diagnostics or provide radiologists with a tool ...
    • 6 Sep 2023
  • Morse Code from MNIST: Accelerating Convolutional Neural Networks in Ultra96v2 using Tensil AI - Final

    rajivbishwokarma
    rajivbishwokarma
    Table of Contents Introduction Training a CNN-based neural network on MNIST? Converting PyTorch model to ONNX Tensil AI accelerator hardware for Ultra96v2 Generating Vivado bitstream for Ultra96v2 LED hardware design Creating PYNQ image for Tensil A...
    • 6 Sep 2023
  • Interfacing LMS6DSL Click Mezzanine with Ultra96-V2 Using Vitis - Blog 4

    Interfacing LMS6DSL Click Mezzanine with Ultra96-V2 Using Vitis - Blog 4

    rahulkhanna
    rahulkhanna
    In this tutorial, we will guide you through the process of interfacing the LMS6DSL Click Mezzanine with the Ultra96-V2 development board using Xilinx Vitis. The LMS6DSL Click Mezzanine is equipped with a sensor that can measure both acceleration and ...
    • 5 Sep 2023
  • Exploring Xilinx Vitis | Zynq MPSoC - Blog 3

    Exploring Xilinx Vitis | Zynq MPSoC - Blog 3

    rahulkhanna
    rahulkhanna
    In this blog post, we will set up the Vitis IDE, where we will walk through the process of creating a workspace, configuring a Platform project, and creating an Application project. The final stage in the hardware export process...
    • 5 Sep 2023
  • PTPIII - Final Project - Ultra-Gimbal

    PTPIII - Final Project - Ultra-Gimbal

    saadtiwana_int
    saadtiwana_int
    Foreword I have some past experience of working with FPGAs. I am, by no mean, an expert, but learnt what I needed to get the jobs done for some medium complexity projects. All my previous FPGA projects were running some IPs in the FPGA fabric an...
    • 5 Sep 2023
  • Path to Programmable III Training Blog #06: MiniZed Color Sensor Webserver - Final

    flyingbean
    flyingbean
    Table of Contents Introduction Project Structure MiniZed Color Sensor Webserver Demo Conclusions References Introduction A color sensor is a type of transducer that converts one form of energy into another form.  Digilent PMOD color module ...
    • 5 Sep 2023
  • Path to Programmable III Training Blog #6 Final Blog-Build Machine Vision Project with Vitis-AI on IP-DPU

    fyaocn
    fyaocn
    Build Machine Vision Project with Vitis-AI on IP-DPU Table of Contents 1 Ultra96v2 and Vitis AI 2 Create Vitis AI development docker environment 3 Create hardware design with vivado 3   Model Hub and Vitis AI 4 Create the IMG 1 Ultra96v2 and...
    • 5 Sep 2023
  • P2P3 - Final Blog - Object Detection and Localisation on ultra96v2 using AI/ML

    manihatn
    manihatn
    Introduction: The final project is based on AI/Machine Learning within the Core Technology Path. The aim of the project was to accelerate object detection and localisation on ultra96v2. I have some prior experience in FPGA design, but this ...
    • 5 Sep 2023
  • Path to Programmable III : Ultra96V2 : ADAS Camera Processing through Deep Learning Unit (DPU) | Final Project Blog |

    prashanthgn.engineer
    prashanthgn.engineer
    Hello Element14 Challengers  Introduction Current trend in Automotive segment moving towards different level of autonomous driving. Advanced Driver Assistance system is the key for the Autonomous vehicles.  Where the sensor clusters is i...
    • 4 Sep 2023
  • Path to Programmable III Training Blog #02: MiniZed Board Requirement & Details

    vishnu123
    vishnu123
    MiniZed is a single-core Zynq 7Z007S development board. With the advent of the latest cost-optimized portfolio from Xilinx, this board targets entry-level Zynq developers with a low-cost prototyping platform.This compact design features on-boa...
    • 4 Sep 2023
  • Path to Programmable III Training Blog 01: Kit Unboxing & MiniZed Board Understanding

    vishnu123
    vishnu123
    Unboxing the MiniZed Box Contains⦁ MiniZed Board – 1 ⦁ Micro USB cable – 1⦁ SDSoc License from AMD Xilinx – 1 . MiniZed Board Understanding Features⦁ Xilinx Zynq single-core SoC XC7Z007S-1CLG225C.⦁ Micron storage: 512MB DDR3L...
    • 4 Sep 2023
  • Implementation of 3GPP MIMO Decoder on MiniZed board with XC7Z007S-1CLG225C Device

    svnagendra2003
    svnagendra2003
    Implementation of 3GPP MIMO Decoder on MiniZed board with XC7Z007S-1CLG225C Device
    • 4 Sep 2023
  • Video Mixer on XC7Z007S-1CLG225C device on MiniZed Board

    svnagendra2003
    svnagendra2003
    Video Mixer on XC7Z007S-1CLG225C device on MiniZed Board
    • 4 Sep 2023
  • Timing optimization techniques for RTL based designs on XC7Z007S-1CLG225C MiniZed board

    svnagendra2003
    svnagendra2003
    Timing optimization techniques for RTL based designs on XC7Z007S-1CLG225C MiniZed board
    • 4 Sep 2023
  • Extensive usage of XADC module on MiniZed Starter Kit

    svnagendra2003
    svnagendra2003
    Extensive usage of XADC module on MiniZed Starter Kit
    • 4 Sep 2023
  • Embedded Vision Engine for Development of a Computer Vision terminal

    pandoramc
    pandoramc
    Table of Contents Vitis AI Camera support Real-Time Vitis AI It is an interesting project from AMD to run inference development solutions. There are several versions of Vitis AI. This time, compared with the last post with PYNQ Computer Vision en...
    • 4 Sep 2023
  • UART Test - Serial Message on Ultra96-V2 - Blog 2

    UART Test - Serial Message on Ultra96-V2 - Blog 2

    rahulkhanna
    rahulkhanna
    In this blog, we will be working on the process of printing messages to the serial port on the Ultra96-V2 development board. Serial communication is a fundamental method for interacting with embedded systems, allowing you to monitor and debug yo...
    • 4 Sep 2023
  • Path to Programmable 3 Final Project - A Simple but Complete Control System Tutorial Project for "Very Very Beginners" Implemented in the Zynq7000 SoC on the MiniZed Board

    ciorga
    ciorga
    Introduction My goal in this project is to practice what I have learned in the training courses by creating a reference tutorial type project that starts from scratch and builds a simple but complete control system utilizing both PL and PS of the Zyn...
    • 31 Aug 2023
  • Minized Synth I

    AMD Zynq SoC MIDI Vintage Sound Synthesizer - Final

    javagoza
    javagoza
    1. Minized Synth I Introduction In a music studio, a newbie synth designer is given a complex sound synthesizer and told to bring out the sound of a 'Grand Piano' using subtractive synthesis. After some tweaking, all that's left is a basic sin...
    • 27 Aug 2023
  • Path to Programmable III with Ultra96 Zynq - Holes in Driveways' real time reporting.

    lfb
    lfb
    As a continuos increasing need, holes in driveways must be fixed in order to preserve cars and reduce maintanance of driving population.  It is known that holes might cause traffic jams, accidents and even deadly car crashes. It is also an expen...
    • 27 Aug 2023
  • Path to Programmable III with MiniZed: Project Blog: Flight Simulator Display using multisensory interface with Processing 4.0!

    Path to Programmable III with MiniZed: Project Blog: Flight Simulator Display using multisensory interface with Processing 4.0!

    navadeepganeshu
    navadeepganeshu
    Table of Contents Introduction The Design Flow Blocks and Interfaces Hardware Implementation Vitis Implementation Using Processing IDE Demo Clips and Video Code and Resources Also Read: PathtoProgrammable3 training blogs Introducti...
    • 27 Aug 2023
>