Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • QuadCop: Navigation, how do I get to a specific GPS coordinate?

    screamingtiger
    screamingtiger
    Previous Posts Here:http://www.element14.com/community/tags#/?tags=quadcop_project Im currently working on 2 major updates this weekend.  I am adding in some sci fi elements and installing sensors to give the QuadCOP a more Science Fiction ...
    • 22 Aug 2015
  • PizzaPi: Building The Admin

    dmrobotix
    dmrobotix
    Back again with another update. I've uploaded another video capture that shows both the customer front-end and some of the administrative front-end. I am almost done building out the UIs for these and then it is a matter of writing the PHP code to li...
    • 22 Aug 2015
  • Meditech: Python + PyGTK + Glade = UI Design

    balearicdynamics
    balearicdynamics
    IntroductionDefinitely the Python language with some content improvements has been adopted to manage the UI, replacing the initial idea to use Qt for two reasons: development optimization and architecture simplification. Unfortunately as many times o...
    • 21 Aug 2015
  • Meditech: Inter-process control

    balearicdynamics
    balearicdynamics
    IntroductionMeditech should be something simple. Simple to use, addressed to non-expert IT users, possibly as much autonomous as possible, possibly able to help the operator, possibly usable with few buttons (=NO KEYBOARD REQUIRED) and much more. Thi...
    • 20 Aug 2015
  • PizzaPi: Customer Frontend

    dmrobotix
    dmrobotix
    Hello, everyone! I apologize for being incommunicado for so long. I was sick for a few weeks and then I had to wrap up work at the lab for the summer. Excuses, excuses, I know. Anyway, I'm here! I'll be posting a lot more as we are now i...
    • 20 Aug 2015
  • TrainingSphere - 7 - A new frame

    amgalbu
    amgalbu
    In my previous post I showed some photos of a frame made of steel wires. I found out this design to be absolutely faulty because it was not rigid enough to dampen vibration induces by motors and propellers. So I started with a new frame frame made of...
    • 19 Aug 2015
  • Sci Fi Your Pi: PiDesk - Project Update #19

    fvan
    fvan
    Previous posts for this project:Sci Fi Your Pi: PiDesk - Project DescriptionSci Fi Your Pi: PiDesk - Project Update #1Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2Sci Fi Your Pi: PiDesk - Project Update #2Sci Fi Your Pi: PiDesk - Revi...
    • 19 Aug 2015
  • QuadCop - Magnetic Sensor Working

    screamingtiger
    screamingtiger
    Previous posts for this project:http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/tags#/?tags=quadcop_project YES, I am hiding some mess OK???  THe QuadCOP is a mess too but it goes together cleanly pretty f...
    • 18 Aug 2015
  • The Picorder: A Star Trek style Tricorder-Schematic

    saturnv
    saturnv
    The attached file is the current schematic drawing of the 'Picorder'.At this time, no other additions or modifications are expected (unless something drastically fails this late in the contest) to be incorporated into the device. It's basic prototype...
    • 16 Aug 2015
  • Meditech: User Interface, optimization and simplification

    balearicdynamics
    balearicdynamics
    IntroductionOne way to optimize the behavior of the Meditech system is adopting the more reliable tools, programming languages and technologies depending on the different tasks that should be accomplished. This implies obviously a multi-language&nbsp...
    • 16 Aug 2015
  • The Picorder : A Star Trek style Tricorder - Aug 15

    saturnv
    saturnv
    Just a quick notification that I have nearly completed the Picorder changes and schematic diagram. Both have taken me longer than anticipated. I had some obstacles to overcome with the 1.5vdc power for the speaker amplifier. My voltage divider needed...
    • 15 Aug 2015
  • Escape The Past: Recipe Transfer to PLC and PLC data logging

    frellwan
    frellwan
    This week I was able to make progress on being able to read the recipe files and load the data to the PLC. I also made some modifications to the OEE data collection to add a header line to the log  file. PLC Recipe Files:In order to load re...
    • 14 Aug 2015
  • Sci Fi Your Pi: PiDesk - Project Update #18

    fvan
    fvan
    Previous posts for this project:Sci Fi Your Pi: PiDesk - Project DescriptionSci Fi Your Pi: PiDesk - Project Update #1Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2Sci Fi Your Pi: PiDesk - Project Update #2Sci Fi Your Pi: PiDesk - Revi...
    • 13 Aug 2015
  • QuadCop: A quick pre update

    screamingtiger
    screamingtiger
    Hello, Its been awhile since I wrote an update.  I have done much work on the quad cop.  I ran into some issues with the MEMS sensor board and have abandoned it in favor of another electronic compass.  So instead of being negative...
    • 11 Aug 2015
  • Meditech Annex III - A more efficient way to manage MySQL database on Raspberry PI from the PC

    balearicdynamics
    balearicdynamics
    IntroductionThe most common way, and probably better known, to manage a MySQL database is using the PhpMyAdmin web application. This sounds good in all that cases where the MySQL database is remotely stored on a web server, especially when the core c...
    • 10 Aug 2015
  • Sci Fi Your Pi: PiDesk - Project Update #17

    fvan
    fvan
    Previous posts for this project:Sci Fi Your Pi: PiDesk - Project DescriptionSci Fi Your Pi: PiDesk - Project Update #1Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2Sci Fi Your Pi: PiDesk - Project Update #2Sci Fi Your Pi: PiDesk - Revi...
    • 9 Aug 2015
  • Meditech Annex II - Python development lifecycle on Raspberry PI

    balearicdynamics
    balearicdynamics
    IntroductionAs Python is an interpreted language the first temptation for develop applications is directly editing the sources on the Raspberry PI, eventually with the help of the Python idle simple IDE installed by default in raspbian; this developm...
    • 9 Aug 2015
  • Meditech Annex I - Setting a C++ Development Environment for Raspberry PI

    balearicdynamics
    balearicdynamics
    This post is an annex to the Meditech project explaining one of the (possible) best practices to setup an efficient development environment for C++ developing on the Raspberry PI platform with the advantage of an advanced IDE and remote compiling wit...
    • 9 Aug 2015
  • Escape The Past: SMTP Email Client

    frellwan
    frellwan
    This week I was able to make progress on a couple of remaining items. First, I was able to get email notifications working and secondly, I was able to get recipes downloaded. I still need to get the recipe data into the PLC, but I should finish that ...
    • 7 Aug 2015
  • Escape the Past: DF1 Communications

    frellwan
    frellwan
    This week I was able to get the DF1 protocol operational. It is not a compete implementation of the protocol, but it implements read and write operations for data transfer to/from a SLC 500 processor.RS-232 communication As mentioned in a previous po...
    • 31 Jul 2015
  • Sci Fi Your Pi: PiDesk - Guide: Endstops with Gertbot

    fvan
    fvan
    Introduction Gertbot Pins Modes Code Demo Conclusion  Introduction In a previous guide, I covered how to control stepper motors using Gertbot. For this post, I'd like to cover the built-in endstop functionality. Endstops ...
    • 30 Jul 2015
  • The Picorder. A Star Trek style Tricorder - Day 93 Demo #1-7-26-15

    saturnv
    saturnv
    players.brightcove.net/.../index.html   So here's the video I could not get uploaded over the weekend. I still want to do a couple more videos to show the readouts better for the demo's since the working screen is on the device and is a TFT 2.8R...
    • 29 Jul 2015
  • Meditech: Text-To-Speech user support

    balearicdynamics
    balearicdynamics
    IntroductionMeditech will be used in many different environments and not always the visual information provided on the screen maybe useful. Receiving helpful audio hints and suggestions on-the-go is a good solution; when the user should activate a pr...
    • 28 Jul 2015
  • The Picorder: Day 93 Operational Demo

    saturnv
    saturnv
    {gallery} Day 93 Picorder in operationMy Partner in crime: Hard at work!!CHASSIS: Power regulatorPower Supply: 5Vdc for testingThe Face of Pi: New PIR sensorPower Board: Pull-up resistorsPIR MOUNTING: Standoff PlacementIMPERFBOARD: PIR mountsSENSOR: ...
    • 27 Jul 2015
  • [Project VIRUS]UPDATE-RPi Robot Takes Shape

    ipv1
    ipv1
    Older Posts:[Project VIRUS][Week 0]Project Description[Project VIRUS][Week 1] Another RPi Robot Part 1[Project VIRUS][Week 2] Another RPi Robot Part 2: Python and Remote Control[Project VIRUS][Week 3] Getting started with OpenCV and RPi Camera[Projec...
    • 26 Jul 2015
<>