Arduino

An open-source platform platform that makes hardware and software accessible for rapid prototyping, learning, experimenting, and tinkering. Discuss topics and share knowledge on the entire range of Arduino compatible boards and accessories, from Classic to MKR boards, and more.

Featured Content
image tile

How to Program the Arduino Opta PLC

This article explores how Arduino-based Opta® PLC can mitigate PLC programming challenges. It also introduces the Arduino PLC programming environment, highlighting its benefits and applications in automation

Read Blog

image tile

Exploring Arduino Pro's Role in Industry 4.0

This webinar highlights how edge computing technology can drive efficiency in applications related to Industry 4.0.

image tile

Arduino Giga R1 WiFi

Buy Now    Tech Specs

The Giga R1 packs BLE and the power of the STM32H7, the processor used in the Portenta H7, into the accessible Mega form factor.

Read Blog
image tile

Nicla Sense

Buy Now

An intelligent board that features industrial-grade sensors, including a Bosch Sensortec BHI260AP motion sensor system with embedded AI.

image tile

Nano 33 BLE Sense

Buy Now

A low-power board with built-in BLE and Bluetooth 5, featuring temperature, pressure, humidity, light, and gestures sensors.

design challenge tile

Arduino Edge Control Board

Buy Now

Designed for precision farming applications, this control board is well suited for irrigation with modular connectivity.

Recent Discussions
Arduino Day Content
More
Recent Blogs
  • Using DFRobot_LIDAR07 with Arduino Uno

    I've used ST microLIDAR Time-of-Flight sensors previously to measure short distances.  A VL6180X to focus my laser cutter laser-focus-assembly-completed and VL53L0/1X sensors for distances up to 4 meters in projects whose...
  • Adding Analog RC Control to an Arduino

    I want to use analog RC control to do stuff wirelessly with an ArduinoMy method up until now for controlling penguins that flap their wings and tell jokes, rude Bender robots, and the Tin Man has been to use WiFi.  This works but I thought I wou...
  • Arduino Portenta - Person Detection

    I recently virtually attended the Arm DevSummit 2021.  One of the workshops was hosted by Edge Impulse and used the Arduino Portenta H7 with the Vision Shield to do Object Classification.  That got me interested in trying to do Object Detec...
  • Porting NeoPixels to the Arduino Portenta

    Part of my project with the Arduino Portenta requires some lighting and I wanted to be able to individually control them. I asked a model railroad mate and he suggested NeoPixels. They only require 3 wires, run on 5v and can be controlled from a rang…
Related Projects
  • 3d printer filament roll holder and monitor for Arduino

    Introduction Updates Weight vs length and vice-versa Finding and testing the load sensor (scale sensor) The filament roll scale design Assembling the parts Some structure improvements Circuit and wiring 1. Power the system and initial…
  • Weather Station that lasts months!

    IntroductionEnergy Harvesting is one of the most important topic for sustainability. We have lot of connected devices > be it smart home devices, city monitoring devices, industry specific devices,etc. Mostly all of them need a continuous source o...
  • Using a Vacuum Fluorescent Display (VFD) with a Microcontroller

    Table of Contents Introduction Exploring the Display Connecting It Up Arduino Code What Characters are Supported? Summary Introduction Sometimes, it’s nice to use a luxury display such as a VFD! This short blog post describes how to get a ...
  • Animation on the Arduino Uno R4 WiFi

    element14 and Arduino were kind enough to send me the new Arduino Uno R4 WiFi and an R4 Minima to try out.  I have a 12 year old grandson who is interested in computers and plan to introduce him to Arduino this summer.  He is already k...
  • 10 Awesome Arduino Projects ! - June 2014

    Sorting Machine - Skittles and M&Ms ? I find this almost therapeutic to watch, perhaps it's a little OCPD in me but seeing an Arduino UnoArduino Uno control a machine which will sort out your sweeties by colour is great. This little video do..…