Arduino

An open-source platform platform that makes hardware and software accessible for rapid prototyping, learning, experimenting, and tinkering. Discuss topics and share knowledge on the entire range of Arduino compatible boards and accessories, from Classic to MKR boards, and more.

Featured Content
image tile

How to Program the Arduino Opta PLC

This article explores how Arduino-based Opta® PLC can mitigate PLC programming challenges. It also introduces the Arduino PLC programming environment, highlighting its benefits and applications in automation

Read Blog

image tile

Exploring Arduino Pro's Role in Industry 4.0

This webinar highlights how edge computing technology can drive efficiency in applications related to Industry 4.0.

image tile

Arduino Giga R1 WiFi

Buy Now    Tech Specs

The Giga R1 packs BLE and the power of the STM32H7, the processor used in the Portenta H7, into the accessible Mega form factor.

Read Blog
image tile

Nicla Sense

Buy Now

An intelligent board that features industrial-grade sensors, including a Bosch Sensortec BHI260AP motion sensor system with embedded AI.

image tile

Nano 33 BLE Sense

Buy Now

A low-power board with built-in BLE and Bluetooth 5, featuring temperature, pressure, humidity, light, and gestures sensors.

design challenge tile

Arduino Edge Control Board

Buy Now

Designed for precision farming applications, this control board is well suited for irrigation with modular connectivity.

Recent Discussions
Arduino Day Content
More
Recent Blogs
  • Using DFRobot_LIDAR07 with Arduino Uno

    I've used ST microLIDAR Time-of-Flight sensors previously to measure short distances.  A VL6180X to focus my laser cutter laser-focus-assembly-completed and VL53L0/1X sensors for distances up to 4 meters in projects whose...
  • Adding Analog RC Control to an Arduino

    I want to use analog RC control to do stuff wirelessly with an ArduinoMy method up until now for controlling penguins that flap their wings and tell jokes, rude Bender robots, and the Tin Man has been to use WiFi.  This works but I thought I wou...
  • Arduino Portenta - Person Detection

    I recently virtually attended the Arm DevSummit 2021.  One of the workshops was hosted by Edge Impulse and used the Arduino Portenta H7 with the Vision Shield to do Object Classification.  That got me interested in trying to do Object Detec...
  • Porting NeoPixels to the Arduino Portenta

    Part of my project with the Arduino Portenta requires some lighting and I wanted to be able to individually control them. I asked a model railroad mate and he suggested NeoPixels. They only require 3 wires, run on 5v and can be controlled from a rang…
Related Projects
  • Arduino IOT cloud controlled Smart irrigated garden

    It's been in the plans to build a raised bed garden as part of our green projects to go along with our off grid solar systems for our Art Studio and Tool shed, which are powered by 1800 watts of solar. I rediscovered Arduino when researching s...
  • 1. AardEnergy – Kick Off - a new project

    1. AardEnergy. A Simple PlanMeasure current and voltage on single phase electrical suppliesCalculate electrical parameters like RMS, Real Power, Apparent Power, Power Factor, Frequency, THD, kWhrUse Arduino Uno with an electrical metering chip ...
  • VALENTINE'S DAY ROSE

       If there is a date to show affection and love to that special person we have in our lives, that date is Valentine's Day. A gift that we always have in mind is to give red roses for the meaning they have, but after a few days they begin t...
  • LEGO Train Track Switch - Servo, LED, PubNub and Node-RED

    I've been working on this Arduino project for a while. Mostly mechanical issues, but finally got a solid solution for my LEGO train track switch. I am also using IoT style messaging to emulate a distributed network of "things". It's...
  • SmarDen: Sustainable gardening via Dropbox

    In order to control plants via Dropbox we built the following control circuit / Cyber Physical System (CPS) / Internet of Things application. To support sustainability, the water used is taken out of a natural pond. The required energy is supplied by…