1. Introducution
2. Dynamic Load Setup
3. Load Regulation Behavior
4. Current Limiting Behavior
5. Short Circuit Protection
6. Conclusions
This is the third blog post of my RoadTest review of the AIM-TTI QPX750SP power supply: AIM-TTI Ben...
The need for power supply protection systemsA robust bench power supply like the QPX750SP with a wider than normal output power range enables test, development, and troubleshooting of systems that would overload, shut down, or damage standard bench p...
1. Introduction
2. Resistive Loads
Aim-TTS QPX750SP
RD Tech DPH5005
ATX Power Supply
LTE 12V Power Brick
Mean Well 12V Power Adapter
Mean Well (NXP) 12V Power Brick
IBM 16V Laptop Charger
ASUS 19V Laptop Charger
LiteON 19V Power B...
Introduction The modulation capability of the instrument virtually turns the instrument into a voltage amplifier with gains of 0.5, 1 or 2. As previously shown in the regulation tests, during modulation the instrument samples the input signal at...
Introduction To explore the regulation capabilities of the SMU I performed a few tests to see how it behaved in voltage priority mode (VPM), current priority mode (CPM), and in the (voltage) modulation mode. Let's briefly explain what all th...
I'm getting ready to launch a roadtest on a 70 W Single-Phase Inverter Using BridgeSwitch for Fan Application. I was sent the board, but I wanted to send a motor with the inverter board. I'd like to get some help in selected a compatible motor....
The Aim-TTi QPX750SP is not a typical bench power supply. A typical bench power supply may have two or three output channels capable of delivering 0 to about 30 VDC at up to say 3 A. For example, my Keysight E36313A is a typical bench sup...
I am thrilled to have been selected to roadtest the BT817 chip and while it has only been 4 days since I received it, I wanted to share some information early on as it may help other people working with the evaluation board.Once I have worked ...
Solar Cell Characterization (Workflow Comparison)Solar or photovoltaic cells are devices that convert light energy into electric energy through the photovoltaic effect. Optimizing power conversion from solar cells is not trivial because of the shape ...
Introduction A Peltier device is a solid-state heat pump that transfers heat from one side to the other. The heat transfer simultaneously reduces the temperature at one side of the device and increases it at the other side, generating in this wa...
Introduction DC-DC converters are devices that convert a source at one DC voltage into another. They can be classified in many ways, such as between linear and switching, step-up and step-down, based on their topology, and so on.Depending on the...
Introduction Properly optimizing energy consumption of battery powered microcontrollers is fundamental to extend the battery life. Questions like when it is better to keep the device idling and when to enter light- or deep-sleep cannot be answer...
1. Motivation
2. Power Supplies
3. Dummy Loads
4. Test Equipment
5. Test Plan
The AIM-TTI QPX750SP is a powerful bench power supply, capable of providing a maximum of 750W DC power within a wide voltage range of 0-80 V. It is a profes...
Greetings! I wanted to share with you a fun opportunity that any roadtester who is also a maker and project builder may enjoy. Our agency has started a series called "Movers and Shakers in the Maker Space." The series is broadcasted o...
This page is a collection of snippets for the RoadTest of the MPM54304 <link to final review> In this road test I aim to answer the following 2 questions:(1) How is the MPM54304 programed the first time?(2) How well do the software tools p...
This is the fourth blog post (and the last one) in a series that has covered my on-going roadtesting work of the Rohde & Schwarz NGU401 SMU instrument. I had to post this update as a separate blog because when I tried to append it to the pr...
I welcome you to my review of MAX31343 Shield. My review is split to multiple chapters linked in following table of contents. Main page of review (marked with yellow star) contains summary, final score, and description of all chapters. Most important...
I welcome you to my review of MAX31343 Shield. My review is split to multiple chapters linked in following table of contents. Main page of review (marked with yellow star) contains summary, final score, and description of all chapters. Most important...
I welcome you to my review of MAX31343 Shield. My review is split to multiple chapters linked in following table of contents. Main page of review (marked with yellow star in table of contents below this text) contains summary, final score, and descri...
Tutorial: Using Shield with ArduinoI welcome you to my review of MAX31343 Shield. My review is split to multiple chapters linked in following table of contents. Main page of review (marked with yellow star) contains summary, final score, and descript...
Contents:
1. Introduction
2. Mikroe’s SGP30 Air Quality 4 click
Mikroe.com
Turning to Element14
Searching for other SGP30 drivers online
Silicon Labs GitHub page for I2C-based Bluetooth Applications
3. Using Simplicity Studio 5
Sta...
I welcome you to my review of MAX31343 Shield. My review is split to multiple chapters linked in following table of contents. Main page of review (marked with yellow star) contains summary, final score, and description of all chapters. Most important...