Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog BT_Sentry Introduction
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
  • Author Author: mcb1
  • Date Created: 30 Apr 2018 4:58 PM Date Created
  • Views 4055 views
  • Likes 20 likes
  • Comments 21 comments
  • bluetooth
  • raspberry pi 3 b+
  • rf signal
  • pi camera
  • bt_sentry
Related
Recommended

BT_Sentry Introduction

mcb1
mcb1
30 Apr 2018

BT_SENTRY

 

My plan for the BlueTooth Unleashed Challenge is to use it to provide an addition to Home Automation.

 

 

Concept

The idea is to detect the bluetooth transmitted from the vehicle and signal other Home Automation functions.

If the vehicle is known then it can open the garage door, and inform the home owner that xx is home.

 

If the system doesn't recognise the vehicle, it can :-

  • trigger a survelliance camera to record video and take snapshots.
  • turn on the outside lights
  • inform the houseowner that they have visitors
  • Send a notification to a smartphone

This system also can record when someone visited and for how long, which may prove useful if they have been up to no good.

 

 

 

 

Background

I live in the country and we have a shared driveway, and then a long (by normal standards) driveway to the house.

image

When we first moved in, it was open paddocks, and you could see anyone coming into the properties. Now that the trees and shrubs have grown, there is no visibility of incoming vehicles.

Being forewarned about who is coming up the driveway, gives you a few minutes to get sorted before they knock on the door.

 

Because we aren't always at home, having a method to capture pictures of incoming vehicles at least allows you to know what and when someone may have visited.

There are legitimate visitors during the day, but there also some others that could be opportunistic with less than desirable reasons for visiting the property.

 

 

 

Why Bluetooth

I've thought about driveway monitors before, and while they can signal that the beam has been broken, it really tells you nothing more.

You're unable to tell what direction or if it was indeed a vehicle, or some loose stock that broke the beam.

 

Bluetooth monitoring is used in NZ to predict travel times. The local transport agency sniffs the MAC address of vehicles going past and then matches that with the next detection point to build up an average travel time.

It is entirely based on history, so can be several hours ago, but people seem happier to have a figure for their journey time, regardless of the accuracy.

 

This idea uses the same method of snooping the MAC address, but for known vehicles we can add other functionality.

 

 

 

Hardware

The detection point needs to be at the start of the driveway, and because there is no power source, this will need to be low power with solar charging.

The PSOC range seems a very good fit, but because of the timeline and my need to upskill, the inital design will be Arduino based and some form of RF transmitter/transceiver.

 

Adding a vehicle detection loop or beam is necessary to ensure those vehicles without bluetooth will also trigger the system.

 

The camera is intended to be a RaspberryPi which will be performing the receiving signal, along with storing the database of known vehicles, and the appropriate response (ie lights, gargage door, announcement)

Depending on the field tests the RPi could also be doing the Bluetooth detection as well (I prefer to avoid picking up the neighbours movements)

 

This will be housed in an outdoor light fitting, so as to appear normal.

Consideration for the antenna needs to be made as most of these fittings are metal.

This was another done in an earlier challenge, and gives the idea, however I plan to use a version with lots of LEDs (similar to the one below) and swap out some LED's for IR and remove others to allow the camera to be mounted.

image  image

 

So my Hero board will be the Raspberry Pi 3 B+

imagebut I will try to use the Cypress PSOC6 which I purchased earlierimage

 

 

 

 

Software

I've used UV4L https://www.linux-projects.org/uv4l/  for a rear view camera Rear View Camera ver 2.0  , and this has a great advantage of allowing streaming to an indoor server as well as simple control over images.

I expect there will be some python scripts to process the incoming trigger information, as well as passing on relevant information to the internal system for storing and notifying the house occupants.

 

I've used OpenHAB  https://www.openhab.org/  during an earlier challenge, and it lent itself to very powerful control and can easily communicate using NodeRed https://nodered.org/  for switching the outdoor lighting.

This also allows control via phone to switch the lights on/off as required, so it has other uses.

 

I can also use something like ITTT https://ifttt.com/   to push a notification out to a smartphone/email, etc that a visitor is there.

 

 

I imagine the bulk of my time will be integrating, testing and refining the various software parts, as the hardware is fairly straight forward. .... BUT this is a Design Challenge and things are never what they seem.

The RedBear BLE board I looked at and tried ordering is a restricted item into NZ, so forward planning and a plan is a must for these.

Design Challenge Blogs   and  Why Challengers Must Post - Upcycle it - Progress Week 3

 

 

 

I've been twarted on my electronic picture of tying it all together, but the pen still works, and the 'Whitelines" paper https://www.whitelinespaper.com/   seemed a really good way to convey it.

image

 

 

 

Previous Design Challenges

I've been involved in a few previous Challenges and helped judge in another. What is Electronic Up-Cycling

 

The links to my previous are :-

Catch Santa Challenge a mini challenge to catch Santa ... except the delivery schedule got all mucked up, but Santa was on time.

Wireless Power - Beyond the Phone   Beyond the Phone - eLIST progress 6 - pictures  including the extra piece The Illuminated Beer Tap

Forget Me Not Design Challenge    eLDERmon Final Summary  Mark Beckett wins Community Choice Award in element14's Forget Me Not design challenge

 

The Teachers Pet Robotics was the only DC I was unable to complete.

This was due to suddenly having to go to England for five weeks and a mountain of additional work.

I did take it for the trip and made the organisers aware of the situation as soon as possible

BOE Robot

 

 

Thanks for the opportunity to apply.

I think this challenge has some exciting potential and it will be interesting to see the variety in the chosen applicants.

 

Mark

 

 

The other posts are here :-

BT_Sentry Introduction
BT_Sentry : Zero Emission Detection
BT_Sentry : Data Transmission
BT_Sentry : Sentry Power
BT_Sentry : Raspberry Pi
BT_Sentry : Bluetooth Options
BT_Sentry : Software
BT_Sentry : Bluetooth Sniffing
BT_Sentry : OpenHAB
BT_Sentry : Notifications
BT_Sentry : MQTT
BT_Sentry : Connecting to MQTT Broker
BT_Sentry : Summary
BT_Sentry : ESP8266 Clients
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 8 years ago +3
    Great idea Mark A good real world application of Bt. I will follow with attention your progress. Enrico
  • mcb1
    mcb1 over 8 years ago in reply to jkutzsch +3
    Sorry jkutzsch I overlooked your query. The area in front of the house/garages is 23m wide by about 18 metres to the driveway. The drive is about 80m long from where our driveway turns and enters the property…
  • fvan
    fvan over 8 years ago +2
    Great intro!
  • mcb1
    mcb1 over 8 years ago in reply to jkutzsch

    Sorry jkutzsch I overlooked your query.

     

    The area in front of the house/garages is 23m wide by about 18 metres to the driveway.

    The drive is about 80m long from where our driveway turns and enters the property.

    Line of sight is 93m to the ideal camera spot, which is no problem with 433MHz.

     

    The ideal camera spot is on the garage facing the driveway, and PIR sensors work better when something crosses them.

     

    My concern with simply using the PIR is we have cats and the odd similar sized opossum running around at times.

    They tend to trigger the outdoor lighting, so maybe the camera will capture their party tricks at night. image

     

    I'm definately looking at the various trigger options, and one is the one introduced by dubbie here RoboBobLet #5 : A Laser RangeFinder.

    The plan last night was to experiment (but didn't happen).

    I have a couple of these radar units that fmilburn introduced here LS Cubed: Little Sister Security System which are still on their way.

    (Frank if you can, can you measure the current consumption please)

     

    They hold promise as the trigger to wake up other parts of the driveway sensor.

     

    Cheers and keep up the ideas, you never know what helps. image

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dstough45
    dstough45 over 8 years ago

    Nice project! I'm looking forward to seeing how it progresses. Good luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to Jan Cumps

    You need to be in the µA

    Agreed.

     

    12v 6AH battery is 72WH, and 50mA at 12v is 0.6W. 72/0.6 gives 120 hours

     

    24hours running requires 0.6 x 24 = 14.4W

     

    Hadley did a great blog about the size of solar panel v load.

    https://nicegear.nz/blog/what-size-solar-panel-and-battery-do-i-need/

     

    And using the 4 hours I'll need 14.4/4 = 4.5 watt panel to allow for losses.

     

    So reducing the load is a prime focus for the next couple of weeks.

    Hopefully the BT modes will transfer to whatever low energy hardware I use.

     

     

    Cheers and thanks for your help/advice/suggestions.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to mcb1

    All active modes in that table are on the high side for long time self-sustainability. You need to be in the µA (even low µA - say 100 or less on average)  range to have decent standalone/solar-powered-backup'd life

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to Jan Cumps

    Jan Cumps

     

    After looking at the specs it isn't low energy. image

    I have two of these

    X-NUCLEO-IDB05A1 - Bluetooth Low Energy expansion board based on SPBTLE-RF module for STM32 Nucleo - STMicroelectronics

     

    I have a few other Cypress modules that are in a box in the garage ... tomorrows job.

     

    You are correct that I'm hoping to capture traffic as it approaches, and I'm presuming that I will need to broadcast that you can connect to me, in order to capture the mac address.

     

    I can't exactly work out what mode but it seems that the current consumption is lower.

    image

    Thanks for the link.

    I'll have a look later.

     

    Mark

    The PSoC tutorial are great.

    I've looked a few of the videos and felt they could be a bit shorter ... sadly got sidetracked before completing them all.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>