Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Number Plate Recognition #4: Loading an Image to FPGA

    taifur
    taifur
    Over the last few years, FPGAs have moved from glue logic to computing platforms. They effectively provide a reconfigurable hardware platform for implementing logic and algorithms. Being fine-grained hardware, FPGAs are able to exploit the par...
    • 13 Jan 2022
  • Number Plate Recognition # 3: Implementing Block RAM using Verilog

    taifur
    taifur
    For making our project we need to work with images and for storing images inside an FPGA we need to use Block RAM. So, in this section, I will show how to implement Block RAM in FPGA using the Vivado tool. What is Block RAM? Block RAMs (or BRAM) stan...
    • 11 Jan 2022
  • Security Hardware Accelerator #5 Complete build of SHA256 accelerator in microblaze core

    fyaocn
    fyaocn
    1. Import new platform of xsa file from vivado. Prepare the platform with xsa in vivado, 64k memory is used. It is Ok for 32k , final code size is about 10k. According to design flow in previous blogs. 2. Creating new Vitis Projects The platform sett...
    • 10 Jan 2022
  • Audio Synth #4 - Use PWM to control LED

    a33333
    a33333
    Table of Contents Audio Synth #1 - The project Audio Synth #2 - Board introduction and IDE setup Audio Synth #3 - Arduino to CmodS7 COMM Test Audio Synth #4 - Use PWM to control LED Audio Synth #5 - Testing the I2S PCM5102 DAC Decoder Board Audio Sy...
    • 10 Jan 2022
  • Number Plate Recognition #2: Working with Verilog

    taifur
    taifur
    What is Verilog Verilog is a Hardware Description Language (HDL). It is a language used for describing a digital system like a network switch or a microprocessor or a memory or a flip−flop. It means, by using an HDL we can describe any digital ...
    • 4 Jan 2022
  • Number Plate Recognition #2: Working with Verilog

    taifur
    taifur
    What is Verilog Verilog is a Hardware Description Language (HDL). It is a language used for describing a digital system like a network switch or a microprocessor or a memory or a flip−flop. It means, by using an HDL we can describe any digital ...
    • 4 Jan 2022
  • Number Plate Recognition #2: Working with Verilog

    taifur
    taifur
    What is Verilog Verilog is a Hardware Description Language (HDL). It is a language used for describing a digital system like a network switch or a microprocessor or a memory or a flip−flop. It means, by using an HDL we can describe any digital ...
    • 4 Jan 2022
  • Audio Synth #3 - Arduino to CmodS7 COMM Test

    a33333
    a33333
    Table of Contents Audio Synth #1 - The project Audio Synth #2 - Board introduction and IDE setup Audio Synth #3 - Arduino to CmodS7 COMM Test Audio Synth #4 - Use PWM to control LED Audio Synth #5 - Testing the I2S PCM5102 DAC Decoder Board Audio Sy...
    • 2 Jan 2022
  • HACK CPUMOD S7 #1: Proposal

    pandoramc
    pandoramc
    The main idea is take a basic CPU to implement in the FPGA. Nowadays, there are some advanced CPU to develop a system like MIPS, ARM, RISC V, Microblaze and so on. Despite the availability of this components, the concept could be obscure for undergra...
    • 29 Dec 2021
  • Number Plate Recognition #1: Introduction & Getting Started with FPGA

    taifur
    taifur
    [Note: I am new in FPGA and just started learning it. I will share my understanding here. I may be wrong in some cases or something can be oversimplified.] Introduction Vehicle Number Plate Recognition (NPR) or License Plate Recognition (LPR) or Regi...
    • 28 Dec 2021
  • Liquid-Level Monitoring Using a Pressure Sensor #5 - Using Vivado and Testing the System

    guillengap
    guillengap
    Table of Contents Project Introduction Getting Started Calibrating the MPX2050DP Pressure Sensor Calculations and Noise Reduction Using Vivado and Testing the System Project Report Updated **********************************************************...
    • 28 Dec 2021
  • Liquid-Level Monitoring Using a Pressure Sensor #4 - Calculations and Noise Reduction

    guillengap
    guillengap
    Table of Contents Project Introduction Getting Started Calibrating the MPX2050DP Pressure Sensor Calculations and Noise Reduction Using Vivado and Testing the System Project Report Updated **********************************************************...
    • 27 Dec 2021
  • Audio synth #2 - Board introduction and IDE setup

    a33333
    a33333
    Table of Contents Audio Synth #1 - The project Audio Synth #2 - Board introduction and IDE setup Audio Synth #3 - Arduino to CmodS7 COMM Test Audio Synth #4 - Use PWM to control LED Audio Synth #5 - Testing the I2S PCM5102 DAC Decoder Board Audio Sy...
    • 22 Dec 2021
  • Liquid-Level Monitoring Using a Pressure Sensor #3 - Calibrating the MPX2050DP Pressure Sensor

    guillengap
    guillengap
    Table of Contents Project Introduction Getting Started Calibrating the MPX2050DP Pressure Sensor Calculations and Noise Reduction Using Vivado and Testing the System Project Report Updated **********************************************************...
    • 22 Dec 2021
  • Audio synth #1 - The project

    a33333
    a33333
    Table of Contents Audio Synth #1 - The project Audio Synth #2 - Board introduction and IDE setup Audio Synth #3 - Arduino to CmodS7 COMM Test Audio Synth #4 - Use PWM to control LED Audio Synth #5 - Testing the I2S PCM5102 DAC Decoder Board Audio Sy...
    • 13 Dec 2021
  • LiFi #1 - Vivado and Verilog

    kluivertcorreia
    kluivertcorreia
    Table of Contents Introduction Getting Familiar with the Board (CMOD S7) Design Flow Setting Up Vivado Installing Board Files Basic Overview of the interface Structural HDL Revisiting Gates Pin Mapping Half Adder Half Subtractor Conclusio...
    • 12 Dec 2021
  • Security Hardware Accelerator #4 Use Vitis and Make the CMOD-S7 work

    fyaocn
    fyaocn
    1 Prepare Xilinx Shell Architecture (XSA) file for Vitis After successfully create the first Block Diagram , it is time to perpare the Xilinx Shell Architecture (XSA) file for Vitis 1.1 Click the Validate Design buttonin the Diagram pane's toolbar (o...
    • 8 Dec 2021
  • Security Hardware Accelerator #3 Create first Block Design and Add Microblaze Core.

    fyaocn
    fyaocn
    1. Add Microblaze Core First It is easy to start with template. But that is not FPGA born to be. I start from scratch, add soft-core, UART, GPIO, peripherals. Then coding with Verilog to make the project run.  2. Create first Block Design ...
    • 6 Dec 2021
  • Security Hardware Accelerator #2 Reinstall Vitis and Add board support

    fyaocn
    fyaocn
    1. Reinstall the Vitis With Vivado I have use the vitis in Ubuntu 18.02, not board support for CMOS-S4 is proper installed. Then I reinstall the Vitis in Windows 10 and added the Board support.  Then Installing Digilent Board Files, ...
    • 1 Dec 2021
  • Liquid-Level Monitoring Using a Pressure Sensor #2 - Getting Started

    guillengap
    guillengap
    Table of Contents Project Introduction Getting Started Calibrating the MPX2050DP Pressure Sensor Calculations and Noise Reduction Using Vivado and Testing the System Project Report Updated **********************************************************...
    • 30 Nov 2021
  • Security Hardware Accelerator #1 Hardware and Vivado Installation

    fyaocn
    fyaocn
    1. Introduction This proposal of Security Hardware Accelerator uses FPGA to encode signals from host hardware and return encryption codes back. This is simple accelerator for extra security. The algorithm can be very complicated requiring more LUTs. ...
    • 25 Nov 2021
  • Liquid-Level Monitoring Using a Pressure Sensor #1 - Project Introduction

    guillengap
    guillengap
    Table of Contents Project Introduction Getting Started Calibrating the MPX2050DP Pressure Sensor Calculations and Noise Reduction Using Vivado and Testing the System Project Report Updated **********************************************************...
    • 24 Nov 2021
  • Up-Down Counter Design using ZedBoard

    subham109
    subham109
    This is my first technical blog which will introduce the readers to the ZedBoard setup for the programmable logic application. It will help first-time users with the setup and develop their first FPGA project. Getting started with Vivado St...
    • 27 Oct 2021
  • Application for summer of FPGA, Anomaly detection using audio data

    vishwasn
    vishwasn
    After the industrial revolution in the 18th-century machines are vital parts of humans and they are very much essential to fulfill the demands of the fast-growing world. We as engineers should try toreduce the complexity and solve the existing proble...
    • 4 Oct 2021
<