Arduino

An open-source platform platform that makes hardware and software accessible for rapid prototyping, learning, experimenting, and tinkering. Discuss topics and share knowledge on the entire range of Arduino compatible boards and accessories, from Classic to MKR boards, and more.

Featured Content
image tile

How to Program the Arduino Opta PLC

This article explores how Arduino-based Opta® PLC can mitigate PLC programming challenges. It also introduces the Arduino PLC programming environment, highlighting its benefits and applications in automation

Read Blog

image tile

Exploring Arduino Pro's Role in Industry 4.0

This webinar highlights how edge computing technology can drive efficiency in applications related to Industry 4.0.

image tile

Arduino Giga R1 WiFi

Buy Now    Tech Specs

The Giga R1 packs BLE and the power of the STM32H7, the processor used in the Portenta H7, into the accessible Mega form factor.

Read Blog
image tile

Nicla Sense

Buy Now

An intelligent board that features industrial-grade sensors, including a Bosch Sensortec BHI260AP motion sensor system with embedded AI.

image tile

Nano 33 BLE Sense

Buy Now

A low-power board with built-in BLE and Bluetooth 5, featuring temperature, pressure, humidity, light, and gestures sensors.

design challenge tile

Arduino Edge Control Board

Buy Now

Designed for precision farming applications, this control board is well suited for irrigation with modular connectivity.

Recent Discussions
Arduino Day Content
More
Recent Blogs
Related Projects
  • UNO R4 on the big screen

    element14 sent me an Arduino UNO R4 MINIMA, so I though I would show that it is compatible with the original UNO in addition to being way more powerful. To do this demo, I just plugged in a display shield designed for an original UNO and presto - it …
  • Adding more Storage to an Arduino: Using 8-pin SPI Flash Memory Chips

    Table of Contents Introduction Simple Read Example Erasing Flash Simple Write Example What’s the Purpose? Connecting the SPI Flash Arduino Flash Library Simple Demo Code Flash Monitor / Programmer Menu access Python access Summary Int…
  • 10 Best ideas for Easy Arduino Projects

    The Arduino platform has become quite popular with people just starting out with electronics. It is an open-source hardware design, based on microcontroller board designs and provide sets of digital and analog I/O pins that can be interfaced to vario…
  • On-line battery bank monitor

    Arduino HomeAn Open-Source platform to create digital devices and interactive objects that sense and control physical devices.Arduino TutorialsArduino Projects 1、On-line battery bank monitorThis project, On-line battery bank monitor, can trace v...
  • Arduino-Based Automatic Guitar Tuner

     One of the most important things when playing guitar is making sure that the instrument is in tune. Even the best guitar player will not sound any good with an out-of-tune guitar. Tuning guitars by hand using a standard tuner has always been co...