![]() | Learn basic electronics, explore STEM subjects, get what you need to know to get started on electronics projects, and more. | The Learning Circuit |
| sudo Sergeant | ||
| The Ben Heck Show |
In today’s episode, we’re going to make a project using Diodes and Logic. Karen wants to build a skylight where there four LEDs, a white one for the moon and three colors (green, blue, and purple) for three different clusters of stars. It will have three switches. If switch one is on, then the green stars and the moon will be on. Blue and purple would be off. If switch 2 is on then the blue stars and the moon will be on. Green and purple would be off. If switch 3 is on then the purple stars and the moon is on. Green and Blue would be off. To make this happen we’ll need some diodes and to draw out our circuits to see how we’ll have to wire it up, to make it work. |
| Product Name | Manufacturer | Quantity | Buy KitBuy Kit |
|---|---|---|---|
2238 - Battery Holder, PP3 (9V) x 1, Strap, Wire Leads | KEYSTONE | 1 | Buy NowBuy Now |
| LED, Purple, Through Hole, T-1 3/4 (5mm), 30 mA, 3 V, 405 nm | VCC | 1 | Buy NowBuy Now |
| LED, Blue, Through Hole, T-1 3/4 (5mm), 20 mA, 3.2 V, 480 nm | CREE | 1 | Buy NowBuy Now |
| LED, Green, Through Hole, 5mm, 20 mA, 3.2 V, 527 nm | CREE | 1 | Buy NowBuy Now |
| LED, Cool White, Through Hole, T-1 3/4 (5mm), 20 mA, 3.2 V, 46.1 cd | CREE | 1 | Buy NowBuy Now |
| Through Hole Resistor, 330 ohm, 250 mW | MULTICOMP | 1 | Buy NowBuy Now |
| Toggle Switch, SPDT, On-Off-On, Panel, 5 A | MULTICOMP | 1 | Buy NowBuy Now |
| Standard Recovery Diode, 1 kV, 1 A, Single, 750 mV, 30 A | NTE ELECTRONICS | 1 | Buy NowBuy Now |