Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Open-source Casio FX-9750 and web broswer app to restore Hasbro Smart R2D2 functionality

    MikeNZ
    MikeNZ
    The droid that outlived its app A graphing calculator, an ESP32, and a toy nobody can play with - until now... Hasbro's Smart R2-D2 was sold in 2016 with an Android app that controlled it over Bluetooth. Modern phones will not ins...
    • 31 Aug 2026
  • Discrete difference amplifier - AC analysis: gain and bandwidth

    Jan Cumps
    Jan Cumps
    This is the AC gain and BW analysis of the difference amplifier module that shabaz designed for a Direct Conversion Receiver. I'm searching for these points: gain at 1 kHz (approx. mid of bandwidth) -3 dB frequencies ...
    • 14 Jul 2026
  • Discrete difference amplifier - DC analysis

    Jan Cumps
    Jan Cumps
    This is the DC analysis of the difference amplifier module that shabaz designed for a Direct Conversion Receiver. Before going into the small signal AC analysis, it's interesting to see how the amplifier behaves in steady state (...
    • 4 Jul 2026
  • GitHub for Professional Beginners: From First Repository to First Release

    shabaz
    shabaz
    Table of Contents Introduction What are Code Branches and Code Commits? Some Terminology, and the Branch Strategy! Main Branch Development Branch Release Branch Feature Branch Local and Remote Push versus Pull versus Pull Request! At-a-Glance Ov...
    • 6 Jun 2026
  • Building a Transistor Audio Preamplifier

    shabaz
    shabaz
    Introduction This blog post discusses a high quality three-transistor audio preamp, intended for speech applications such as radio or intercoms. The circuit was designed by michaelkellett and there is more detail at the blog page Two p...
    • 25 May 2026
  • Reflow Micro Table: Compact USB PD Reflow Table with Browser Control

    Reflow Micro Table: Compact USB PD Reflow Table with Browser Control

    pvit
    pvit
    www.youtube.com/watch Reflow Micro Table is a compact Bluetooth-controlled reflow table with an 80×70 mm working area. It is built for those who assemble PCBs from time to time and do not want a bulky professional-grade machine taking up desk ...
    • 11 Apr 2026
  • Simple DCR (Direct Conversion Receiver) – Part 2: Common Emitter Amplifier

    shabaz
    shabaz
    Table of Contents Introduction Circuit Diagram Dealing with Inputs and Outputs Power Supply Problem! Applying a Signal Frequency Response Loading the Amplifier Testing Both Stages Together Summary For all blog posts in this series, click here, o...
    • 24 Mar 2026
  • A 4-zone universal transmitter node for open-drain sensors (Proof of Concept)

    BigG
    BigG
    Introduction Traditional home security systems have long relied on a centralized architecture. All of the signal processing and control logic lives in a single, often bulky, cabinet. The user interface is usually just a simple keypad used for arming ...
    • 19 Mar 2026
  • Simple DCR: Assembling a 7 MHz (40m) Direct Conversion Radio Receiver – Part 1

    shabaz
    shabaz
    Table of Contents Introduction How Does It Work? How to Build It? Circuit Diagram What Has Been Constructed So Far? Audio Amplifier Testing the Amplifier’s Third Stage Summary For all blog posts in this series, click here, or type simple_d...
    • 12 Mar 2026
  • EoRa-S3-900TB with FreeRTOS — LoRa Camera Control System --Avg 174 µA

    AB9NQ-William
    AB9NQ-William
    A long-range wireless camera battery control system built on the EoRa-S3-900TB development board (ESP32-S3 + SX1262 LoRa). A FreeRTOS-based Transmitter (TX) sends commands over LoRa to a deep-sleep Receiver (RX) that controls camera power v...
    • 28 Feb 2026
  • Easy Xmas Gift: Simple LED Name Signs or Night-Lights

    shabaz
    shabaz
    I had a small request from a friend to produce a night-light that spelled out his kids' names. This turned out to be a very easy project. I obtained quarter-circle wood dowel with a 45-degree cut on the inside, instead of a sharp 90 degree corne...
    • 8 Dec 2025
  • MiniThermaDrive: Fun with 3D Printer Heating Elements - Part 1

    shabaz
    shabaz
    Table of Contents Introduction What can it be used for? High-Level Design Driver Board Summary Introduction Ever wanted to heat something to a precise temperature? I have, but I initially didn’t know how to go about it. 3D printer spares a...
    • 5 Nov 2025
  • LoRa Standalone Sensor Network ~45 µA Node with radio.sleep and deep sleep

    AB9NQ-William
    AB9NQ-William
    "LoRa BME280 Sensor Network" a collaboration between Anthropic's Claude and William Lucid. Project requires two, "Ebyte" EoRa-S3-900TB Development Boards; one for Gateway and one for Node. One 74HC04 for each node to reroute the Lora DIO1 signal to ...
    • 9 Oct 2025
  • CH340: Building Yet Another USB-C to UART Adapter Board

    shabaz
    shabaz
    Table of Contents Introduction Features Circuit Diagram Building It Using It Summary Introduction USB-to-UART adapters are extremely useful when connecting devices, as UART is a widely standard protocol available on many microcontrollers and per...
    • 27 Aug 2025
  • Building a VK5JST Antenna Analyzer for HF, VHF and UHF

    shabaz
    shabaz
    Table of Contents Introduction Obtain a Kit of Parts Building an Enclosure Flex PCB Construction Panel Meter End Panel RF Connector Assembly Main Board Parts Soldering Joining the End Panel and Main Board Attaching the End Panel/Main Board Assembly...
    • 8 Jun 2025
  • A Three-Way Prototyping Board for Awkward Through-Hole Components

    shabaz
    shabaz
    Table of Contents Introduction What Problems Does it Solve? Working with Dual-in-Line (DIL)Headers Working With Pi Pico and other Wide DIP Devices Easy Desoldering Easy Grounding Large Screw Terminals and Connectors Support Summary Introd...
    • 14 Mar 2025
  • Half-Hour Project: Building a Simple Audio Amplifier

    shabaz
    shabaz
    Table of Contents Introduction How Does it Work? Building It Using It Summary Introduction A while back I built a little audio amplifier based on a circuit found in an old book. The amplifier performed reasonably OK (by that I mean adequat...
    • 5 Mar 2025
  • KiCad 8: Working with Circuit Simulations!

    shabaz
    shabaz
    Table of Contents Introduction Create the Schematic Adding SPICE models Adding Simulation Voltages Running a Simulation Plotting Frequency Response Simulating Parts of a Circuit (Excluding some Components) Summary Introduction The recent release...
    • 5 Sep 2024
  • Bridgetek EVE Series - Touch Enabled Graphical User Interfaces

    BRT-Marketing
    BRT-Marketing
    Bridgetek’s products include the EVE family of display controllers which make it easy to add attractive and fully featured touch-enabled graphical user interfaces to existing and new product designs. To improve the user experience and functiona...
    • 26 Jan 2024
  • High Voltage Isolated Measurement Board: Initial Prototype

    High Voltage Isolated Measurement Board: Initial Prototype

    shabaz
    shabaz
    Introduction In an earlier blog post  Very Low-Cost Pulse-Width Modulation (PWM), and Isolated Analog Measurements  a method was discussed to perform isolated analog measurements at a sub-£1/$1 price. It was fine for slow-ch...
    • 13 Dec 2023
  • Very Low-Cost Pulse-Width Modulation (PWM), and Isolated Analog Measurements

    shabaz
    shabaz
    This is just an ultra-quick blog post about an interesting circuit. I wanted to be able to measure an output up to about 1kV, and so I really desired the measurement to be isolated! I also wanted it to be cheap. This blog post shows the method I won&...
    • 24 Nov 2023
  • Writing Decent Blogs: A Blog Checklist!

    shabaz
    shabaz
    Table of Contents Introduction: What’s a Blog Checklist? Good Flow, Bad Flow? Value Fun to Read? Is the Content Appropriate? Is the Content Relevant? Use a Table of Contents Write an Introduction Write a Summary Make Use of the Editor To...
    • 12 Nov 2023
  • GitHub for Beginners: Feature Development for Projects

    GitHub for Beginners: Feature Development for Projects

    shabaz
    shabaz
    This blog post is a joint effort by Jan Cumps   and shabaz   Table of Contents Introduction IDE Capabilities JetBrains Products Visual Studio Code A Suggested Strategy Fork the Project Repository Cloning your Reposi...
    • 11 Aug 2023
  • Using Buses in Circuits with KiCad 7

    Using Buses in Circuits with KiCad 7

    shabaz
    shabaz
    This topic is a bit fiddly to describe in words, so I hope the video will suffice. This blog won't have much text : ( I feel like a Ronin when I'm not having to type though! : ( https://youtu.be/T5Zy_BWg3Tw
    • 29 Jul 2023
  • Vintage Curvy PCB Traces with KiCad 7

    Vintage Curvy PCB Traces with KiCad 7

    shabaz
    shabaz
    Table of Contents Introduction What’s Required? Running the Plugin Fixing Issues Summary Introduction Old-school printed circuit boards (PCBs) often had wavy copper traces! They were done manually by rolling out UV-light-blocking crepe sti...
    • 3 Jul 2023
>