RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!

Review Blogs

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Raspberry Pi CM5 roadtest - system boot and RTL-SDR setup

    Raspberry Pi CM5 roadtest - system boot and RTL-SDR setup

    gpolder
    gpolder
    System boot Now that Linux is installed, it's time for the first boot. I'm using a Joy-IT RB-LCD10 touchscreen monitor with a resolution of 1280 × 800 pixels. During startup, the system asks for several configuration parameters, including the l...
    • 16 Sep 2026
  • Raspberry Pi CM5 - Frigate NVR Benchmark Preparation Part 2

    ralphjy
    ralphjy
    Thermal Tests continued I had forgotten to mention in my previous post that after the roadtest benchmarking is complete that I still want to monitor thermal and power parameters on the Frigate NVR.  To that end, I'm going to create MQTT sens...
    • 14 Sep 2026
  • Raspberry Pi CM5 - Frigate NVR Benchmark Preparation Part 1

    ralphjy
    ralphjy
    My objective for this roadtest is to evaluate the performance of the CM5 IO Development kit in implementing a Frigate NVR for my home security cameras. This is the description in my Roadtest Application: " I currently run a home automa...
    • 12 Sep 2026
  • Raspberry Pi CM5 - Firmware Installation and Configuration

    ralphjy
    ralphjy
    Hardware is put together and ready to install and configure the OS firmware and install and configure the Frigate Docker container.  The CM5 in the roadtest uses eMMC rather than an SD card for storage so the process is slightly different using ...
    • 6 Sep 2026
  • Raspberry Pi CM5 roadtest - flashing the operating system

    gpolder
    gpolder
    Introduction Flashing an operating-system image to the Compute Module 5 is slightly different from what you may be used to with a traditional Raspberry Pi. With a regular Raspberry Pi, the usual procedure is to write Raspberry Pi OS to a microSD card...
    • 5 Sep 2026
  • Raspberry Pi CM5 roadtest - first impressions

    gpolder
    gpolder
    After a long wait, the Raspberry Pi Compute Module 5 Development Kit finally arrived at my desk, ready for its road test.My proposed plan is to test the Compute Module 5 with Software Defined Radio (SDR), using both RTL-SDR and Ettus Research USRP B2...
    • 29 Aug 2026
  • Ras Pi CM5 roadtest - 02 - network, storage, and web cam

    saramic
    saramic
    For my RoadTest review of the CM5 I am building a remote dog feeder. I am planning to use a pair of CSI (Camera Serial Interface) cameras, which are still in transit. After my unboxing post, I thought it would be wroth while to run thr...
    • 29 Aug 2026
  • Raspberry Pi CM5 - Initial Assembly

    ralphjy
    ralphjy
    I finally received my CM5 Development kit for the roadtest, so I thought I'd get started assembling it. Unboxing Not much exciting about the shipping package, so I'll get right to the good stuff.   There were two boxes included, the...
    • 22 Aug 2026
  • Ras Pi CM5 roadtest - 01 - unboxing

    saramic
    saramic
    To keep myself accountable, I thought it best to blog my progress with the Raspberry Pi Compute Module 5 Development Kit before doing a full RoadTest review. My roadtest plan was to build a remote-control dog feeder that, with a bit of...
    • 22 Aug 2026
  • Pynq Z2 oled display from Jupyter

    James_UoD
    James_UoD
    I have looked at many examples, blogs and websites to try to get an output from an SSD1306 OLED connected to the Pynq Z2 Arduino pins or to  a Grove Arduino shield. If you are interested to understand my testing and experimental logic, read on. ...
    • 10 Aug 2026
  • Raspberry Pi+ low latency video streaming

    abhaydevcloudsupport
    abhaydevcloudsupport
    hey there i have been experimenting Raspberry Pi zero 2 w Camera setup and exploring low latency video streaming for remote monitoring, has anyone used WebRTC or similar technologies for this approach to archive near real time video streaming using R...
    • 8 Jun 2026
  • Element13 April Fools RoadTest

    ntewinkel
    ntewinkel
    You’ve gotta love it when a company goes all in on an April fools joke and calls your bluff…  I saw the April Fools days posts about changing “element14” to “element13” and setting up an Aluminum foil Road Te...
    • 21 May 2026
  • Received element13 Foil Headwave Aluminium aTtenuator DevKit for review

    ralphjy
    ralphjy
    I just received the Aluminium aTtenuator DevKit for review. The sturdy Aluminium foil was neatly folded and came with a complement of stickers. I had proposed using the foil as a Faraday shield to mitigate my tinnitus. The most difficult part o...
    • 5 May 2026
  • Arduino Uno Q - USB Audio

    ralphjy
    ralphjy
    Now that I've got two different ways to attach USB peripherals (hub and OTG adapter) to the Uno Q, I decided to try out a couple of audio apps with a USB speaker. First I used the Sound Generator Brick to create some music.  This h...
    • 25 Apr 2026
  • Arduino Uno Q and USB3 adapter with USB-C PD

    ralphjy
    ralphjy
    While I was waiting to receive my USB-C Hub, I watched the Official Arduino Days 2026: Day 1 video on YouTube.  At the 1 hour and 33 minute mark there is a presentation about using Custom AI Models in AppLab.  Christopher Mendez is the...
    • 14 Apr 2026
  • Arduino Uno Q - Standalone Operation

    ralphjy
    ralphjy
    Received the shipment of the USB-C accessories for the roadtest.  Thanks OwainM  and E14Alice .  Stickers are a nice addition. Multicomp Pro USB-C PD Power Supply 30W, MP009260 TP-Link USB-C 9-Port Hub USB-C Cable 2M US...
    • 12 Apr 2026
  • Arduino nano r4 review

    neerajrd82
    neerajrd82
    Section: Unboxing, Initial Setup & Failure Analysis – Arduino Nano R4 1. Unboxing & First Impressions The Arduino Nano R4 was received in standard Arduino packaging with the board securely enclosed in an anti-static cover. Package ...
    • 11 Apr 2026
  • Arduino Uno Q - AppLab initial configuration and examples

    ralphjy
    ralphjy
    I received notification that the additional parts (USB-C hub and power supply) for the roadtest had shipped, so hopefully I'll receive those parts soon.  In the meantime, I've gotten started installing AppLab and configuring the Uno Q an...
    • 5 Apr 2026
  • Arduino Uno Q - getting started

    ralphjy
    ralphjy
    Simple Baseplate I will probably 3D print a custom case later when I do my final roadtest project, but for initial testing I just want a simple baseplate to protect the board with easy access to all of the connectors.  With a quick search I...
    • 23 Mar 2026
  • Arduino Uno Q - Board received

    ralphjy
    ralphjy
    I just received my Arduino Uno Q board via FedEx for the roadtest.  Thanks E14Alice  and OwainM .  There will be a second shipment later that has the USB-C Hub and USB-C power supply.  While I wait for the other par...
    • 18 Mar 2026
  • Giga Oscilloscope

    dougw
    dougw
    Intro The last demo I want to show in this road test is an oscilloscope application. The Arduino Giga with its display has the infrastructure to implement an oscilloscope function so I wanted to include a quick demo of this in action.. This demo simp...
    • 2 Dec 2025
  • GIGA Paint

    dougw
    dougw
    Intro This is one more little demonstration of how powerful the combination of an Arduino Giga and its touch LCD is. A very simple finger paint program can be implemented using only the hardware included in the road test kit. Here is a brief video d...
    • 30 Nov 2025
  • GIGA MQTT Client

    dougw
    dougw
    Intro For quite a while now I have wanted to explore the idea of using MQTT as a text messaging system, where users publish and subscribe to a topic of mutual interest - forming an interest group. The Arduino GIGA with its display is an excellent&nbs...
    • 27 Nov 2025
  • STM_WURTH_Special_Project STWIN_box

    STMicro, WURTH Elektronik and E14 Special Project - SensorTile Wireless Industrial Node

    Robert Peter Oakes
    Robert Peter Oakes
    STMicroelectronics, WURTH Elektronik and Element14 have created a Special Project which comprises an STMicroelectronics Motor Control Evaluation kit. EVLSPIN32G4-ACT  Motor control Evaluation Board STLINK-V3SET  Programmer/debugg...
    • 26 Nov 2025
  • Arduino GIGA Touch Display HID Keyboard

    dougw
    dougw
    Intro I have implemented lots of HID style peripherals in the past, but I have never made a capacitive touch keyboard HID before. The GIGA with its touch display means a touch keyboard can be implemented without any extra hardware, so that is what th...
    • 17 Nov 2025
>